Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Documents
Currently Being Moderated

LG announces Optimus LTE2 with 2GB of RAM

VERSION 1 
Created on: 4/05/2012 11:57 AM by squadMCU - Last Modified:  4/05/2012 11:58 AM by squadMCU

Not to be outdone by its Korean counterpart, LG announced its own flagship smartphone on the same day as the the Galaxy S III. The  Optimus LTE2, as it is called, is no less when it comes to features and  specifications and in some aspects even outdoes Samsung's offering.

 

http://st.gsmarena.com/vv/newsimg/12/05/lg-optimus-lte2/gsmarena_001.jpg

For starters, the design seems to be a bit better. While Samsung has  gone with an all plastic body, LG has opted for a bit of glass and  metal, in other words, something befitting of a flagship device.

 

The  display on the phone is something that LG likes to call TrueHD IPS  display. It's likely to be a 720p display and the 'True' part comes from  it having a standard RGB subpixel layout, unlike the display on the  Galaxy S III that uses a PenTile RGBG layout. Looking at the performance  of recent LCDs, we think the display on the Optimus LTE2 is going to be more than a match for the one on the Galaxy S III.

 

The main feature here, however, is the inclusion of a stonking 2GB of RAM,  a first for any smartphone. While it is debatable if the extra gigabyte  will make any noticeable difference, at least you will never have to  worry about running out of memory while multitasking.

 

Other features include wireless induction charging, LTE connectivity, a camera that can be operated using your voice, 2,150mAh battery and Android  4.0. Unfortunately, there is no mention of what processor the phone is running on but the presence of LTE suggests that it could be (and we hope it is) Qualcomm's Snapdragon S4.

The  phone is expected to go on sale in Korea by mid-May. Hopefully, LG  announces international availability soon, along with some proper  specifications.

 

Source

Comments (0)