Potentiometers, Variable Resistors
Devices that control the current that flows through a circuit.
Trimmer Potentiometers
A variable device that opposes the flow of current. The resistance of these devices is changed using a rotary portion of the device (usually needing a separate tool) that is attached to the center axis of the component.
|
View all Trimmer Potentiometers
|
Adjustable Power Resistor
A variable device that opposes the flow of current. The resistance of these devices is changed moving a central terminal between one end and the other of the component.
|
View all Adjustable Power Resistor
|
Thumbwheel Potentiometers
A variable device that opposes the flow of current. The resistance of these devices is changed using a rotary disk that is attached to the center axis of the component.
|
View all Thumbwheel Potentiometers
|
Slide
A variable device that opposes the flow of current. The resistance of these devices is changed using a stem that moves between one end and the other of the component.
|
View all Slide
|
Scale Dials
A removable device with a face that is marked in predefined units to indicate the degree that a unit has been turned.
|
View all Scale Dials
|
Value Display Potentiometers
A variable device that opposes the flow of current. The resistance of these devices is changed by pushing a button or rotating a wheel. The values that the device is being changed to is displayed on the front of the unit.
|
View all Value Display Potentiometers
|
Kits
A grouping of potentiometers of various styles, sizes, and values.
|
View all Kits
|
Rotary Potentiometers, Rheostats
A variable device that opposes the flow of current. The resistance of these devices is changed using a revolving stem that is attached to the central axis.
|
View all Rotary Potentiometers, Rheostats
|