Login or
REGISTER
Research
Design
Search / Ordering
- Hillcrest Labs, a subsidiary of InterDigital, Inc. (NASDAQ:IDCC), is a leading global supplier of software, components, and intellectual property to enable the intelligent use of sensors in consumer electronics and IoT devices. For more than 10 years, Hillcrest’s Freespace® sensor processing technology has powered advanced motion controllers in a wide variety of products including Smart TV’s, set-top boxes, PC’s, and game consoles. Today, Hillcrest’s products are used in the development of devices in the virtual reality (VR), augmented reality (AR), robotics, TV, and motion remote control segments. Their proprietary and patented Freespace technology transforms human and machine movement into high quality, application-ready information which enables developers and manufacturers to create everyday products that work with precision.
FSM-9 and FSM-9 OEM Freespace® Sensor Modules
Hillcrest’s FSM-9 is a low-cost, battery operable, fully calibrated inertial measurement unit (IMU) / attitude heading reference system (AHRS).
FSM30x Series IMU Modules
The Hillcrest Labs FSM30X incorporates the BNO080, a 32.768 kHz crystal and passive components into a compact module form factor.
BNO08x Series IMU
Hillcrest’s BNO080 is a SiP IMU that integrates a triaxial accelerometer, triaxial gyroscope, magnetometer, and a 32-bit microcontroller running SH-2 firmware.
Hillcrest and Bosch New Product Discoveries Episode 17
On episode 17 of New Product Discoveries Randall discusses features of an IMU (Inertial Measurement Unit) from Hillcrest Laboratories and a Transport Data Logger from Bosch Connected Devices and Solutions.
Publish Date: 2018-04-10
Meet Hillcrest Labs
Hillcrest Labs is a leading global supplier of software, hardware and services that enable the intelligent use of sensors in consumer electronics and IoT devices.
Publish Date: 2017-11-30