Identifying Capacitor Polarization
Polarized capacitors will always have some sort of designator on them identifying polarity. This is important, because hooking one up backwards can be dangerous.
Aluminum caps can be marked in a number of different ways. Radial, through-hole cans will commonly have a line down the negative side of the body, with the negative lead being shorter as well. Radial, surface mount cans will have a colored portion on the top indicating the negative pad. Axial cans will have a line on one side with arrows pointing to the negative lead, or an indented band that designates the positive lead.
Surface mount tantalum chips will have a line and/or a notch on the positive end. Axial will have a notch on the positive side. Radial has either an arrow or positive indicator above the positive lead.
Below are some images of the examples above with full descriptions of what each one is. If you’re working with these products and are unsure or having a hard time deciphering, you can always refer to the datasheet or contact someone for assistance.
Figure 1: Line and short lead indicate negative lead
Figure 2: Colored block on top indicates negative lead
Figure 3: Line with arrows are pointing at negative lead
Figure 4: Indented band and + signs indicate positive lead
Figure 5: Chamfered edge and line indicate positive lead
Figure 6: Chamfered edge indicates positive lead
Figure 7: Line and + symbol are difficult to see here, but if you can see them on the image they indicate the positive lead.
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum