Maker.io main logo

What Makes the Arduino Uno Mini LE Different?

119

2026-02-09 | By Andrew Kazour

Microcontrollers Arduino

Everyone who’s tinkered with electronics has probably used an Arduino Uno at some point. It’s one of the most popular microcontroller boards in the world as it is reliable, simple, and a great platform for learning how hardware and software come together.

To celebrate the legacy of this amazing board, Arduino released the Arduino Uno Mini Limited Edition (LE), which is a smaller and slightly more powerful version that keeps all the power of the original in a new gold-and-black design. Let’s take a deep dive into what makes it special and how it compares to its older brother.

Image of What Makes the Arduino Uno Mini LE Different? Image Credit: https://commons.wikimedia.org/wiki/File:UNO-mini-LE-Packaging-sml-1024x683.png

________________________________________

1. A Smaller Tribute to the Original

The Uno Mini LE is a scaled-down version of the original Uno, which was made to mark over a decade of Arduino innovation. Even though it’s about half the size, it has many of the components and performance results as the Uno.

Just like the full-sized board, it uses the ATmega328P as the main microcontroller and the ATmega16U2 as the USB-to-serial converter. That means everything works exactly the same way as the Uno. It is basically the Uno, but smaller and with some very slight upgrades.

Image of What Makes the Arduino Uno Mini LE Different?

________________________________________

2. What’s Inside the Uno Mini LE

Underneath the gold accents, the Uno Mini LE is a fully functional development board. It has all you need to make your projects just like with the Uno. Even with the small size, it has the same GPIO pins as the Uno R3.

Key Specs:

  • Microcontroller: ATmega328P (8-bit AVR, up to 16 MHz)
  • USB Interface: ATmega16U2
  • Memory: 32 KB Flash, 2 KB SRAM, 1 KB EEPROM
  • Operating Voltage: 5V
  • Input Voltage Range (VIN): 6–20V
  • Digital I/O Pins: 14 (6 PWM capable)
  • Analog Inputs: 6 (10-bit ADC)
  • Communication: UART, SPI, I²C
  • USB Connection: USB-C
  • Max Current per I/O Pin: 20 mA
  • Max 3.3V Pin Current: 500 mA

One of the biggest improvements is the jump from the old USB-B connector to a USB-C port. This modernizes the board and makes it a lot easier for people to actually interface with. Most people don't have a USB-B cable, but now we all have USB-C cables to charge our phones, which makes it more convenient to use.

Image of What Makes the Arduino Uno Mini LE Different?

________________________________________

3. How It Compares to the Uno

Functionally, both boards are identical. They share the same microcontroller, the same pin layout, and the same I/O voltage levels. If your code runs on the Uno, it will run on the Uno Mini LE without any changes.

Here’s what’s the same:

  • 14 digital I/O and 6 analog input pins.
  • PWM, I²C, SPI, and UART capabilities.
  • 5V logic and 16 MHz clock speed.
  • Arduino IDE and Arduino Cloud compatibility.

And here’s what’s new:

  • Compact form factor — about a fourth the size of the original board.
  • USB-C connector instead of USB-B.
  • Higher current capacity on the 3.3V pin (500 mA vs 50 mA).

Despite its smaller footprint, the Uno Mini LE manages to keep the same pin headers (just in a denser layout), making it compatible with jumper wires and breadboards. This makes it perfect for prototyping and easier to fit into a housing due to its size.

Image of What Makes the Arduino Uno Mini LE Different? Image credit: https://en.wikipedia.org/wiki/Arduino_Uno

________________________________________

4. Power and Performance

Power delivery on the Uno Mini LE is handled by an MPM3610AGQV step-down converter, capable of supplying up to 1.2A. This allows the board to maintain stable operation even when powering multiple peripherals. This could mean in many circumstances you won't need an external power supply going directly into the peripherals and can use on-board power. The board can be powered through USB-C up to 5.5V or through the VIN pin, which accepts up to 20V.

Image of What Makes the Arduino Uno Mini LE Different? MPM3610AGQV step-down converter

Image Credit: https://www.digikey.com/en/products/detail/monolithic-power-systems-inc/MPM3610AGQV-P/5299006

________________________________________

5. Ideal Use Cases

This little Arduino has just as many use cases as the original, if not more:

  • Educational projects — same functionality, smaller footprint.
  • Embedded prototypes — fits into compact enclosures.
  • IoT and sensor applications — 3.3V devices can draw more current.
  • Portable robotics and drones — lighter and space-efficient.
  • Collectors and enthusiasts — unique numbered design and premium finish.

It’s designed as both a functional tool and a commemorative piece that celebrates what Arduino has done over the years. It can be used in many use cases, just like the Uno R3, but with the added benefit of being smaller with some upgrades.

Image of What Makes the Arduino Uno Mini LE Different?

Image Credit: https://commons.wikimedia.org/wiki/File:RoboRobo_Educational_Robots_2023.jpg

________________________________________

Conclusion

The Arduino Uno Mini Limited Edition is a really great small protoboard for all your needs. It has everything that made the original Uno a great board, but with a smaller form factor. This smaller factor makes it a direct upgrade from the original and a worthy commemoration piece.

Whether you’re learning embedded programming, prototyping new hardware, or simply adding it to your collection, the Uno Mini LE is one of the best ways to do it.

Mfr Part # ABX00062
ARDUINO UNO MINI LE
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.