Maker.io main logo

Air Velocity Sensor Breakout - FS3000 Hookup Guide

207

2025-05-06 | By SparkFun Electronics

License: None Arduino Qwiic

Courtesy of SparkFun

Guide by QCPete, Ell C

Introduction

Need to keep track of the airflow in your data center or around your servers? How about ‎making sure your HVAC and air control systems are functioning at full capacity? Or, if you're ‎more fun, what about figuring out how fast your RC airplane is going? Well, the SparkFun ‎Air Velocity Sensor Breakout - FS3000-1005 and FS3000-1015 can help you with all that ‎and more! It's super easy, super Qwiic to hookup, and super fun to play with. Let's have a ‎look!‎

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need ‎everything though depending on what you have. Add it to your cart, read through the guide, ‎and adjust the cart as necessary.‎

Air Velocity Sensor Breakout - FS3000-1005 Wish List

Air Velocity Sensor Breakout - FS3000-1015 Wish List‎

Note: If you decide to use the Artemis RedBoard Nano, make sure to install the Arduino ‎Board Add-On in Arduino and select the appropriate board when uploading code!‎

Suggested Reading

If you aren't familiar with the Qwiic system, take a look here for an overview.‎

qwiic_1

We also recommend taking a look at the following tutorials if you aren't familiar with the ‎concepts covered in them.‎

  • What is an Arduino? What is this 'Arduino' thing anyway? These tutorials dive into what an ‎Arduino is and along with Arduino projects and widgets.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software ‎on Windows, Mac, and Linux.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use ‎today.‎

Hardware Overview

FS3000‎

The FS3000 is a surface-mount type air velocity module utilizing a MEMS thermopile-based ‎sensor. It features a digital output with 12-bit resolution and comprises a “solid” thermal ‎isolation technology and silicon carbide coating to protect it from abrasive wear and water ‎condensation.‎

There are two versions of this sensor with different upper ranges (1005/1015). The 1005 ‎version which can sense 0 to 7.23m/s (0 to 16.17mph) and 1015 version which can sense ‎‎0 to 15m/s (0 to 33.6mph). By looking at the PCB, there will be a solder blob indicating ‎which version that you ordered and received. You can also check out the markings labeled ‎on the IC. You'll also notice the arrow on the matching the silkscreen indicating what ‎direction air should flow for a measurement. For the scope of this tutorial, we will be using ‎the FS3000-1005 mostly to highlight the board and connect.‎

1005_2

FS3000-1005 [ SEN-18377 ]‎

1015_3

FS3000-1015 [ SEN-18768 ]‎

Below is a table of a few of the specifications taken from the datasheet. For more in-depth ‎information on this chip, please refer to the datasheet linked in the Resources and Going ‎Further.‎

table_4

Qwiic Connectors

Our Qwiic Ecosystem makes sensors pretty much plug and play. There are two Qwiic ‎connectors on either side of the Qwiic Air Velocity Sensor board to provide power and I2C ‎connectivity simultaneously. The sensor's I2C lines are connected to two 2.2kΩ pull-up ‎resistors. The I2C address of the board is 0x28.

board_5

Pins

Power

Ideally, power will be supplied via the Qwiic connectors on either side of the board. ‎Alternatively, power can be supplied through the header along the bottom side of the board ‎labeled 3V3 and GND. The input voltage range should be between 2.7-3.3V. The usual ‎current draw is around 10mA.‎

power_6

I2C

The I2C pins break out the functionality of the Qwiic connectors. Depending on your ‎application, you can connect to these pins via the plated through holes for SDA and SCL.‎

i2c_7

VCM and ADCR

VCM is an output from the sensor that provides a common bias voltage. With a power ‎supply voltage at 3.3V (usual for Qwiic), the VCM pin will output 1.25V. The current ‎datasheet does not provide any more information about this pin; however, it is most likely a ‎bias voltage used with some sort of analog gain stage internal to the sensor (prior to its ‎internal ADC). This can be useful for unique more advanced projects that may benefit from ‎having a known bias voltage tied to another analog system.‎

ADCR stands for ADC Reference. This is an input to the FS3000 which allows you to provide ‎a reference voltage for the sensor's internal ADC. Note, you must first cut the "ADC-REF" ‎jumper (on the bottom side of the board) before providing a custom voltage to this pin. By ‎default, it is connected to VDD.‎

output_8

Jumpers

LED

If power consumption is an issue, cutting this jumper will disable the Power LED on the ‎front of the board.‎

pwr_9

PWR LED

on Top Side

led_10

LED Jumper

on Bottom Side

ADC-REF

Cut the ADC-REF jumper to provide your own custom ADC reference voltage on the ADCR ‎header pin. By default (jumper closed), it is connected to VDD.‎

jumper_11

I2C

The SparkFun Air Velocity Sensor has pull up resistors attached to the I2C bus; if multiple ‎sensors are connected to the bus with the pull-up resistors enabled, the parallel equivalent ‎resistance will create too strong of a pull-up for the bus to operate correctly. As a general ‎rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected ‎to the bus. If you need to disconnect the pull up resistors, they can be removed by cutting ‎the traces on the corresponding jumpers highlighted below.‎

bus_12

Board Outline

outline_13

Hardware Hookup

Using the Qwiic system, assembling the hardware is simple. All you need to do is connect ‎your Air Velocity Sensor Breakout to your chosen development board with a Qwiic cable ‎or adapter cable. Otherwise, you can use the I2C pins broken out if you do not have a Qwiic ‎connector on your development board or if you do not want to use a Qwiic connection. If ‎you are not using a Qwiic-enabled board, make sure your input voltage and logic are either ‎running at 3.3V or you are shifting the logic level from whatever logic your controller runs at ‎to 3.3V.‎

hookup_14

Software Setup and Programming

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop.

If this is your first time using Arduino, please review our tutorial on installing the Arduino ‎IDE. If you have not previously installed an Arduino library, please check out our installation ‎guide.‎

SparkFun has written a library to work with the Qwiic Air Velocity Sensor. You can obtain ‎this library through the Arduino Library Manager by searching for "SparkFun FS3000". Find ‎the one written by SparkFun Electronics and install the latest version. If you prefer ‎downloading libraries manually, you can grab them from the GitHub Repository or by ‎clicking on the button below.‎

SparkFun Air Velocity Sensor Breakout - FS3000 (Qwiic) Arduino Library GitHub

Readings

The FS3000 has a response time of 125ms. In the provided example, we are only taking ‎readings from the sensor once per second, so this is well above the response time. If you ‎wish to take a higher frequency of readings, make sure to add in at least a 125ms delay in ‎between each read.‎

To calculate or understand airflow and how it relates to diameter, you can use this tool.‎

Functions

Below is a list of the functions that can be used with the Air Velocity Sensor, along with a ‎description of what each function does and how to use it.‎

  • FS3000() - Base constructor

  • begin() -- Initialize the sensor. Returns false if sensor is not detected.‎

  • isConnected() -- Returns true if I2C device ack's

  • fs.setRange() -- Sets the range for the IC that is connected to the Arduino ‎microcontroller. You can input AIRFLOW_RANGE_7_MPS for the FS3000-1005 ‎or AIRFLOW_RANGE_15_MPS for the FS3000-1015.‎

  • readRaw() -- Read from sensor, checksum, return raw data (409-3686)‎

  • readMetersPerSecond() -- Read from sensor, checksum, return m/s (0-7.23)‎

  • readMilesPerHour() -- Read from sensor, checksum, return mph (0-33ish)‎

Note: If you are using a board with an Apollo core, please note that 100KHz on the Apollo ‎‎2.1.1 doesn't currently work. You will need to use 400KHz or jump back to Apollo 2.1.0.‎

Example Code

Once you've installed the FS3000 library, you should ‎see File > Examples > SparkFun_FS3000_Arduino_Library > Example01_BasicReadings to open the example sketch.‎

code_15

Alternatively, you can copy and paste the code below into a fresh Arduino sketch.‎

Copy Code
/******************************************************************************
  Example_01_BasicReadings.ino

  Read values of air velocity from the FS3000 sensor, print them to terminal.
  Prints raw data, m/s and mph.
  Note, the response time on the sensor is 125ms.

  SparkFun FS3000 Arduino Library
  Pete Lewis @ SparkFun Electronics
  Original Creation Date: August 5th, 2021
  https://github.com/sparkfun/SparkFun_FS3000_Arduino_Library

  Development environment specifics:

  IDE: Arduino 1.8.15
  Hardware Platform: SparkFun RedBoard Qwiic
  SparkFun Air Velocity Sensor Breakout - FS3000 (Qwiic) Version: 1.0

  Artemis RedBoard @ 400KHz (Core v2.1.0) 
  (note, v2.1.1 has a known issue with clock stretching at 100KHz)  

  Do you like this library? Help support SparkFun. Buy a board!

    SparkFun Air Velocity Sensor Breakout - FS3000-1005 (Qwiic)
    https://www.sparkfun.com/products/18377

    SparkFun Air Velocity Sensor Breakout - FS3000-1015 (Qwiic)
    https://www.sparkfun.com/products/18768

  Hardware Connections:
  Use a Qwiic cable to connect from the RedBoard Qwiic to the FS3000 breakout (QWIIC).
  You can also choose to wire up the connections using the header pins like so:

  ARDUINO --> FS3000
  SDA (A4) --> SDA
  SCL (A5) --> SCL
  3.3V --> 3.3V
  GND --> GND

  This program is distributed in the hope that it will be useful,
  but WITHOUT ANY WARRANTY; without even the implied warranty of
  MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
  GNU General Public License for more details.

  You should have received a copy of the GNU General Public License
  along with this program.  If not, see <http://www.gnu.org/licenses/>.
******************************************************************************/

#include <Wire.h>
#include <SparkFun_FS3000_Arduino_Library.h> //Click here to get the library: http://librarymanager/All#SparkFun_FS3000

FS3000 fs;

void setup()
{
  Serial.begin(115200);
  Serial.println("Example 1 - Reading values from the FS3000");

  Wire.begin();

  if (fs.begin() == false) //Begin communication over I2C
  {
    Serial.println("The sensor did not respond. Please check wiring.");
    while(1); //Freeze
  }

  // Set the range to match which version of the sensor you are using.
  // FS3000-1005 (0-7.23 m/sec) --->>>  AIRFLOW_RANGE_7_MPS
  // FS3000-1015 (0-15 m/sec)   --->>>  AIRFLOW_RANGE_15_MPS
  fs.setRange(AIRFLOW_RANGE_7_MPS);
  //fs.setRange(AIRFLOW_RANGE_15_MPS); 

  Serial.println("Sensor is connected properly.");
}

void loop()
{
    Serial.print("FS3000 Readings \tRaw: ");
    Serial.print(fs.readRaw()); // note, this returns an int from 0-3686

    Serial.print("\tm/s: ");
    Serial.print(fs.readMetersPerSecond()); // note, this returns a float from 0-7.23 for the FS3000-1005, and 0-15 for the FS3000-1015 

    Serial.print("\tmph: ");
    Serial.println(fs.readMilesPerHour()); // note, this returns a float from 0-16.17 for the FS3000-1005, and 0-33.55 for the FS3000-1015 


    delay(1000); // note, reponse time on the sensor is 125ms
}

Set your Board and Serial Port and then upload the sketch to your Arduino. Then open ‎the serial monitor. Make sure your baud rate is set to 115200. You'll begin to see output, ‎including raw data and translated miles per second and miles per hour.‎

open_16

Note that peak in the middle of the readings? That's where I pointed the sensor at the fan!‎

Troubleshooting

Need help?

If your product is not working as you expected or you need technical assistance or ‎information, head on over to the SparkFun Technical Assistance page for some initial ‎troubleshooting.

If you don't find what you need there, the SparkFun Forums are a great place to find and ask ‎for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.‎

Resources and Going Further

For more on the Air Velocity Sensor Breakout, check out some of the links below:‎

Mfr Part # 18377
QWIIC FS3000 AIR VELOCITY SENSOR
SparkFun Electronics
$111.35
View More Details
Mfr Part # 18768
SPARKFUN AIR VELOCITY SENSOR BRE
SparkFun Electronics
$147.51
View More Details
Mfr Part # 10215
USB MICRO-B CABLE - 6 FOOT
SparkFun Electronics
Mfr Part # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
More Info
View More Details
Mfr Part # 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Mfr Part # 21309
SPARKFUN AIR VELOCITY SENSOR QWI
SparkFun Electronics
More Info
View More Details
Mfr Part # 21310
SPARKFUN AIR VELOCITY SENSOR QWI
SparkFun Electronics
$127.79
View More Details
Mfr Part # 14425
QWIIC CABLE - BREADBOARD JUMPER
SparkFun Electronics
More Info
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.