Maker.io main logo

Another Ambassador Moment: Using the Adafruit Feather nRF52 Bluefruit LE

59

2021-04-09 | By Fredy Martinez

License: See Original Project

This project was designed by one of Digi-Key’s own university ambassador students. Check out how it works in the video below!

 

As technologies advance and projects become increasingly complex, it’s important to understand the basics of boards and their technologies before diving into more intricate projects. The Adafruit Feather nRF52 Bluefruit LE, which will be discussed in this article, is one board that can be used in a variety of different projects and applications.

board_1

project_2

Justification

Bluetooth is a critical technology in many different electrical systems today, which is why I chose to create a project with the Adafruit Feather nRF52 Bluefruit LE. This project, which follows Kevin Townsends Learning Guide and introduces the basics of using the Bluefruit nRF52, will introduce the nRF52 and some potential issues that can arise during setup.

BOM

Tools

Other Useful Information

pinout_3

feather_4

Project Description

nRF52_5

The first step when getting started with then RF52 is to solder in plain male headers. By doing this, the user can plug the Feather into a solderless breadboard. Using an adjustable circuit board holder allowed me to maneuver around the board to solder the headers in place. The board could have been held for the entire solder job, but I chose to solder one header on each side for the purpose of this project.

The rest of the headers were then soldered while the board was lying down. This technique is helpful because the initial soldering keeps the headers in place and allows the user to solder the rest of the headers quickly. The NeoPixel ring was harder to solder because of the headers, but the same technique can be repeated to simplify the process using the holder.

When the headers and NeoPixel ring are soldered, the battery can be plugged in to test that the board turns on. Once powered, it’s crucial to ensure that the board shows up in the device manager (check ports). If the board doesn’t show up, the drivers can be downloaded here.

Next, install the board for the Arduino IDE using the board manager:

  • Download and install the Arduino IDE (at least v1.8)
  • Start the Arduino IDE
  • Go into Preferences
  • Add https://www.adafruit.com/package_adafruit_index.json as an 'Additional Board Manager URL'
  • Open the Boards Manager option from the Tools -> Board menu and install 'Adafruit nRF52 by Adafruit' (see image below)

If bootloader issues arise, they may need an update; follow this.

After finishing the hardware setup, we can move onto the software. From here, you can download the sample I used from Peripherals -> Controller.

It’s important to note that this file is incomplete — a few lines of code must be added for the Neopixel to respond to the commands. This requires the user to download the Neopixel libraries through the Arduino IDE library manager.

Once the controller.ino is compiling, download the Bluefruit Connect app, connect to your device, and go to the color picker option.

Working with the Adafruit Feather nRF52

This project was a straightforward introduction to the capabilities of the nRF52 that requires little background knowledge. The most challenging part was setting up the board in the Arduino IDE, as I ran into some issues with updating the bootloader but was able to troubleshoot.

If you’re familiar with soldering and the Arduino IDE, you can quickly breeze through this introduction and kickstart some unique projects. Stay tuned for my next article, in which I’ll examine a more practical approach to using the nRF52.

Code

MAIN

Copy Code
/*********************************************************************
This is an example for our nRF52 based Bluefruit LE modules

Pick one up today in the adafruit shop!

Adafruit invests time and resources providing this open source code,
please support Adafruit and open-source hardware by purchasing
products from Adafruit!

MIT license, check LICENSE for more information
All text above, and the splash screen below must be included in
any redistribution
*********************************************************************/

#include <bluefruit.h>
#include <Adafruit_NeoPixel.h>

// OTA DFU service
BLEDfu bledfu;

// Uart over BLE service
BLEUart bleuart;

// Function prototypes for packetparser.cpp
uint8_t readPacket (BLEUart *ble_uart, uint16_t timeout);
float parsefloat (uint8_t *buffer);
void printHex (const uint8_t * data, const uint32_t numBytes);

// Packet buffer
extern uint8_t packetbuffer[];


Adafruit_NeoPixel pixel = Adafruit_NeoPixel(16, 5);

void setup(void)
{
Serial.begin(115200);
while ( !Serial ) delay(10); // for nrf52840 with native usb

// turn off neopixel
pixel.begin(); // This initializes the NeoPixel library.
for(uint8_t i=0; i<NUMPIXELS; i++) {
pixel.setPixelColor(i, pixel.Color(0,0,0)); // off
}
pixel.show();

Serial.println(F("Adafruit Bluefruit52 Controller App Example"));
Serial.println(F("-------------------------------------------"));

Bluefruit.begin();
Bluefruit.setTxPower(4); // Check bluefruit.h for supported values
Bluefruit.setName("Bluefruit52");

// To be consistent OTA DFU should be added first if it exists
bledfu.begin();

// Configure and start the BLE Uart service
bleuart.begin();

// Set up and start advertising
startAdv();

Serial.println(F("Please use Adafruit Bluefruit LE app to connect in Controller mode"));
Serial.println(F("Then activate/use the sensors, color picker, game controller, etc!"));
Serial.println();
}

void startAdv(void)
{
// Advertising packet
Bluefruit.Advertising.addFlags(BLE_GAP_ADV_FLAGS_LE_ONLY_GENERAL_DISC_MODE);
Bluefruit.Advertising.addTxPower();

// Include the BLE UART (AKA 'NUS') 128-bit UUID
Bluefruit.Advertising.addService(bleuart);

// Secondary Scan Response packet (optional)
// Since there is no room for 'Name' in Advertising packet
Bluefruit.ScanResponse.addName();

/* Start Advertising
* - Enable auto advertising if disconnected
* - Interval: fast mode = 20 ms, slow mode = 152.5 ms
* - Timeout for fast mode is 30 seconds
* - Start(timeout) with timeout = 0 will advertise forever (until connected)
*
* For recommended advertising interval
* https://developer.apple.com/library/content/qa/qa1931/_index.html
*/
Bluefruit.Advertising.restartOnDisconnect(true);
Bluefruit.Advertising.setInterval(32, 244); // in unit of 0.625 ms
Bluefruit.Advertising.setFastTimeout(30); // number of seconds in fast mode
Bluefruit.Advertising.start(0); // 0 = Don't stop advertising after n seconds
}

/**************************************************************************/
/*!
@brief Constantly poll for new command or response data
*/
/**************************************************************************/
void loop(void)
{
// Wait for new data to arrive
uint8_t len = readPacket(&bleuart, 500);
if (len == 0) return;

// Got a packet!
// printHex(packetbuffer, len);

// Color
if (packetbuffer[1] == 'C') {
uint8_t red = packetbuffer[2];
uint8_t green = packetbuffer[3];
uint8_t blue = packetbuffer[4];
Serial.print ("RGB #");
if (red < 0x10) Serial.print("0");
Serial.print(red, HEX);
if (green < 0x10) Serial.print("0");
Serial.print(green, HEX);
if (blue < 0x10) Serial.print("0");
Serial.println(blue, HEX);
for(uint8_t i=0; i<16; i++) {
pixel.setPixelColor(i, pixel.Color(red,green,blue));
}
pixel.show(); // This sends the updated pixel color to the hardware.
}

// Buttons
if (packetbuffer[1] == 'B') {
uint8_t buttnum = packetbuffer[2] - '0';
boolean pressed = packetbuffer[3] - '0';
Serial.print ("Button "); Serial.print(buttnum);
if (pressed) {
Serial.println(" pressed");
} else {
Serial.println(" released");
}
}

// GPS Location
if (packetbuffer[1] == 'L') {
float lat, lon, alt;
lat = parsefloat(packetbuffer+2);
lon = parsefloat(packetbuffer+6);
alt = parsefloat(packetbuffer+10);
Serial.print("GPS Location\t");
Serial.print("Lat: "); Serial.print(lat, 4); // 4 digits of precision!
Serial.print('\t');
Serial.print("Lon: "); Serial.print(lon, 4); // 4 digits of precision!
Serial.print('\t');
Serial.print(alt, 4); Serial.println(" meters");
}

// Accelerometer
if (packetbuffer[1] == 'A') {
float x, y, z;
x = parsefloat(packetbuffer+2);
y = parsefloat(packetbuffer+6);
z = parsefloat(packetbuffer+10);
Serial.print("Accel\t");
Serial.print(x); Serial.print('\t');
Serial.print(y); Serial.print('\t');
Serial.print(z); Serial.println();
}

// Magnetometer
if (packetbuffer[1] == 'M') {
float x, y, z;
x = parsefloat(packetbuffer+2);
y = parsefloat(packetbuffer+6);
z = parsefloat(packetbuffer+10);
Serial.print("Mag\t");
Serial.print(x); Serial.print('\t');
Serial.print(y); Serial.print('\t');
Serial.print(z); Serial.println();
}

// Gyroscope
if (packetbuffer[1] == 'G') {
float x, y, z;
x = parsefloat(packetbuffer+2);
y = parsefloat(packetbuffer+6);
z = parsefloat(packetbuffer+10);
Serial.print("Gyro\t");
Serial.print(x); Serial.print('\t');
Serial.print(y); Serial.print('\t');
Serial.print(z); Serial.println();
}

// Quaternions
if (packetbuffer[1] == 'Q') {
float x, y, z, w;
x = parsefloat(packetbuffer+2);
y = parsefloat(packetbuffer+6);
z = parsefloat(packetbuffer+10);
w = parsefloat(packetbuffer+14);
Serial.print("Quat\t");
Serial.print(x); Serial.print('\t');
Serial.print(y); Serial.print('\t');
Serial.print(z); Serial.print('\t');
Serial.print(w); Serial.println();
}
}

// PACKETPARSER.CPP

Copy Code
#include <string.h>
#include <Arduino.h>
#include <bluefruit.h>


#define PACKET_ACC_LEN (15)
#define PACKET_GYRO_LEN (15)
#define PACKET_MAG_LEN (15)
#define PACKET_QUAT_LEN (19)
#define PACKET_BUTTON_LEN (5)
#define PACKET_COLOR_LEN (6)
#define PACKET_LOCATION_LEN (15)

// READ_BUFSIZE Size of the read buffer for incoming packets
#define READ_BUFSIZE (20)


/* Buffer to hold incoming characters */
uint8_t packetbuffer[READ_BUFSIZE+1];

/**************************************************************************/
/*!
@brief Casts the four bytes at the specified address to a float
*/
/**************************************************************************/
float parsefloat(uint8_t *buffer)
{
float f;
memcpy(&f, buffer, 4);
return f;
}

/**************************************************************************/
/*!
@brief Prints a hexadecimal value in plain characters
@param data Pointer to the byte data
@param numBytes Data length in bytes
*/
/**************************************************************************/
void printHex(const uint8_t * data, const uint32_t numBytes)
{
uint32_t szPos;
for (szPos=0; szPos < numBytes; szPos++)
{
Serial.print(F("0x"));
// Append leading 0 for small values
if (data[szPos] <= 0xF)
{
Serial.print(F("0"));
Serial.print(data[szPos] & 0xf, HEX);
}
else
{
Serial.print(data[szPos] & 0xff, HEX);
}
// Add a trailing space if appropriate
if ((numBytes > 1) && (szPos != numBytes - 1))
{
Serial.print(F(" "));
}
}
Serial.println();
}

/**************************************************************************/
/*!
@brief Waits for incoming data and parses it
*/
/**************************************************************************/
uint8_t readPacket(BLEUart *ble_uart, uint16_t timeout)
{
uint16_t origtimeout = timeout, replyidx = 0;

memset(packetbuffer, 0, READ_BUFSIZE);

while (timeout--) {
if (replyidx >= 20) break;
if ((packetbuffer[1] == 'A') && (replyidx == PACKET_ACC_LEN))
break;
if ((packetbuffer[1] == 'G') && (replyidx == PACKET_GYRO_LEN))
break;
if ((packetbuffer[1] == 'M') && (replyidx == PACKET_MAG_LEN))
break;
if ((packetbuffer[1] == 'Q') && (replyidx == PACKET_QUAT_LEN))
break;
if ((packetbuffer[1] == 'B') && (replyidx == PACKET_BUTTON_LEN))
break;
if ((packetbuffer[1] == 'C') && (replyidx == PACKET_COLOR_LEN))
break;
if ((packetbuffer[1] == 'L') && (replyidx == PACKET_LOCATION_LEN))
break;

while (ble_uart->available()) {
char c = ble_uart->read();
if (c == '!') {
replyidx = 0;
}
packetbuffer[replyidx] = c;
replyidx++;
timeout = origtimeout;
}

if (timeout == 0) break;
delay(1);
}

packetbuffer[replyidx] = 0; // null term

if (!replyidx) // no data or timeout
return 0;
if (packetbuffer[0] != '!') // doesn't start with '!' packet beginning
return 0;

// check checksum!
uint8_t xsum = 0;
uint8_t checksum = packetbuffer[replyidx-1];

for (uint8_t i=0; i<replyidx-1; i++) {
xsum += packetbuffer[i];
}
xsum = ~xsum;

// Throw an error message if the checksum's don't match
if (xsum != checksum)
{
Serial.print("Checksum mismatch in packet : ");
printHex(packetbuffer, replyidx+1);
return 0;
}

// checksum passed!
return replyidx;
}

 

Mfr Part # 1463
ADDRESS LED RING SERIAL RGB
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.