Maker.io main logo

Arduino Flame Detector with Alarms and Automatic Fire Extinguish

1,277

2025-04-22 | By Mirko Pavleski

License: General Public License Relays Arduino

A flame detector is an electronic device designed to sense the presence of flames or fire. There are several types of flame detectors, including ultraviolet, infrared, multispectrum detectors, and optical flame detectors. In the device described in this project, we will use an infrared type of flame detector, which is widespread, inexpensive, and has satisfactory characteristics.

bkihj

As the name itself tells us, this detector module consists of an infrared receiving LED, which is connected to an operational amplifier that processes the detected signal. Infrared LED has the ability to detect a light source in the infrared part of the spectrum. In the case of a flame, most of the spectrum that is emitted is in the infrared region.

In addition to the infrared sensor, we also use a microcontroller, which, when detecting a flame from the sensor, activates other processes, in this case a light and sound alarm, as well as a pump immersed in a water tank which at that moment begins to extinguish the flame to prevent its spread. Actually, I made this device together with one of my students, and it is a high school graduation project.

hbk

The device is very simple to make and consists of only a few components.

- Arduino Uno microcontroller board,

- Infrared Flame detector module,

- Water pump with hoses

- 5V Relay module

- 2 LEDs with appropriate current limiting resistors, 470 Ohms.

- Buzzer

- and Battery (in my case 2 lithium cells in series with a total of 7.4V and 1 cell for the water pump)

Let's first analyze the hardware part. For the Flame detector, I use a standard IR sensor module with transmitter and receiver LEDs, where we need to unsolder and remove the transparent transmitter LED.

dfg

The main part of the water pump is an electric motor, which requires a current of more than 100mA to operate. On the other hand, the Arduino outputs can only handle a current of up to 40mA. For this reason, the water pump is connected via an electromagnetic relay module, which consumes about 20mA. The pump also uses a separate power source because the motor brushes often reset the microcontroller because they were previously connected to the same source. LEDs are, by definition, current consumers, so they are connected to the Arduino outputs through current-limiting resistors with a value of 470 ohms, so according to Ohm's law, a current of about 5mA will flow through them. The buzzer is a component that connects directly to the Arduino and is controlled by pulse width modulation (PWM).

As for the Arduino code, it is extremely simple and therefore reliable, which should be a basic feature for this type of device.

sdgft

At the beginning, variables are defined and created, and then in void setup, the inputs and outputs are defined, as well as their starting values. Then, in the loop function, we use an if-else statement that allows us to make decisions depending on the value of a variable.

Now let's see how the device works in real conditions. First, I'll turn off the power to the water pump for practical reasons and test the rest of the device. First, we need to adjust the sensitivity of the IR detector using this small potentiometer. Now the sensor is adjusted, and we can connect the pump.

jklj

If a flame appears in front of the sensor, an audible and visual alarm will be activated, and the water pump will start drawing water from the tank to extinguish the fire.

And finally, a short conclusion. This Arduino project is very simple to make and has a huge practical application and represents an excellent demonstration of controlling external devices (in this case, a pump, siren, and light signal) depending on some occurring condition detected by an appropriate sensor. Just to mention again that we created this project together with my students as a final high school exam.

vbn

Copy Code
//Arduino Flame Detector

 int relayPin = 5;
 int buzzerPin = 2;
 int flamePin = 8;
 int TONE1 = 900;     // First tone frequency
 int TONE2 = 1200;    // Second tone frequency
 int DURATION = 500;  // Duration of each tone in milliseconds
 int blueled = 3;
 int redled = 4;
 int Flame = HIGH;

void setup() 
{
  Serial.begin(9600);
  pinMode(buzzerPin, OUTPUT);
  pinMode(relayPin, OUTPUT);
  pinMode(redled, OUTPUT);
  pinMode(blueled, OUTPUT);
  digitalWrite(redled, LOW);
  digitalWrite(blueled, LOW);
  digitalWrite(relayPin, LOW);
  pinMode(flamePin, INPUT);
  
}

void loop() 
{
  Flame = digitalRead(flamePin);
  if (Flame == LOW)
  {
     digitalWrite(buzzerPin, LOW);
     digitalWrite(redled, LOW);
     digitalWrite(blueled, LOW);
     digitalWrite(relayPin, LOW);
     noTone(buzzerPin);
  }
    
  else
  {
    digitalWrite(relayPin, HIGH);
    tone(buzzerPin, TONE1);
    digitalWrite(redled, HIGH);
    digitalWrite(blueled, LOW);
    delay(DURATION);
    tone(buzzerPin, TONE2);
    digitalWrite(redled, LOW);
    digitalWrite(blueled, HIGH);
    delay(DURATION);
  }
}
Mfr Part # A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
Mfr Part # ST0253
FLAME SENSOR MODULE
SunFounder
Mfr Part # 4546
SUBMERSIBLE 3VDC HORIZONTAL PUMP
Adafruit Industries LLC
Mfr Part # DFR0017
GRAVITY DIGITAL 5A RELAY MODULE
DFRobot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.