Maker.io main logo

Bluetooth Low Energy (BLE) Tutorial for Beaglebone

82

2021-11-29 | By Sheikh Shuhad

License: General Public License BeagleBone

1. Introduction

This is a simple example showcasing how to control a BleuIO dongle connected to a Beaglebone Black using a python script.

When running the script, it will first ask for the com port where the dongle is connected (usually ‘/dev/ttyACM0’). After that, the BleuIO will start advertising. Every 8th second it will turn on one of the onboard Beaglebone Black LEDs whilst changing the BLE advertising name to indicate which LED is on.

We are using the Linux Debian image: ‘OMAP3/DM3730 Debian 9.5 2018-10-07 4GB SD LXQT’ (https://beagleboard.org/latest-images).

 Beaglebone Bluetooth low energy

2. About the Code

You can get access to the project HERE

https://github.com/smart-sensor-devices-ab/beaglebone_bleuio_example

We are using the Adafruit_BBIO python library that comes with the Beaglebone to control the onboard LEDs. First, we define the LED names and then set them as GPIO Outputs. Then we define the advertising messages that the BleuIO will switch between. Let's break one down:

“10:09:42:6C:65:75:49:4F:20:4C:45:44:20:30:20:4F:4E:”

“10” is the size of the advertising packet in HEX.

“09” is the flag for device name (Complete Local Name).

“42:6C:65:75:49:4F:20:4C:45:44:20:30:20:4F:4E” is the packet itself, translated from HEX to ASCII it says: “BleuIO LED 0 ON”

Afterwards the user is presented with a message to input the com port which the BleuIO is connected to. If you are not using a USB Hub the port should be ‘/dev/ttyACM0’.

You can change the comport name in the Python script and fill in your COM port.

Copy Code
com_input = "/dev/ttyACM0"

The script continues into the main loop, where it will first make sure all LEDs are off and then start BLE advertising.

The loop iterates through all four LEDs. In every iteration it turns one LED on and advertise the LED name then continue to the next LED. This will continue until the script is aborted.

Copy Code
import serial
import time
import Adafruit_BBIO.GPIO as GPIO


LED_USR0 = "USR0"
LED_USR1 = "USR1"
LED_USR2 = "USR2"
LED_USR3 = "USR3"

GPIO.setup(LED_USR0, GPIO.OUT)
GPIO.setup(LED_USR1, GPIO.OUT)
GPIO.setup(LED_USR2, GPIO.OUT)
GPIO.setup(LED_USR3, GPIO.OUT)

LED0_ON_ADV_MSG = "10:09:42:6C:65:75:49:4F:20:4C:45:44:20:30:20:4F:4E:"
LED1_ON_ADV_MSG = "10:09:42:6C:65:75:49:4F:20:4C:45:44:20:31:20:4F:4E:"
LED2_ON_ADV_MSG = "10:09:42:6C:65:75:49:4F:20:4C:45:44:20:32:20:4F:4E:"
LED3_ON_ADV_MSG = "10:09:42:6C:65:75:49:4F:20:4C:45:44:20:33:20:4F:4E:"

# Turn off all LEDs
GPIO.output(LED_USR0, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR1, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR2, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR3, GPIO.LOW)
time.sleep(0.1)

print("\nBlueIO BeagleBone Example!\n\n")
connecting_to_dongle = 0
com_input = ""

start_input = 0
valid_input = 0
while start_input == 0:
com_input = input(
"Enter Com port of Dongle (default for BeagleBone: '/dev/ttyACM0'):\n>>"
)
print("\nComport to use: " + com_input)
input_continue = input(
"If your happy with your choice just press Enter to continue the script. Else type E to exit or R to redo your choice. \n>>"
)
if input_continue.upper() == "E":
start_input = 1
elif input_continue.upper() == "":
start_input = 1
elif input_continue.upper() == "R":
valid_input = 0
start_input = 0
if input_continue.upper() == "E":
print("Exiting script...")
exit()

console = None

while 1:
try:
print("Please wait...")
time.sleep(0.5)
console.write(str.encode("AT+DUAL"))
console.write("\r".encode())
time.sleep(0.5)
print("Starting Advertising...")
console.write(str.encode("AT+ADVSTART"))
console.write("\r".encode())
time.sleep(0.5)
led_turn = 0
# Turn off all LEDs
GPIO.output(LED_USR0, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR1, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR2, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR3, GPIO.LOW)
time.sleep(0.1)
while True:
if led_turn == 0:
print("\nTurning LED USR0 ON")
console.write(str.encode("AT+ADVRESP="))
console.write(LED0_ON_ADV_MSG.encode())
console.write("\r".encode())
GPIO.output(LED_USR0, GPIO.HIGH)
GPIO.output(LED_USR1, GPIO.LOW)
GPIO.output(LED_USR2, GPIO.LOW)
GPIO.output(LED_USR3, GPIO.LOW)
led_turn = led_turn + 1
elif led_turn == 1:
print("\nTurning LED USR1 ON")
console.write(str.encode("AT+ADVRESP="))
console.write(LED1_ON_ADV_MSG.encode())
console.write("\r".encode())
GPIO.output(LED_USR0, GPIO.LOW)
GPIO.output(LED_USR1, GPIO.HIGH)
GPIO.output(LED_USR2, GPIO.LOW)
GPIO.output(LED_USR3, GPIO.LOW)
led_turn = led_turn + 1
elif led_turn == 2:
print("\nTurning LED USR2 ON")
console.write(str.encode("AT+ADVRESP="))
console.write(LED2_ON_ADV_MSG.encode())
console.write("\r".encode())
GPIO.output(LED_USR0, GPIO.LOW)
GPIO.output(LED_USR1, GPIO.LOW)
GPIO.output(LED_USR2, GPIO.HIGH)
GPIO.output(LED_USR3, GPIO.LOW)
led_turn = led_turn + 1
elif led_turn == 3:
print("\nTurning LED USR3 ON")
console.write(str.encode("AT+ADVRESP="))
console.write(LED3_ON_ADV_MSG.encode())
console.write("\r".encode())
GPIO.output(LED_USR0, GPIO.LOW)
GPIO.output(LED_USR1, GPIO.LOW)
GPIO.output(LED_USR2, GPIO.LOW)
GPIO.output(LED_USR3, GPIO.HIGH)
led_turn = 0

time.sleep(8)

except KeyboardInterrupt:
GPIO.output(LED_USR0, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR1, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR2, GPIO.LOW)
time.sleep(0.1)
GPIO.output(LED_USR3, GPIO.LOW)
time.sleep(0.1)
print("Exiting script...")
exit()
except:
print("\n\nDongle not connected.\n")
connecting_to_dongle = 0
while connecting_to_dongle == 0:
try:
print("Trying to connect to dongle...")
console = serial.Serial(
port=com_input,
baudrate=57600,
parity="N",
stopbits=1,
bytesize=8,
timeout=0,
)
if console.is_open.__bool__():
connecting_to_dongle = 1
print("\n\nConnected to Dongle in port: " + com_input + ".\n")
except:
print(
"Dongle not found. Retrying connection to port: "
+ com_input
+ "..."
)
time.sleep(5)

3. Using the example project3.1 What you will need

4. How to setup project

4.1 Downloading the project from GitHub

Get access to the project HERE

https://github.com/smart-sensor-devices-ab/beaglebone_bleuio_example

Either clone the project or download it as a zip file and unzip it, into a folder on your BeagleBone.

You can also create a new python file using the Cloud9 IDE from the BeagleBone (run by going to http://192.168.7.2:3000/).

Beaglebone Bluetooth low energy project

Copy the code and paste it into the newly created file.

Beaglebone Bluetooth low energy application

4.2 Installing pyserial

To run the script, you will need to install the python library pyserial.

The easiest way of doing this is just connecting to the BeagleBone via shh (the default password is temppwd):

Beaglebone Bluetooth low energy project

or using the bash tab in the Cloud9 IDE and type:

Copy Code
sudo pip3 install pyserial

5. Running the example

Go to the folder where you have the python script file and run:(Pyserial needs sudo-privileges to function.)

Copy Code
sudo python3 name_of_script.py
Mfr Part # SSD005/4-V2W
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
Mfr Part # SSD005/4-V2B
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
Mfr Part # BBB01-SC-505
BEAGLEBONE BLACK AM3358 REV C
GHI Electronics, LLC
$121.48
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.