Maker.io main logo

Build a Bristlebot of Your Own

280

2025-01-24 | By Sara McCaslin

License: Attribution Adhesive Batteries Misc Hand Tools Vibration / Haptic

Bristlebots are fun, exciting, and a great introduction to STEM. In this article, you will learn how ‎bristlebots work—and how to build your very own. We discuss the tools and equipment you’ll ‎need, then look at how a bristlebot works from an electrical perspective. From there, we move ‎on to assembling your bristlebot, troubleshooting it, and experiments you can perform with it.‎

Fig1

Complete bristlebot with decorations.‎

What You’ll Need

Here’s a list of the basic supplies needed to build a bristlebot similar to that shown above:‎

Fig2

Basic supplies for making a bristlebot.‎

How a Bristlebot Works

The motion of a bristlebot is based on electricity and solid dynamics but is easy to understand. ‎The bristlebot uses a tiny electric motor (the same type of motor that makes video game ‎controllers and cell phones vibrate) to move, and it is powered by a coin cell battery. ‎

For an electrical circuit to work, it must be complete with no breaks in where the electricity, or ‎the current, needs to flow. You complete an electrical circuit when you connect the battery to the ‎motor. In this case, current flows from the battery through the red wire to the motor, making the ‎motor turn. After it passes through the motor, the current flows back to the battery through the ‎black wire. ‎

Now let’s talk about positive and negative. The negative side of the coin battery is the top, while ‎the positive side is the completely flat bottom. The red wire, or positive wire, connects to the ‎positive side of the battery. The negative side, or black wire, connects the negative part of the ‎battery to the ground wire on the motor.‎

The completed circuit makes a tiny weight inside the motor spin. This spinning weight is just off-‎balance enough to make the motor vibrate and buzz. The vibration and buzzing of the motor are ‎directly transferred to the toothbrush head, which will begin to move the bristles if it is on a flat ‎surface, making the robot move around.‎

Fig3

An assembled bristlebot.‎

Assembling Your Bristlebot

Here are the basic instructions for assembling the bristlebot.‎

  • Peel the adhesive backing from the motor OR use foam tape to attach the motor to the ‎toothbrush. Remember to leave enough room for the battery.‎

  • Peel the backing from one side of the foam tape. Stick that side of the foam tape to the ‎flat surface of the toothbrush. ‎

  • Peel the backing off the other side of the foam tape. Place the red (positive) wire so that ‎the metal part of the wire will be at the center bottom of the battery. Attach the battery to ‎the foam tape so that its bottom surface is stuck to the tape and will touch the bottom of ‎the battery.‎

  • Touch the blue or black (negative) wire to the top of the battery—the bristlebot should ‎now be vibrating.‎

  • Customize your bristlebot (see below).‎

Fig4

An example of adding very basic decorations to your Bristlebot.‎

Experiments to Perform

There are so many interesting experiments to perform with your bristlebot, so here are a few ‎ideas to help you learn even more about electricity:‎

  • Which works better: the motor at the front or the back?‎

  • What changes can I make to make the bristlebot more stable?‎

  • What types of motors or batteries let the bristlebot move the fastest?‎

  • What type of toothbrush bristles work best (e.g., slanted, straight)?‎

  • What shape of toothbrush head works the best?‎

  • Create an obstacle course with books, cardboard, erasers, etc., and other objects to see ‎how long it takes the bristlebot to move around them.‎

  • What type of surface (carpet, tile, etc.) does the Bristlebot move the best on?‎

  • Build bristlebots with friends and see which is the fastest. Can you figure out why?‎

Troubleshooting Your Bristlebot

There are some common issues that builders run into with bristlebots, so here is a short ‎troubleshooting guide.‎

How do I turn off my bristlebot?‎

It’s very simple: remove the top wire from the battery. ‎

How long will my robot’s batteries last?‎

They can last up to two hours, but it is important to disconnect the battery when you are not ‎using the bristlebot. ‎

How do I help my bristlebot to move straight?‎

This is an extremely common design challenge. Here are different ways to try:‎

  • Position the battery and motor symmetrically to prevent veering to one side or the ‎other.‎

  • Adjust bristles for a straight direction.‎

  • Experiment with stiffer bristles and shorter lengths for stability.‎

  • Attach a lightweight tail for stability (see image below).‎

  • Use a guiding track of books or cardboard (or something similar) if other methods ‎don't work.‎

Each bristlebot may require a bit of tweaking, so experiment with these techniques to find the ‎best setup for yours!‎

Fig5

Adding a tail can help stabilize a bristlebot, and this is just one example.‎

My bristlebot falls over!‎

This is another common challenge for bristlebot designers. Here is a list of potential solutions to ‎try:‎

  • Consider slightly angling the bristles outward; this can give the bot more lateral ‎stability, like the legs on a tripod.‎

  • Use a small piece of foam or a rubber band to cushion the motor, which can help ‎absorb some vibrations and make the movement smoother.‎

  • Attach a tail (twist-tie, paperclip, or small plastic straw, etc.).‎

  • Let the bristlebot lie on its side and vibrate for 5 to 10 minutes to slow the motor ‎down.‎

  • Use a lower-power battery or less powerful motor.‎

The motor no longer vibrates

If your motor stops vibrating, first make sure that the correct wire is touching the battery. Check ‎for broken wires (these wires are quite fragile and can break close to the base). Finally, the ‎battery could be drained.‎

The motor seems weak

The battery is most likely running out of power and will need to be replaced soon.‎

Conclusion

Building a bristlebot is fun, assembling it is easy, and designing it to perform the way you want is ‎definitely a design challenge.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.