Maker.io main logo

Build Your Own All-Sky Camera with a Raspberry Pi

936

2025-02-07 | By Sara McCaslin

License: See Original Project Raspberry Pi SBC

All Sky cameras take pictures of the sky during the day or at night to capture a complete view of ‎the sky to reveal the motion of stars, auroras, meteor showers, satellite movements, and more. ‎When the correct type of camera is used, a 180° view of the sky is possible. This information ‎can be used by amateur and professional astronomers alike and can serve as a fascinating ‎introduction to astronomy.‎

Copy of Figure 01

All sky image showing a meteor, by Michael L. Umbricht / Ladd Observatory. Source: Wikimedia.‎

You can learn how to build your own Raspberry Pi All Sky camera with readily available ‎components and software. This article goes over the parts, setup, enclosure, and testing.‎

How Can I Make My Own Using Raspberry Pi?‎

Below is a basic list of the equipment and software you will need to create a basic All Sky ‎camera:‎

Hardware

Basic hardware that you will need for the circuitry:‎

Software

Only two types of software are needed: the Raspberry Pi OS and the All Sky camera software, ‎AllSky.‎

Enclosure

The basics of the enclosure are composed of:‎

Note that the enclosure must also be of sufficient size for the clear dome to rest upon it and over ‎the camera.‎

Setup the Raspberry Pi

Flash Raspberry Pi OS onto the microSD card using Raspberry Pi Imager. You will choose your ‎device, operating system, and the type of storage you are using.‎

Copy-of-Figure02

Basic setup used for this project.‎

You will see the option customization screen appear. Select Edit Settings and go to the Options ‎tab. Make sure the only checked box is Play Sound when finished. ‎

Copy-of-Figure03a

Copy-of-Figure03b

Customization settings.‎

If your computer has problems when the verification step starts, restart the installer, and click ‎CANCEL when verification starts.‎

Once the SD card is ready, place it in the Raspberry Pi. Plug the adapter into the wall and boot ‎the Raspberry Pi. Note you will need a keyboard and a screen to work with the RP, so get those ‎connected and connect your camera before starting. Once the operating system loads and the ‎GUI is displayed on the screen, download any needed updates.‎

Installing the AllSky Software

Next, install AllSky software. Start by going here https://github.com/AllskyTeam/allsky and ‎reading the documentation here. Once you have reviewed the basic documentation, go to the ‎command line and type: ‎

Copy Code
sudo apt-get install git

After that process has finished, enter this at the command line.‎

Copy Code
cd
git clone --recursive https://github.com/AllskyTeam/allsky.git
cd allsky
./install.sh

This will start the AllSky installer. You must have your camera installed before the installation. ‎Follow the prompts on the screen. Notice that you will need to enter the latitude and longitude of ‎where you are located. This can be obtained via a quick Google search. After this, you will be ‎prompted to reboot your system. There will be a message that says you need to update your ‎camera settings using ‘AllSky Settings’ in the WebUI. You may also need to update config.sh ‎and ftp-settings.sh

After the reboot, go to the WebUI by going to “http://allsky.local” or “http://allsky.localhost” in a ‎web browser using the Raspberry Pi. The default username is “admin” and the default password ‎is “secret”.‎

From there, go to AllSky settings.‎

Setting Up AllSky

To schedule the software to start automatically on boot, go to the command line bash and enter ‎this code:‎

Copy Code
sudo crontab -e
@reboot /home/pi/allsky/allsky.sh

You can monitor performance by accessing the camera remotely via SSH or VNC. ‎

There are many different settings that can be adjusted to obtain excellent image quality. A ‎sample of these are shown below. These include exposure, brightness control, white balance, ‎shutter speed, and some additional features that may be AllSky software specific.‎

Copy-of-Figure04

The settings screen for AllSky. ‎

Exposure Settings

Here are the most common exposure settings and what they mean:‎

  • Manual Exposure: supports better control over how much light the camera gathers. This ‎is especially useful for obtaining images of faint objects such as stars.‎

  • Automatic Exposure: automatically adjusts the exposure based on the camera’s ‎environment, which accounts for changes during the day or night. There are also limits ‎you can set on automatic exposure to keep it from over-adjusting.‎

  • Exposure Time: this can be set in terms of seconds of exposure. Just be aware that the ‎longer the exposure, the greater the possibility of moving objects being blurred. ‎

Brightness Control

Brightness control is another key parameter in obtaining clear, high-quality images of the sky. ‎

  • Gain: adjusts how much the camera signal is amplified. High gain = more sensitive to ‎light but introduces more noise.‎

  • Gamma Correction: adjusts the brightness and contrast of the image. To make dark ‎areas of the image brighter without overexposing the lighter parts.‎

  • Brightness Adjustments: fine-tunes the brightness of the final image for well-balanced ‎light and dark images.‎

White Balance

White balance works to ensure colors are accurately rendered. This can be set manually or ‎automatically and is especially important to account for a sky with a color cast.‎

Day/Night Profiles

AllSky supports the creation of separate profiles for day and night using the settings just ‎discussed. Night images, for example, may require a longer exposure if you want to capture the ‎path of meteors or stars, whereas a shorter exposure is best for daytime. ‎

Shutter Speed (for HQ Camera Modules)‎

If you have a Raspberry Pi HQ Camera, additional control may be possible over the shutter ‎speed. Shutter speed relates to how fast the camera captures the image. ‎

Software-Specific Adjustments for AllSky

AllSky software makes it possible to adjust settings for how often an image of the sky is taken ‎and can adjust the exposure as needed. It also provides noise reduction, which can be crucial to ‎obtaining a quality image of the sky.‎

Building the Enclosure

The standard enclosure for a Raspberry Pi is approximately 3.5x2.25x1 in, and it is ‎recommended that this enclosure be used along with the waterproof enclosure. It can be ‎attached to the waterproof enclosure with hook and loop tape, making it easy to remove the ‎Raspberry Pi as needed.‎

Copy-of-Figure05

The Raspberry Pi enclosure with the camera included. ‎

To assemble the enclosure, mount the camera inside the clear dome or waterproof housing. You ‎will need a slit for the camera ribbon to pass through to the Raspberry Pi board. Keep in mind ‎that the slit for the enclosure will be to the side of the camera. Ensure the dome is clean and free ‎of scratches for clear images, and add desiccant packs inside the enclosure to prevent fogging. ‎Next, seal the housing to protect against moisture and dirt. Do not forget that the housing must ‎also be stable to ensure no movement in the photos.‎

Copy-of-Figure06

Camera dome.‎

Testing the System ‎

The camera should be positioned where a clear view of the sky can be obtained. Once the ‎enclosure has been placed and stabilized, test the camera. This can be done through AllSky's ‎web GUI. Next, you can obtain a live view through your camera in the AllSky web GUI, and ‎from there start making adjustments to key parameters that will improve image quality. If there is ‎a message about the RPi command not being found, simply unplug the camera, turn off the ‎Raspberry Pi, then plug the camera back in and restart it.‎

Finding Your Images

The photo below shows the path to the images, which are placed in files labeled by date. These ‎images can easily be copied to a flash drive or shared file system such as Google Drive, ‎OneDrive, or Dropbox. If desired, they can also be shared with the AllSky project.‎

Copy-of-Figure07

The path for locating the images.‎

Is There Anything Else I Can Use an All Sky Camera For?‎

All Sky cameras are a great way to monitor the movement of clouds, observe the effects of light ‎pollution on the night sky, and capture rare celestial events. It can also be used as a wildlife ‎camera or to create artistic imagery that includes elements of the sky.‎

Conclusion

Capturing incredible images of the sky and nightscape is easy to do without many parts needed. ‎With a Raspberry Pi, a good-quality USB or RPi camera, and the right software, you can begin ‎adding amazing sky photos to your photo albums.‎

Mfr Part # SC0073
SBC 1.4GHZ 4 CORE 1GB RAM
Raspberry Pi
Mfr Part # SC0445
AC/DC WALL MNT ADAPTER 5.1V 15W
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.