Maker.io main logo

Getting Started with Plasma 2040

187

2022-03-18 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

If you've not played with addressable LED strips yet, you've been missing out. ‎Customisable lighting effects in any or all colours of the rainbow, purchasable ‎by the metre, easily installable around your desk, inside your gaming PC or ‎just draped fabulously around your person. Figuring out what kind to buy, how ‎to power them and how to wire them up can be a little intimidating for ‎beginners though, which is where Plasma 2040 comes in!‎

About Plasma 2040‎

Plasma 2040 is an LED strip driver board that uses the shiny new RP2040 ‎chip from Raspberry Pi. We've designed it to be compact, easy to use, and ‎straightforward to power. Like all our RP2040 boards, you can use it with C++, ‎MicroPython, or CircuitPython - we'll be using our custom build of ‎MicroPython in this tutorial. If you'd rather use CircuitPython that's really easy ‎too - scroll down to the bottom of the tutorial for a quick primer on how to get ‎things started.‎

In this tutorial, we'll discuss how to connect different kinds of LEDs up to ‎Plasma 2040 and then we'll walk you through building and programming a set ‎of fairy lights which you can hang over your desk and signal green (available) ‎and red (busy) at the push of a button.‎

What You'll Need

  • A Plasma 2040
  • A USB-C cable
  • Some addressable LEDs! We'll be using RGB LED wire in this tutorial as ‎it comes with connectors, you get 5m in a packet and it looks really ‎pretty. We stock quite a few kinds though, if you'd rather use ‎something different the next section will tell you what you'll need to do ‎to connect them up
  • A computer to program Plasma 2040 from (the software you'll need, ‎Thonny, is free and available for Raspberry Pi, PC, Mac, or Linux)
  • Small flathead screwdriver for wrangling the screw terminals

Connecting Up Different Kinds of LED Strips

We stock flexible LED strips in RGB and RGBW varieties, and in WS2812 ‎‎(three wire) and APA102 (four wire) flavours. The flexible LED strips come ‎with a silicone sleeve over the top, to help protect the LEDs from dust and ‎moisture. We also stock some more exotic types of addressable LEDs, like ‎ones with a built-in diffuser. They'll all work with Plasma 2040, though some ‎are more straightforward to connect up than others.‎

Most of our LEDs come in 1m lengths with connectors on both ends, so ‎they're really easy to chain together and plug into Plasma 2040. These are ‎the strips we sell that come with connectors pre-attached:‎

  • Ultra-dense RGB Micro LED Strip
  • Neon-like RGB LED Strip with Diffuser
  • ‎5m Flexible RGB LED Wire

‎and the 144 pixel per meter variants of:

  • Flexible RGB LED Strip (NeoPixel/WS2812/SK6812 compatible)
  • Flexible RGBW LED Strip (NeoPixel/WS2812/SK6812 compatible)‎
  • Flexible RGB LED Strip (DotStar/APA102/SK9822 compatible)‎

The connector below is the one that needs attaching to Plasma 2040.‎

connector_1

If you take a look at the business end of Plasma 2040, you'll notice it has ‎screw terminals for plugging in your LEDs. This means you need to convert ‎that plug into bare wires somehow!‎

end_2

A neat way of doing this is with a 3 wire or 4 wire LED strip output cable. We ‎like these cables as they make a nice solid connection and you can easily ‎plug and unplug the LEDs if you need to, without having to unfasten the ‎screw terminals. If you're using LED wire, it comes with an output cable, you ‎don't need to buy one separately.‎

cable_3

cable_4

Hooking up the 30 and 60 LEDs per metre flavours of RGB and RGBW ‎Flexible LED Strip is slightly more complicated. If you buy 5m of strip it will ‎come on a reel with nice connectors at both ends. If you buy less than 5m, ‎our post ninjas will slice up one of these reels, so you could end up with just a ‎start connector, just an end connector (which can't be connected to the ‎Plasma), or no connectors at all!‎

You can solder wires on to the pads at the end of the strip and plug those ‎into Plasma 2040 or, if you'd prefer to avoid soldering, you could use one of ‎these clippy connectors instead (3 wire or 4 wire).‎

wire_5

When working with LED strips (especially if you're attaching your own ‎connector), you'll need to make sure to connect your controller to the correct ‎end - if you look at the strip closely there'll be some arrows on the strip to ‎show you in which direction the data should flow (so the arrows should point ‎away from your microcontroller).‎

From here on in, we'll be showing you the specific steps we took to get our ‎LED wire going - they should be similar for most WS2812/Neopixel LEDs. You ‎can find the parameters you'll need for different types of LEDs (like four wire ‎APA102 LEDs) in the Plasma documentation on Github.‎

Plugging in the LEDs

If you're using LED wire like us, unfurl it. It can get a bit squished in transit so ‎it's best to spread it out a bit and make sure none of the wires are kinked. ‎The wires are coated in plastic so they don't short against each other, but it's ‎possible there might be tiny breaks in the plastic if they've been really folded ‎up. Nothing bad will happen if the wires end up making contact with each ‎other, but you might notice some unpleasing flickering or glitching.‎

In the packet with the LED wire, you should have a loose connector with bare ‎wires on one end. We'll be using this to connect the plug on the LED wire to ‎the screw terminals on Plasma 2040.‎

plug_6

These LEDs are WS2812 addressable LEDs, so they have three wires - 5V, ‎data, and ground. With more traditional LED strips, you can tell which wire is ‎which (and what end the controller needs connecting to) from the markings ‎on the strip, but with this LED wire the 5v line is the one that's marked in red ‎on the connector, the data line is the one in the middle, and the ground line is ‎the one that's left over.‎

Loosen the screws on the connector on Plasma 2040 with a flathead ‎screwdriver, poke the wire ends into the connector, and tighten the screws ‎back up. You'll probably find it easier to do one wire at a time. Give the wires ‎a little tug when you're done to make sure they're anchored solidly in the ‎connector. Be sure that the terminal is gripping the metal wire, and not the ‎plastic sleeve (you can strip off a little bit of the plastic sleeve to expose ‎more of the wire if that helps).‎

terminal_7

Once that's in place then the fiddly bit is done, you can go ahead and plug in ‎your LEDs and your USB-C cable.‎

fiddly_8

Installing Our Custom MicroPython Build

If you're brand new to Raspberry Pi Pico/RP2040s, you might find the step by ‎step instructions in our Getting Started with Raspberry Pi Pico tutorial useful ‎‎- it will show you how to install our custom MicroPython build and goes into ‎more detail about how to use Thonny . Here's a quick TLDR!‎

  • Download the most recent MicroPython .uf2 from the Releases page of ‎our pimoroni-pico Github repository (either version, with Blinka or ‎without, will work)
  • Hold down the BOOT button of Plasma 2040, and then press, and ‎release, the RESET button. This will put it into bootloader mode, and it ‎should appear as a drive on your computer called RPI-RP2
  • Copy the .uf2 file to the RPI-RP2 drive - once you've done that Plasma ‎‎2040 will reboot running Pirate brand MicroPython (it won't show up as ‎a drive anymore)
  • Install Thonny
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'. If ‎everything's working as it should look something like this. The flashing ‎cursor next to the >>> in the 'Shell' box tells you that Plasma 2040 is ‎talking to your computer and is ready to accept instructions!‎

thonny_9

Lighting Up the Onboard RGB LED

As a test that the board is working properly and you have the correct version ‎of MicroPython installed, you can light up the onboard RGB LED red with the ‎following code - you can enter it line by line in the REPL (that's the bottom ‎‎'Shell' box in Thonny) or copy and paste the whole thing into the top box and ‎hit the green run button to save the code to your Plasma 2040. If you choose ‎to save it, you'll be prompted for a filename.‎

Copy Code
from plasma import plasma2040
from pimoroni import RGBLED

led = RGBLED(plasma2040.LED_R, plasma2040.LED_G, plasma2040.LED_B)

led.set_rgb(255, 0, 0)

The three numbers after set_rgb are an RGB (Red Green Blue) colour code, and ‎each number should be between 0-255.‎

Lighting Up the LED Strip

LIGHTING UP ONE LED

Lighting up the LED strip is pretty similar to lighting up the onboard LED. ‎Here's how to light up the first LED of your strip red (you can change the 50 to ‎however many LEDs you have in your strip).‎

Copy Code
import plasma
from plasma import plasma2040

NUM_LEDS = 50

led_strip = plasma.WS2812(NUM_LEDS, 0, 0, plasma2040.DAT)

led_strip.start()
led_strip.set_rgb(0, 255, 0, 0)

The first number in the set_rgb command is which LED you're giving an ‎instruction to - LED 0 is the first LED in our strip. The following three numbers ‎are the RGB colour code, as before. If you'd rather control your LEDs by ‎specifying a HSV (Hue Saturation Value) colour code, you can do that with ‎the set_hsv function (we'll be sticking to RGB in this tutorial though).‎

HALP, IT'S NOT RED!‎

If the first LED is lighting up green or blue, that probably means that your LED ‎strip has a different colour order to the default (GRB). You can fix this by ‎changing the led_strip = line to specify a different colour order, like this:‎

Copy Code
led_strip = plasma.WS2812(
NUM_LEDS, 0, 0, plasma2040.DAT, rgbw=False, color_order=plasma.COLOR_ORDER_RGB
)

HALP, I HAVE RGBW LEDS!‎

If your LEDs are in (surprise) disco mode or if fewer of them are lighting up ‎than expected, you may have RGBW LEDs. Peer closely at the LED strip - if ‎one half of each LED is yellow, then they have an extra white element, lucky ‎you. Try initialising your led_strip object like this:‎

Copy Code
led_strip = plasma.WS2812(NUM_LEDS, 0, 0, plasma2040.DAT, rgbw=True)

LIGHTING UP ALL THE LEDS

Okay, we can do better than one LED. How about lighting up all the LEDs red? ‎We can do this for adding a for i in range statement, which repeats ‎the set_rgb instruction to light up every LED between 0 and 49.‎

Copy Code
import plasma
from plasma import plasma2040

NUM_LEDS = 50

led_strip = plasma.WS2812(NUM_LEDS, 0, 0, plasma2040.DAT)

led_strip.start()

for i in range(NUM_LEDS):
led_strip.set_rgb(i, 255, 0, 0)

HALP, IT'S TOO RED!‎

Setting the red channel of the RGB strip to 255 means that the red element ‎of the LEDs is set to maximum red. If you want to tone the brightness down ‎a bit, or if being on full all the time is making your LEDs a little bit toasty, ‎change this to a smaller number. Setting it to 127 instead will reduce the ‎brightness to (about) half.‎

RAINBOW INTERLUDE

At this point, you've probably had enough of red LEDs. If you haven't checked ‎out our examples yet and fancy a palette cleanser, now might be a good time ‎to try out some adjustable speed rainbows (you can just copy and paste the ‎example into the top box in Thonny, and press the green run button). This ‎rainbow example also shows you how you can make use of the nifty current ‎sensing circuitry on Plasma 2040.‎

MAKING A BUSY LIGHT

Back to it! To use our newfound powers to make a busy light, all we need to ‎do add a bit more code so we can use the buttons to switch between modes. ‎The Button helper functions in our shared pimoroni module make this nice and ‎straightforward.‎

Copy Code
import plasma
from plasma import plasma2040
from pimoroni import RGBLED, Button

NUM_LEDS = 50

led = RGBLED(plasma2040.LED_R, plasma2040.LED_G, plasma2040.LED_B)
led.set_rgb(0, 0, 0)

button_a = Button(plasma2040.BUTTON_A)
button_b = Button(plasma2040.BUTTON_B)
button_boot = Button(plasma2040.USER_SW)

led_strip = plasma.WS2812(NUM_LEDS, 0, 0, plasma2040.DAT)

led_strip.start()

while True:
if button_a.read():
for i in range(NUM_LEDS):
led_strip.set_rgb(i, 255, 0, 0)
led.set_rgb(255, 0, 0)
if button_b.read():
for i in range(NUM_LEDS):
led_strip.set_rgb(i, 0, 255, 0)
led.set_rgb(0, 255, 0)
if button_boot.read():
for i in range(NUM_LEDS):
led_strip.set_rgb(i, 0, 0, 0)
led.set_rgb(0, 0, 0)

We've also brought back the RGBLED function we used earlier, to change the ‎colour of the onboard LED to match the colour of the LED strip. Now when ‎you press A the LEDs should light up red, when you press B they'll light up ‎green, and when you press the boot button they'll turn off. Now all you need ‎to do is hang up your LEDs (or install them in a suitable vessel...)‎

light_10

‎... and your busy light is complete! If you want your program to run whenever ‎your project is powered up, save it to Plasma 2040 as main.py. If you do this ‎you don't need to have your busy light plugged into a computer running ‎Thonny, you can power it from any old USB port. You could power your ‎Plasma 2040 from a USB power bank to make your busy light portable, or ‎even wearable (how about a Big Bad Hat of Just Say No?)‎

CircuitPython

Want to use CircuitPython on your Plasma 2040 instead of MicroPython? No ‎problem! To install CircuitPython -‎

  • download the Plasma 2040 CircuitPython .uf2 here . You'll also need ‎the CircuitPython driver bundle (be sure to grab the one that matches ‎the version of CircuitPython that you just downloaded)‎
  • Hold down the BOOT button of Plasma 2040, and then press, and ‎release, the RESET button. This will put it into bootloader mode, and it ‎should appear as a drive on your computer called RPI-RP2
  • Copy the CircuitPython .uf2 to the RPI-RP2 drive. After a few seconds, it ‎should reappear as a drive called CIRCUITPY
  • Unzip the driver bundle that you downloaded earlier. You'll ‎need neopixel.mpy (if you have WS2812 LEDs) or adafruit_dotstar.mpy (if you ‎have APA102 LEDs), as well as adafruit_bus device and simpleio.mpy - you can ‎find them all in the lib folder. Copy them across to the lib folder on the ‎CIRCUITPY drive
  • With CircuitPython, you always save your code as code.py, and it will run ‎automatically. You don't need to use Thonny, you can edit code.py with ‎any text editor.‎

Here's a version of our busy light code for CircuitPython!‎

Copy Code
import board
import digitalio
import adafruit_rgbled
import busio
import neopixel

NUM_LEDS = 50

BRIGHTNESS = 1

led_strip = neopixel.NeoPixel(board.DATA, NUM_LEDS, brightness=BRIGHTNESS, auto_write=True)

button_boot = digitalio.DigitalInOut(board.USER_SW)
button_boot.direction = digitalio.Direction.INPUT
button_boot.pull = digitalio.Pull.UP

button_a = digitalio.DigitalInOut(board.SW_A)
button_a.direction = digitalio.Direction.INPUT
button_a.pull = digitalio.Pull.UP

button_b = digitalio.DigitalInOut(board.SW_B)
button_b.direction = digitalio.Direction.INPUT
button_b.pull = digitalio.Pull.UP

led = adafruit_rgbled.RGBLED(board.LED_R, board.LED_G, board.LED_B, invert_pwm = True)

def button_read(button):
return not button.value

while True:
if button_read(button_a):
led_strip.fill((255, 0, 0))
led.color = (255, 0, 0)
if button_read(button_b):
led_strip.fill((0, 255, 0))
led.color = (0, 255, 0)
if button_read(button_boot):
led_strip.fill((0, 0, 0))
led.color = (0, 0, 0)

There's also neopixel and dotstar examples in the examples folder of the ‎CircuitPython driver bundle you can play with, to get them to work with ‎Plasma 2040 you'll just need to point them at the correct pins -‎

For WS2812 LEDs:‎

Copy Code
pixel_pin = board.DATA

or

For APA102 LEDs:‎

Copy Code
dots = dotstar.DotStar(board.CLK, board.DATA, 30, brightness=0.2)‎

Next Steps

Now that you know how to make LED strips light up, you could experiment ‎with switching between LEDs and colours to make custom patterns and ‎effects, or you could add a sensor breakout and make the lights ‎automatically do stuff based on temperature or light level - check out ‎our MicroPython examples for some ideas!‎

That's all folks!‎

Mfr Part # PIM582
PLASMA 2040
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.