Maker.io main logo

Kitronik Bluetooth Control App - How to Guide

67

2023-07-06 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide by Kitronik Maker

At Kitronik we have recently released a Google Play Store app called Kitronik ‎Bluetooth Control. This Android app allows you to control a Kitronik :MOVE mini ‎buggy over Bluetooth. In this blog we will learn how to code and setup your ‎micro:bit to be controlled using the app, how to connect to your micro:bit using the ‎Bluetooth on your phone, and how to use the control app.‎‎ ‎

The new Kitronik Bluetooth Control app replaces our previous Android app. We ‎suggest that you switch to this new app for a better and more consistent ‎experience.‎

Code your micro:bit

Let’s get started by coding our micro:bit to control it from the Kitronik Bluetooth ‎Control app. The full code can be found below using the embedded MakeCode ‎project, or at the end of this blog. To code your micro:bit you need to open the ‎project in MakeCode, connect your micro:bit to the MakeCode project using a USB ‎cable, and click the Download button.‎‎

code_1

Microsoft MakeCode | Terms of Use | Privacy | Download

Now let’s take a look at how the code for the :MOVE mini buggy works. The ‎micro:bit starts out by displaying a b* symbol on its LEDs to show that it is waiting ‎for a Bluetooth connection. When the micro:bit has received a Bluetooth connection ‎it will then set two variables to zero and show a smiley face symbol on its LEDs. ‎When the Bluetooth is disconnected, the micro:bit will display a sad face symbol on ‎its LEDs.‎

works_2

The code then contains a forever loop which will continue to repeat for the entire ‎time the micro:bit is turned on. Inside the forever loop the micro:bit will check and ‎modify two variables called changeServo1 and servo1Value. These variables are ‎used to control the :MOVE mini attachment connected to the buggy. ‎The changeServo1 variable is used to tell the micro:bit which direction to move the ‎servo’s value, either increasing or decreasing. The servo1Value then stores the ‎current value of this servo. When changeServo1 is set to 1, ‎the servo1Value variable is increased by 1 each time the forever loop repeats. ‎When changeServo1 is set to -1, the servo1Value variable is decreased by 1 each ‎time the forever loop repeats. Then when changeServo1 is set to 0, ‎the servo1Value variable is not changed. At the end of the forever loop ‎the servo1Value variable is written to pin 0 to set the buggy servo attachment to ‎that position.‎

position_3

The final part of the code is an event handler. The code inside the event handler is ‎used to react to the Bluetooth messages sent to the micro:bit from the Kitronik ‎Bluetooth Control app. When the micro:bit receives a Bluetooth message this code ‎will check to see if the event value matches one, we have setup. When the event ‎value does match with one of in the if statements we have setup, then the code ‎inside that block will be run. The four of the first eight event values in our event ‎handler are used to move the buggy forward, backward, left, and right when a ‎button on the app is pressed down. The other four of these eight are used to stop ‎the buggy from move when a button on the app is released. The last four event ‎values are used to control the buggy servo attachment by changing the value ‎stored in the changeServo1 variable.‎

Connect to your micro:bit using Bluetooth

To connect to your micro:bit using Bluetooth we are going to need to put the ‎micro:bit in Bluetooth pairing mode. We can do this in two different ways. First you ‎can do this by pressing and holding the A B buttons and then turning on the ‎micro:bit. Second you can do this by pressing and holding the A B buttons while ‎the micro:bit is already turned on, and then pressing the reset button on the back of ‎the micro:bit. In either case we need to hold the A B buttons down until the ‎Bluetooth symbol is displayed on the micro:bit’s LEDs.‎

Once in Bluetooth pairing mode, go to the Bluetooth settings on your Android phone. ‎With Bluetooth turned on, selected to pair a new device. Your phone will begin to ‎search for Bluetooth devices nearby and should show you a BBC micro:bit in the ‎list of available devices. When you can see your BBC micro:bit in the Bluetooth ‎devices list, click on it and follow the instructions to connect to your micro:bit. ‎When this is successful your micro:bit will display a tick symbol on its LEDs.‎

Using the Kitronik Bluetooth Control App

With the Kitronik Bluetooth Control app downloaded from the Google Play Store we ‎can now start using the app to control the :MOVE mini buggy. Let’s start by ‎opening the app and allowing it access to the Location and Nearby devices ‎permissions.‎

With this done and the micro:bit connected over Bluetooth; we can now see the ‎micro:bit in the paired devices list on the app. From here you can click on your ‎paired micro:bit from the list and the app will connect to it. Once connected you will ‎see a smiley face displayed on your micro:bit’s LEDs.‎

connect_4

On the next screen of the app, you will see six arrows. The four arrows shaped like ‎a diamond in the middle of the screen are used to control the movement of the ‎Kitronik :MOVE mini buggy. These are to move the buggy forwards and backwards, ‎then to spin the buggy left and right. The two bold arrows on the right side of the ‎screen are used to control the third attachment servo that can be connected to ‎the :MOVE mini. These allow you to control any attachments you have connected ‎to your buggy.‎

control_5

Full Code

Copy Code
let servo1Value = 0
let changeServo1 = 0
basic.showLeds(`
# . . # #
# . . # #
# # # . .
# . # . .
# # # . .
`)
basic.forever(function () {
if (changeServo1 != 0) {
servo1Value = changeServo1
if (servo1Value < 0) {
servo1Value = 0
}
if (servo1Value > 180) {
servo1Value = 180
}
pins.servoWritePin(AnalogPin.P0, servo1Value)
}
})
bluetooth.onBluetoothConnected(function () {
changeServo1 = 0
servo1Value = 0
basic.showLeds(`
# # . # #
# # . # #
. . # . .
# . . . #
. # # # .
`)
})
bluetooth.onBluetoothDisconnected(function () {
basic.showLeds(`
# # . # #
# # . # #
. . # . .
. # # # .
# . . . #
`)
})
control.onEvent(EventBusSource.MES_DPAD_CONTROLLER_ID, EventBusValue.MICROBIT_EVT_ANY, function () {
if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_1_DOWN) {
pins.servoWritePin(AnalogPin.P1, 0)
pins.servoWritePin(AnalogPin.P2, 180)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_1_UP) {
pins.servoWritePin(AnalogPin.P1, 90)
pins.servoWritePin(AnalogPin.P2, 90)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_2_DOWN) {
pins.servoWritePin(AnalogPin.P1, 180)
pins.servoWritePin(AnalogPin.P2, 0)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_2_UP) {
pins.servoWritePin(AnalogPin.P1, 90)
pins.servoWritePin(AnalogPin.P2, 90)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_3_DOWN) {
pins.servoWritePin(AnalogPin.P1, 0)
pins.servoWritePin(AnalogPin.P2, 0)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_3_UP) {
pins.servoWritePin(AnalogPin.P1, 90)
pins.servoWritePin(AnalogPin.P2, 90)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_4_DOWN) {
pins.servoWritePin(AnalogPin.P1, 180)
pins.servoWritePin(AnalogPin.P2, 180)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_4_UP) {
pins.servoWritePin(AnalogPin.P1, 90)
pins.servoWritePin(AnalogPin.P2, 90)
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_A_DOWN) {
changeServo1 = -1
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_A_UP) {
changeServo1 = 0
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_B_DOWN) {
changeServo1 = 1
} else if (control.eventValue() == EventBusValue.MES_DPAD_BUTTON_B_UP) {
changeServo1 = 0
}
})

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.

Mfr Part # 5652
MOVE:MINI MK2
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.