Maker.io main logo

Kitronik Spooky Halloween Project Ideas

53

2022-10-27 | By Kitronik Maker

License: See Original Project 3D Printing Switches

Courtesy of Kitronik

Guide by Kitronik Maker

With Halloween creeping up on us, we’ve made some spooky resources to give your decorations a techy twist! It’s a great time of year to test out some ideas and to dust off your making skills.

spider_1

This year we have a theme, movement! Firstly, we have a moving prop, and we also have a device that detects movement to scare those that venture too close! We've also thrown in the odd making tip along the way, for good measure!

Halloween 2018 Project Ideas:

To mix it up even further, we chose to highlight two different manufacturing techniques, 3D Printing and Laser Cutting. At the same time, both of these projects can be handmade. For example, the spider project could be made with craft foam or Papier-mâché, and the SpookO’Matic can be hand tooled from Perspex, Plywood, or MDF. Let's get making!

Halloween 2018 - 3D Printed Surprise Spider:

3d_2

This 3D printing project would look great in a window or hidden by a doorway. When activated, the servo turns a winch, suddenly lowering the spider onto your unsuspecting victim!

We Used:

You Will Also Need:

  • 3D Printer
  • Glue (superglue, hot glue or poly cement will work)
  • Sticky Pads or double-sided tape
  • Thread
  • Our design files

design_3

When 3D printing the spider, use support material and a brim in order to avoid the legs coming loose from the print bed. The winch drum shouldn’t need any support material when printed on its side.

glue_4

We glued the winch drum to a servo horn then pressed onto the servo. For this, we used superglue although hot glue would work fine as well. As soon as the glue is dry, the spider is attached by the black thread tied and wound around the drum.

drum_5

The microbit and servo are held onto the battery cage with double sided sticky pads. Tip: The spider descends slightly faster than it ascends. Because of this, adjust your microbit code so that it always comes back to the same height. A guide on driving a servo using the BBC micro:bit can be found here.

Halloween 2018 - The Spook O'Matic:

matic_6

This build is a great example of how different project kits can be combined to make a custom control circuit. It uses our light activated switch kit to sense the shadow of someone moving past, and also our record playback kit to scare them with a spooky noise! We decided to laser cut a Perspex case for it, however, you can also design your own from our range of materials.

We Used:

You Will Also Need:

files_7

The DXF of this design is free to download below. Set the text to a very light engrave setting, since frosted black Perspex engraves to a vivid white very easily.

download_8

We used jumper cables and pin headers to test the interface circuit, but you can solder directly into the PCB holes.

Both kits were assembled as standard except for a few components. The LEDs of both kits, as well as the phototransistor of the light activated switch, were soldered with a length of wire to let them poke through the casing. The battery connections for both boards were soldered to the same 2xAA battery pack. Finally, the two interface wires were added. Solder one wire from the positive output of the light activated board to the “3V” hole of the playback kit, then solder the negative output to the “Ply” hole.

kits_9

Before screwing on the front of the case, the potentiometer on the light activated switch needed adjusting. This will change the amount of light needed to activate the switch, so adjust it for the lighting conditions where you want to use it.

case_10

The LEDs and phototransistor poke through the front of the case which is held on with M3 screws. All that’s left now is to record a sound into it, we used the classic evil laugh from Thriller! As an additional challenge, see if you can use the light activated switch output to trigger the 3D printed spider as well. This should make both builds motion activated, and into a spooktacular double surprise!

Bonus Tip:

The webs in the background were cut from our polyethylene foam sheets. It’s a really easy material to work with using scissors, craft knives, or even a laser cutter.

Other Spooky Links:

If our Halloween 2018 project ideas have got you in the making mood, why not check out or Halloween 2016 and 2017 project ideas.

©Kitronik Ltd – You may print this page & link to it, but must not copy the page or part thereof without Kitronik's prior written consent.

Mfr Part # 2589
SERVOMOTOR RC 130 RPM 4.8-6V
Kitronik Ltd.
Mfr Part # 5669-20
KITRONIK INVENTORS KIT FOR MICRO
Kitronik Ltd.
Mfr Part # EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
Mfr Part # 2149
RECORD PLAYBACK KIT
Kitronik Ltd.
More Info
View More Details
Mfr Part # 2112
LIGHT ACTIVATED SWITCH
Kitronik Ltd.
Mfr Part # WP25D
SOLDERING IRON 25W 230V
Apex Tool Group
$115.10
View More Details
Mfr Part # T0051388799
WSW SAC L0 SN3,0AG0,5CU3,5%
Apex Tool Group
$112.47
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.