Maker.io main logo

Make a Phone Call Using the SIM900 GSM Shield & Arduino - Visuino Tutori

24

2026-04-01 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Wifi Arduino ESP32

In this tutorial, you will learn how to make a phone call using the SIM900 GSM Shield and Visuino.

With one button, you will be able to start a call and end the call with the second button.

 You will also learn how to use the "Serial Software" component in Visuino.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

  • SIM900 GSM Shield

  • SIM card (You should disable the PIN request on the SIM card before using it with the GSM shield)

  • Breadboard

  • 2X button

  • 2X 1kΩ resistor

  • 5V power supply with enough amps for the shield

  • Visuino program: Download Visuino

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

The Circuit

  • Connect the SIM900 GSM Shield to the Arduino

  • Connect Arduino pin [5V] to breadboard positive pin [Red line]

  • Connect Arduino pin [GND] to breadboard negative pin [Black line]

  • Connect Arduino digital pin [2] to button1 on the breadboard and to resistor1.

  • Connect the other side of the resistor 1 to the breadboard pin [GND]

  • Connect the other pin of button 1 to the breadboard positive pin [5V]

  • Connect Arduino digital pin [2] to button1 on the breadboard and to resistor1.

  • Connect the other side of the resistor 1 to the breadboard pin [GND]

  • Connect the other pin of button 1 to the breadboard positive pin [5V]

  • Connect with the Jumpers on the shield pins D8 (RX) & D7 (TX) as you see it in the picture

  • Make sure that the antenna is connected to the shield

  • Connect the 5V Power Supply to the shield, and set the switch on the shield to the External Power (See the picture)

  • Once the Power is connected, hold the Power button for 2 seconds

  • Once the connection with the Network is established, the LED will blink every 3 seconds

The Circuit

The Circuit photo 2

The Circuit photo 3

Start Visuino, and Select the Arduino UNO board type.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Software Serial Port" component

  • Add "Add "Text Value" component

  • Add 2X "Debounce Button" components.

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Set Components

  • Double-click on "TextValue1," and in the Elements window, drag "Set Value" to the left side, and in the properties window, set "Value" to ATDP+ PHONE_NUMBER (International Format) & add a semicolon at the end

Example: ATDP+38470987541;

  • In the Elements window, drag another "Set Value" to the left side, and in the properties window, set "Value" to ATH

Example: ATH

  • Close the Elements window

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Connect Components

  • Connect Arduino digital pin [2] to "Button1" pin [In]

  • Connect Arduino digital pin [3] to "Button2" pin [In]

  • Connect "Button1" pin [Out] to "TextValue1" > "Set Value1" pin [In]

  • Connect "Button2" pin [Out] to "TextValue1" > "Set Value2" pin [In]

  • Connect "TextValue1" pin [Out] to "SoftwareSerial1" pin [In]

  • Connect "SoftwareSerial1" pin [RX] to Arduino Digital pin [7]

  • Connect "SoftwareSerial1" pin [TX] to Arduino Digital pin [8]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

When you power the Shield, wait a bit for the connection with the network to be established. Once the connection is established, the LED on the Shield will blink every 3s.

Now you can press a button, and you will make a call. To end the call, just press the other button.

Congratulations! You have completed your GSM project with Visuino. Also attached is the Visuino project that I created for this. You can download and open it in Visuino: https://www.visuino.eu

Using the Serial Window to Send Commands

  • Add "Software Serial Port" component

  • Connect Arduino Serial pin [Out] to "SoftwareSerial1" pin [In]

  • Connect "SoftwareSerial1" pin [RX] to Arduino Digital pin [7]

  • Connect "SoftwareSerial1" pin [TX] to Arduino Digital pin [8]

  • Connect "SoftwareSerial1" pin [Out] to Arduino Serial pin [In]

Upload the project (see the step Generate, Compile, and Upload The Arduino Code), and in Visuino select the "Serial" tab, select the Port, and click the "Connect" button.

  • Once connected, you can start sending the commands to the module by typing, for example: AT;

  • This will ask the GSM Shield for the current status

Also attached is the Visuino project

Using the Serial Window to Send Commands

Troubleshooting

  • Supplying the SIM900 shield with enough power is very important; if it does not get enough power, it might turn off

  • AT command must have a semicolon at the end, or it might return the message "NO CARRIER"

  • Some mobile operators might block the GSM modules; in that case, contact your mobile operator and ask for more information.

Extra

  • You can connect the headphones and a microphone to the audio jack connectors on the shield.

  • Instead of the buttons, you could connect a sensor, for example, a PIR motion detection sensor, to trigger a phone call every time movement is detected. Check this tutorial for more information: https://www.instructables.com/How-to-Use-PIR-Sensor-and-a-Buzzer-Module-Visuino-/

  • Experiment with other AT commands:

  • Command ATA – Accepts the incoming call.

  • Command ATH – Hangs up the call.

  • Command AT+CMGF=1\r will set the SIM900 shield to text mode

  • Command AT+CMGS=PHONE-NUMBER (international format) will send SMS to a number

  • Command  AT+CMGR=1\r will read the first SMS from the inbox

  • Command AT+CMGR=2\r will read the second SMS from the inbox

  • Command AT+CMGR=ALL\r will read all SMS from the inbox

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.