Maker.io main logo

Moving Gear Bracelet

139

2022-04-28 | By Odd_Jayy (Jorvon Moss)

License: See Original Project Programmers

This project has been on my mind for months. I recently found a bracelet on Thingiverse that is made of gears, which I immediately printed and began wearing. It’s more of a fidget toy, something you can turn with your hands, but I thought, “Why not add a motor?”

So, I did, and the result has been amazing.

You can download the code and STL files here.

Step #1: Print the Bracelet

The bracelet is very easy to print. I printed it flat on the print bed with supports. For sizing, I recommend measuring your wrist and making the bracelet about 2 to 5 inches bigger than your wrist. For other humans like myself who have strange wrists, make it as big as you need to, just note you will need to fit the components, and the left-over room can be fixed with foam.

Print the Bracelet

Step #2: Clean the Bracelet

Once you print the bracelet it will have a lot of supports on it, and some of the supports will be in the gears making it impossible for them to move. To fix this problem, I recommend using a precision knife and carefully begin cutting the supports from the gears. To help with the process, I recommend, after removing the supports, slowly try rotating the gears, being careful not to damage anything.

Step #3: Test

After the gears are good and ready, make sure to twist the gear knob to loosen them up a bit. Just keep spinning it until it feels smooth.

Step #4: Dremel

So, this is where things get interesting. There is a visible hole in the knob gear, using a Dremel rotary tool and drill through the knob gear until it comes off. Try to make the hole in the bracelet a bit bigger since this is where the servo will go.

Dremel

Step #5: Circuit

The circuit is simple:

Circuit

I used the above circuit and simply omitted the LEDs and wired the servo directly to the microcontroller board. I also added a switch for on and off.

Step #6: Print Enclosure

Print Enclosure

The enclosure is shaped to fit with the bracelet, and you should be able to easily glue it to the inside.

Step #7: Assembly

Assembly

This is pretty much what you should have after following the guide thus far. Insert the controller and wires into the enclosure and glue them in place.

Assembly

Step #8: The Finish

Finally, place the power switch on the outside of the enclosure. If needed, glue some foam to the inside to help hold the bracelet on your wrist.

The Finish

 

Mfr Part # 2589
SERVOMOTOR RC 130 RPM 4.8-6V
Kitronik Ltd.
Mfr Part # 11026
JUMPER M/M 7" 30AWG 30PCS
SparkFun Electronics
Mfr Part # 1501
TRINKET 5V ATTINY85 EVAL BRD
Adafruit Industries LLC
Mfr Part # 17620
HOT GLUE GUN 25W WITH PLASTIC TR
Aven Tools
Mfr Part # XN100
KNIFE PRECISION WITH BLADE
Apex Tool Group
Mfr Part # ENDER-3 V2
32-Bit Mainboard 3D Printer
Creality 3D
$474.69
View More Details
Mfr Part # AO469
60 WATT SOLDERING STATION
SRA Soldering Products
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.