Maker.io main logo

Printing TPU/TPE on Your LulzBot

39

2024-02-22 | By Lulzbot

License: See Original Project 3D Printing

Courtesy of LulzBot

Guide by LulzBot

‎3D printed parts don’t have to just be made of hard plastic! The options for flexible 3D ‎printable materials have grown significantly over the years and open a whole new world ‎of creativity and design options. From creating wearable items like bracelets and watch ‎bands to manufacturing tools and jigs, you can give your prints some bend, elasticity, or ‎even bounce. There are many applications for these filaments, especially when paired ‎with your LulzBot machine.‎

LulzBot stocks many flexible filament colors and types that you can choose from that ‎pair perfectly with their printers. These rubbery materials behave much differently than ‎your typical PLA or ABS plastics, so I tested out four different varieties of flexible ‎filaments on my LulzBot Sidekick printer with a variety of designs, as well as the tools ‎you need to get started 3D printing these filaments.‎

Here’s what you need to know to get started making flexible prints on your LulzBot ‎machine. ‎ ‎

Getting started with the Basics

There are two main types of flexible 3D printing filaments: thermoplastic polyurethane ‎‎(TPU) and thermoplastic elastomers (TPE). Both are very similar materials that create a ‎flexible print. In general, TPE is a bit softer, which can make it a little more challenging to ‎print with. The outcome of TPE prints can be closer to a rubber. You can find both TPE ‎and TPU filaments offered by LulzBot here.‎

Also, keep an eye out for the shore hardness of the material. Shore hardness is a measure ‎of how much the material can resist being indented when pressure is applied. This helps ‎you determine how hard or flexible the items printed from the material will be. It is used ‎as a measure in many industries that use flexible rubber-like materials, not just 3D ‎printing. There is an “A” scale for softer materials, and a “D” scale for harder materials. ‎The higher the number, the harder the material. TPU and TPE filaments commonly have ‎shore hardness values in the 80As or 90As.‎

The shore hardness is often either listed in the product description or the name of the ‎filament itself. For example, the shore hardness of the Fenner Drives NinjaFlex 85A ‎Filament offered by LulzBot is 85A.‎‎ ‎

Getting the Equipment, you need

When I originally got my LulzBot 747 Sidekick, it came with a SK1.75mm Tool Head. ‎Although this smaller 1.75mm nozzle is possible to print flexible materials with, I highly ‎recommend getting an additional 2.85mm Tool Head if you don’t already have one for ‎printing flexibles. The larger size is helpful for creating a consistent flow of the material ‎and preventing clogging.‎

LulzBot machines make it very easy to swap out the Tool Heads. With just a few screws ‎removed and cords unplugged, you can swap in a new Tool Head to your LulzBot printer.‎

Also, double check that you have a direct drive Tool Head. All LulzBot printers currently ‎have direct drive, making any current LulzBot printer a great fit for your flexible 3D ‎printing projects. Direct drive Tool Heads don't need large retractions and can provide ‎better control over notoriously hard to control flexible materials.

‎Retracting is a process through which a print head pulls some filament back into the Tool ‎Head to prevent stringing during the printing process. Large retractions can cause issues ‎for flexible materials since they stretch when pulled, rather than immediately responding ‎to the machine's motion like more traditional plastics. The other common Tool Head type, ‎Bowden head, can work too, but might risk some additional stringing and require ‎additional work to dial in the print quality.

sidekick_1

Heated Glass Print Bed

I absolutely love my magnetic print bed on my LulzBot Sidekick 747. It makes print ‎removal a dream. But in the case of flexible filaments, a glass print surface is ‎recommended. LulzBot offers a reversible PEI/glass bed that is perfect for these projects. ‎TPU/TPE likes to stick to PEI a little too much. The swap out is simple and absolutely ‎worth it. ‎

On top of the glass, don’t forget to lay down some of your glue stick to ensure adhesion ‎of your print. In case you forget, within LulzBot’s slicer program, Cura LE, the default ‎print profiles for flexibles give you tips in there as well, reminding you to use glue.‎

bed_2

Device Settings

When in doubt, set up the LulzBot to avoid clogging and encourage the prints to stick to ‎the print bed. Flexible filaments love to try to clog your device, so using a larger nozzle, ‎appropriate heats, and removing the filament guide tube, when necessary, helps you ‎print TPU and TPE on your LulzBot printer.

‎LulzBot’s Cura platform has a number of settings built in for flexible filaments, including ‎NinjaTek’s NinjaFlex and JABIL’s SEBS filament. You will even see some notes pop up for ‎more effective printing giving suggestions to:‎

  1. Use a glue stick with PEI or print directly on glass for NinjaFlex and SEBS
  2. Not use the filament guide tube for SEBS

These preloaded material profiles are a fantastic starting point to do your first flexible ‎prints with, and then you can adjust as needed.‎‎ ‎

Materials

It’s time to dive into printing and testing. There are many filament options that LulzBot ‎offers, but we’ll focus on four types that LulzBot sent me to try out: NinjaFlex TPU ‎‎(green), Polymaker TPU (yellow), BASF TPU (natural), and JABIL TPE (black).‎

I printed a few models in each material to get a good comparison between them and ‎understand what it is like using them with LulzBot machines. The models I picked were ‎a LulzBot impression seal included as part of LulzBot's LulzLesson (3D printing lesson ‎plans that can be used in the classroom), a 20 sided die, and a collection of custom ‎space shaped bracelets that I designed. As someone who went to high school during ‎the Silly Bandz craze of the early 2010s, I couldn't resist making some of my own with ‎the bendable filament. These small prints gave a good reflection of the detail, elasticity, ‎and durability of the prints.

materials_3

NinjaFlex TPU

NinjaFlex is one of the original flexible 3D printing materials and provides some of the ‎best elasticity in a 3D print. This springiness was really impressive. The designs came out ‎super clean from the LulzBot Sidekick 747 printer using the default settings listed in the ‎Cura profile provided by LulzBot. It had very clean levels of detail with almost no ‎stringing.‎

While it wasn’t the full stretchiness of the original Silly Bandz, it was definitely the ‎closest of all the materials. I was also able to compress the 20-sided die more than the ‎dice made with the other filaments and it bounced back very well. Despite the elasticity, ‎it still felt durable. I think that was my personal favorite one to work with.

ninjaflex_4

Polymaker PolyFlex TPU

For the Polymaker PolyFlex TPU 95A filament I was able to use very similar settings to ‎NinjaFlex. TPU filaments tend to be similar in temperature and settings, but make sure to ‎check the packaging to be sure. The level of detail on this filament was also very high. ‎The spool it came on did create a higher tendency to get tangled when used without a ‎guide tube. So I recommend trying to use the PTFE guide tube, or watching the initial ‎layers longer than typical to make sure it is on the right track.‎

The 20-sided dice made of this material had the least give of all the designs. The thinner ‎designs were definitely bendable, but it definitely felt on the harder side. This is ‎evidenced also by the higher shore hardness number of 95 for this material. As one of the more affordable options for filament though, it still performed very well ‎and is one to consider for your project.

polymaker_5‎ ‎

Jabil TPE-SEBS

Jabil TPE-SEBS 1300 85A was the only TPE filament tested on the list, so I was very ‎interested to see how it compared to the TPU options. Although it did have a bit more ‎stringing, it still performed very well on the LulzBot printer. This one printed at a higher ‎heat for both the print bed and the filament. I used a temperature of 245 degrees C ‎which tended to give a pretty high print quality.‎

The end product was a bit silkier and more rubber like. There was a bit more of a ‎softness at its core that made it feel polished. This filament I got in the black color which ‎meant it was the only one that didn’t have any degree of transparency to the final ‎products.‎

Note you can also purchase this filament in a 3.5kg roll if you are looking for bulk for ‎larger projects. ‎ ‎

tpeseries_6

BASF Ultrafuse TPU

Last up was the BASF Ultrafuse TPU 85A. When you are looking for longer term ‎industrial use, this is a great option. While my print attempts with this one did have the ‎most stringing, I think it just needs a bit more effort dialing in the print.‎

The prints out of BASF did return perfectly to their original shape, even when bent or ‎indented pretty dramatically. It felt very durable. Ultrafuse has a number of unique ‎properties with resistance to hydrolysis, resistance to microbiological attack, high wear ‎resistance, and excellent damping behavior. Definitely check this out for parts that need ‎long term bounce back and flexibility like manufacturing tools and jigs.‎

Overall, all of the materials worked so much better on my LulzBot printer than I ‎expected. I thoroughly expect these to be a frequent part of my printing projects from ‎now on.‎

And there are plenty more flexible material options offered by LulzBot as well for you ‎to explore.‎

basf_7

Tips

Lastly, some general tips for purchasing and using all of these materials on your LulzBot ‎‎3D printer:

  • Flexible filaments are often sold in quantities of 0.75kg or 1kg. Be sure to check ‎the amount when you purchase to make sure you have enough for your project. ‎
  • To allow for more squish or bend, use a lower density of material inside of your ‎designs. For my 20-sided dice that I printed, I wanted them to have some bounce ‎when they rolled, so I used a 10% infill. The impression stamps had areas with ‎thin backing that also allowed for a bend. ‎
  • All of the filaments take some extra pressure to get them initially loaded into the ‎tool head. Since it bends and flexes while being loaded into the machine it takes ‎some careful guidance, and then a bit of force to get it to catch on the gears ‎inside the Tool Head. ‎ ‎
  • When loading the filament, be sure to check the temperature on the LulzBot ‎printer. Flexible filaments have differing temperature requirements that don’t ‎match the default ABS or PLA profiles on the printer. ‎ ‎
  • Some filaments work better when the tension is reduced. That might mean ‎unspooling and respooling some of the filament as it can tend to slightly stick to ‎itself on the spool, or removing the PTFE guide tube.‎

So, get out there and get printing! Having a few spools of flexible filament is always great ‎for opening up new ideas and allowing for unique creative projects. I’m definitely going ‎to experiment with more fashion applications of these filaments down the line, and I ‎can’t wait to see what you make on your LulzBot printer with them too.‎

tips_8

About Guest Author Erin Winick

Erin Winick has a B.S. in mechanical engineering with extensive experience working as a ‎STEM communicator. Previously working as a science communicator for the ‎International Space Station and reporter for MIT Technology Review. Erin devotedly ‎enjoys teaching others about STEM and has led many freelance and personal STEM ‎communication projects. In her free time, she pursues her passion of 3D printing while ‎designing science and engineering inspired projects and clothes.‎

erin_9

 

Mfr Part # RM-TE0004
FILAMENT WHITE TPU 0.118" 750G
LulzBot
$118.73
View More Details
Mfr Part # RM-TE0124
POLYMAKER POLYFLEX TPU95 FILAMEN
LulzBot
Mfr Part # KT-PR0058
NORTH AMERICA ONLY - LULZBOT TAZ
LulzBot
More Info
View More Details
Mfr Part # KT-HB0024
TAZ SIDEKICK 747 GLASS/PEI PRINT
LulzBot
$109.62
View More Details
Mfr Part # KT-HB0018
TAZ SIDEKICK 747 MAGNETIC FLEX B
LulzBot
$146.15
View More Details
Mfr Part # KT-MS0020
PTFE TUBE KIT- 2.85MM
LulzBot
Mfr Part # KT-HB0014
TAZ ETCHED MODULAR PRINT BED
LulzBot
More Info
View More Details
Mfr Part # KT-CP0162
LULZBOT TAZ DUAL EXTRUDER V3.1 T
LulzBot
$904.32
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.