Maker.io main logo

Tips and Tricks: Dual More With the Dual Extruder v3

19

2023-10-12 | By Lulzbot

License: See Original Project 3D Print Accessories 3D Printer 3D Printing

Courtesy of LulzBot

Guide by LulzBot

lulz_1

Submitted by Cathryn on Thu, 08/23/2018 - 21:56‎

Dual-Color/Material 3D Printing with the LulzBot TAZ Dual Extruder v3 Tool Head

‎The Dual Extruder v3 Tool Head is optimized for printing models with soluble support ‎material. However, advanced users have successfully printed dual-colored and multi-‎material models. There are only a few simple steps to follow!‎‎

‎Dual color or dual material 3D printing requires a model specifically designed for dual ‎extrusion, saved as two separate .STL files, one for each material or color. For the ‎purposes of this tutorial, we are using THIS MODEL.‎‎

  1. Load both STL files into Cura LE. At this point it doesn't matter if both models fit on ‎the bed plate.

load_2

2. Select the part of the model you wish to print with extruder 1 and choose Print ‎Selected Model with Extruder 1. Do the same for the second part of the model and ‎select Print Selected Model with Extruder 2.‎

select_3

3. Right click anywhere in the dark grey area of the Prepare screen to pull up the Options ‎menu and choose Select All Models. Right click again and choose Merge Models. The ‎two models will move together on the virtual print bed as they will be printed. Position ‎the combined model as desired on the print bed. (Selecting Center Selected Model will ‎place the model directly in the center of the print surface.)‎

right_4

right_5

right_6

Printing With Ooze Shield or Prime Tower Enabled

Sometimes, particularly with two colors that have a high degree of contrast, oozing ‎between the colors may occur. Enabling the Ooze Shield Setting in Cura LE can help ‎mitigate this. An ooze shield is a thin, removable shield that prints around your model, ‎minimizing color bleeding. Enabling the Prime Tower also helps reduce oozing and ‎adding a brim to the prime tower aids in bed adhesion. ‎

ooze_7

Important Tips: ‎

When selecting materials for your dual-colored print, be mindful of the ‎temperature settings for both the heat bed and the nozzle. Materials with similar ‎temperature settings adhere better to one another than materials with drastically ‎different settings. ‎

LulzBot Mini Users: Want to join the ranks of Dual Extruder v3 Users? Get ‎a LulzBot TAZ 6 or a Factory Refurbished LulzBot TAZ 6! ‎

Suggested Material Combinations:‎‎ ‎

  • ABS and NinjaFlex

  • bronzeFill and copperFill

  • bambooFilland woodFill

  • ABS and HIPS

  • PLA and PLA (any same-material combination)

  • Conductive PLA and bronzeFill‎

dual4_8

Share your successful prints and additional tips and tricks on our forum!‎

‎3D Model Attribution‎

‎“Two color Rocktopus” by Dp90pusika used under the Creative Commons - Attribution - ‎Share Alike license.‎

Related Products

LulzBot TAZ Dual Extruder v3.1 Tool Head | 0.5 mm
2.85mm PolyLite PLA Polymaker
LulzBot TAZ 6

Mfr Part # KT-PR0051NA
TAZ WORKHORSE EDITION NORTH AMER
LulzBot
More Info
View More Details
Mfr Part # KT-CP0162
LULZBOT TAZ DUAL EXTRUDER V3.1 T
LulzBot
$904.32
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.