Maker.io main logo

Wireless RC Robot with Arduino and XBees

76

2019-03-26 | By SparkFun Electronics

License: See Original Project Programmers Wireless Arduino XBee

Courtesy of SparkFun

Introduction

In this tutorial, we will expand on the SIK for RedBot to control a robot wirelessly with XBee radios! We'll explore a different microcontroller and wirelessly control the RedBot at a distance. Beware, we'll need to solder the wireless controller together.

wireless rc robot

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Wireless RC Robot with Arduino and XBees Wish List SparkFun Wish List

Heads up! This tutorial uses the RedBot mainboard programmed with Arduino and shadow chassis. Depending on your setup, you can choose different motor drivers for your motor and chassis.

  • Wild Thumper 6WD Chassis - Black (34:1 gear ratio)

  • Circular Robotics Chassis Kit (Three-Layer)

  • Actobotics Kit - ActoBitty 2

  • Multi-Chassis - Tank Version

Tools

You will need a soldering iron, solder, and general soldering accessories. If you have not soldered before, we suggest looking at the tool kits. You will also need a wire stripper and some wire depending on the XBees that you are using.

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

Hardware Hookup

Assembled Shadow Chassis

We'll assume that you have a fully assembled robot with the Shadow Chassis.

2_Shadow-Chassis-Guide

Assembly Guide for RedBot with Shadow Chassis

Assembly Guide for the RedBot Kit. This tutorial includes extra parts to follow to go along with the RedBot Inventor's Kit tutorial.

Motor and Power Switches

Make sure to flip the MOTOR and POWER switches to the RUN and ON positions respectively.

3_Motor-and-Power-Switches

Motor Wires

To be consistent with the hookup used with the assembly and experiment guide, make sure that the motor wires match the table and image below.

Left Motor:

4_Table1

Right Motor:

5_Table3

 6_Motor-Wires

Software Serial Switch

To avoid bricking the XBee on the RedBot or uploading, it is recommended to utilize the software serial port. Make sure to flip the switch to the "XBEE SW SERIAL" side.

7_flip-the-switch

Assembled Wireless Joystick

We'll also assume that you have a wireless joystick assembled together. Check out the Hardware Hookup section in the Wireless Joystick Hookup Guide for more information. Note that you will need to solder the components together as opposed to the solderless RedBot Kit.

8_Wireless-hookup-guide

Wireless Joystick Hookup Guide

A hookup guide for the SparkFun Wireless Joystick Kit.

The example code used in this tutorial works for both the dual joystick and single joystick.

9_dual-joystick-and-single-joystick

Jumper Wire for XBee 3's

The following code works with a XBee Series 1 set to transparent mode. If you are using an XBee Series 3, you may need to add a jumper between the XBee Series 3's reset pin and A5 for the Wireless Joystick. Simply cut and strip a piece of wire to add between reset pin on the XBee's female socket and A5.

10_solder-to-pin

Solder Pin for XBee Series 3

Once the wire is soldered, it should look similar to the image below.

11_Jumper-wire

Jumper wire between A5 and RESET pin on the XBee Series 3

Configuring XBees

To configure the XBees, we will be using the XBee Series 1 firmware. It is recommended to configure each XBee using the XBee Explorer USB.

12_Configuring-XBees

If you have not already, check out the Starting with XCTU section under Exploring XBees and XCTU to configure your XBees.

13_Exploring-XBees

Exploring XBees and XCTU

How to set up an XBee using your computer, the X-CTU software, and an XBee Explorer interface board.

Point-to-Point Configuration

For simplicity, we will be sending commands with the XBees in transparent mode set for a point-to-point configuration. Make sure to configure each XBee with a unique MY address if there are more than two XBees in your CH and PAN ID. You will then need to adjust the DL address for each respective XBee.

14_Table4

Point-to-Multipoint (i.e. Broadcast Mode)

Tip: Controlling more than one robot? To control multiple XBees as a point-to-multipoint configuration, simply configure the transmitting XBee attached to the wireless joystick to broadcasting mode by setting DL = FFFF. Just make sure to configure your XBees with unique addresses.

15_Table5

Setting Up Arduino

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

Wireless Controller

SAMD21 Drivers

The wireless joystick has a built-in CDC. Depending on your operating system, you may need to install the drivers. Make sure to check out the section on drivers as explained in the SAMD21 Mini/Dev Breakout Hookup Guide.

16_SAMD21-Driver

Board SAMD21 Add-Ons

There are a few board add-ons to install. If you have not already, make sure to install the Arduino SAMD boards and the SparkFun board definitions as explained in the SAMD21 Mini/Dev Breakout Hookup Guide. These are the same add-ons used for the wireless joystick.

17_Board-SAMD21-Add-Ons

RedBot Mainboard

FTDI Drivers

Remember, to program your robot right from your browser, you will first need to install some FTDI drivers. Follow the steps in How to Install FTDI Drivers to do so. This is also explained in the RedBot Guides.

18_FTDI-Drivers

How to Install FTDI Drivers

How to install drivers for the FTDI Basic on Windows, Mac OS X, and Linux.

Arduino Library

Note: If you have not previously installed an Arduino library, please check out our installation guide.

Make sure to install the RedBot library as explained in the RedBot Library Quick Reference. You'll also find the quick overview of the RedBot Library, classes, methods, and variables.

Experiment 1: Sending and Receiving a Signal

Introduction

There are a few methods of transmitting data between two Arduinos and a pair of XBees. You can send a serial character in transparent mode, packet in API mode, or control with an I/O pin. For simplicity, we will sending a character in transparent mode.

Parts Needed

You will need the following parts from the required materials:

  • 2x XBees (Configured to Series 1 Firmware)

  • 1x Cerberus Cable (or 1x micro-B USB and 1x mini-B USB Cable)

  • 1x Assembled Shadow Chassis w/ RedBot Mainboard

  • 4x AA Batteries

  • 1x Assembled Wireless Joystick

  • 1x LiPo Battery

1.1: Sending

For this part of the experiment, we are going to send a character from the controller to the RedBot on the same channel.

Hardware Hookup

If you have not already, insert the XBee and battery into the controller. Then connect the controller to your computer via USB cable.

19_Hardware-Hookup

Open the Sketch

Copy and paste the following code into the Arduino IDE. Select the SAMD21 DEV Breakout as the board, select the COM port that it enumerated on, flip the Wireless Joystick's switch to the ON position, and hit upload.

Copy Code
    /* 1_1_XBee_Transmit_Basic_SAMD21.ino

   XBee Transmit Basic SAMD21 Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   This is example code for the Wireless Joystick with SAMD21. Any character entered through the
   Serial Monitor will be sent to the hardware UART pins. Assuming that you have a pair of
   XBees Series 1 modules (or Series 3 modules configured with 802.15.4 protocol) on the
   same channel, a character will be transmitted wirelessly between the XBees. The receiving
   XBee will then pass the character to the an ATmega328P microcontroller to eventually control a robot.

  Note: You may need to connect A5 to the XBee Series 3's reset pin on the Wireless Joystick
  for certain XBee Series 3 modules. For more details, check out the xbee3_RESET() function.
*/

char c_data;//send values through the serial monitor for debugging

//LED to check if the LED is initialized.
const int status_LED = 13;

//needed for certain XBee Series 3 modules
#define xbee_reset A5

void setup() {

  SerialUSB.begin(9600);// Initialize Serial Monitor for DEBUGGING

  //Uncomment this if you want to wait until the serial monitor is open.
  //while (!SerialUSB); //Wait for Serial Monitor to Open

  SerialUSB.println("Wireless Joystick Controller Initializing");
  Serial1.begin(9600); // Start serial communication with XBee at 9600 baud

  xbee3_RESET();//in case XBee3 has issues initializing, hardware reset

  //Status LED to see if the Controller is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  SerialUSB.println("Wireless Joystick Controller's XBee Ready to Communicate");
  delay(10);
}//end setup

void loop() {

  //send commands via serial monitor for testing here
  if (SerialUSB.available()) {
    c_data = SerialUSB.read();//take character from serial monitor and store in variable

    Serial1.print(c_data);//send to XBee

    //echo back what was sent to serial monitor
    SerialUSB.println("Sending Character Here, ");
    SerialUSB.println(c_data);
    digitalWrite(status_LED, HIGH); //turn ON Status LED

  }

  delay(100);//add short delay for LED for feedback, this can be commented out if it is affecting performance
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

void xbee3_RESET() {

  //HARDWARE RESET
  /*
    - XBee Series 3 Hardware Reference Manual
    - Pg 31 Power Supply Design recommends decoupling capacitor between Vcc and GND.
      Tested with 10uF capacitor and without. This was not necessary.
    - Pg 60 Brown Out Detection. This is REQUIRED. Add a jumper between the XBee's Reset and A5
    https://www.digi.com/resources/documentation/digidocs/pdfs/90001543.pdf

    - Power cycle XBee Series 3 by grounding RESET Pin to avoid dicontinuities in ramp up and brown out detection
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2017/06/14/rmu_e203_avdd_ramp-j176

    - Minimum Time to Force Reset:
    - EFM32 devices = 50ns; EFM32PG/JG: Pearl and Jade Gecko =100ns
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2016/07/22/minimum_reset_holdt-PglD
  */
  pinMode(xbee_reset, OUTPUT);
  digitalWrite(xbee_reset, HIGH);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, LOW);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, HIGH);

  /*
    //SOFTWARE RESET
    //Software reset does not work with XBee Series 3... Needs a hardware reset
    delay(500);//wait until XBee Series 3 to start up after hardware reset
    Serial1.write("+++"); //Enter Command Mode
    delay(500);//short delay as the XBee gets into command mode
    Serial1.write("ATFR");//AT command for software reset
    Serial1.write("\r");//carriage return
    Serial1.write("\n");//new line
  */
}

Code to Note

The code sets up a variable to keep track of the character being sent, an LED for indicator on pin 13 when we are sending a character, and a pin to reset the XBee. Since the controller uses the SAMD21, we will initialize the serial monitor for debugging using SerialUSB and the hardware serial using Serial1 to send characters using an XBee at 9600 baud. The code will briefly toggle A5 to reset an XBee 3 when the board is powered up in our custom function called xbee3_RESET(). Once we are finished initializing, the LED will blink three times. Then we will listen to the serial monitor for any characters in an if() statement. If a character is sent through the serial terminal, we will pass the character on to the XBee and echo it back to the serial monitor for debugging.

1.2: Receiving

For this part of the experiment, we are going to have the RedBot receive a character from the first controller.

Hardware Hookup

If you have not already, insert the XBee into the RedBot. Then connect the Redbot to your computer via USB cable.

20_connect-the-Redbot

Open the Sketch

Copy and paste the following code into the Arduino IDE. Since we are uploading code for the RedBot Mainboard, we will need to select Arduino/Genuino Uno for the RedBot mainboard, select the corresponding COM port that it enumerated on, and flip the POWER switch to the ON position. Once these settings are adjusted, you can hit the upload button.

Copy Code
   /* 1_2_XBee_Receive_Basic_ATmega328P.ino
   XBee Receive Basic ATmega328P Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   The first step to controlling the RedBot remotely is to first drive it
   from the Serial Monitor in a tethered setup. This is example code
   for the RedBot Mainboard with ATmega328P. After uploading this sketch,
   keep the RedBot tethered to your computer with the USB cable. Flip the
   switches to the respective sides: MOTOR => RUN and POWER => ON. You
   will also need to have UART flipped to the XBee_SW_Serial side.

   Assuming that you have a pair of XBees 1s (or 3 configured with
   802.15.4 protocol) on the same channel, a character will be
   transmitted wirelessly between the XBees. Any charactered received
   from the XBee connected to the software serial defined pins will
   be passed to the Serial Monitor. For troubleshooting, any character
   sent through the Serial Monitor will be echoed back.

*/

#include <RedBot.h>  //include RedBot library

char c_data;  // variable for holding incoming data from XBee to Arduino

// We'll use RedBot SoftwareSerial to communicate with the XBee:
// For Atmega328P's
// XBee's DOUT (TX) is connected to pin 14 (Arduino's Software RX)
// XBee's DIN (RX) is connected to pin 15 (Arduino's Software TX)
#include <RedBotSoftwareSerial.h>
RedBotSoftwareSerial RedBotXBee; //make instance of Software Serial, pins defined already in modified Software Serial Library

//LED to check if the LED is initialized.
const int status_LED = 13;

void setup() {
  // Set up both ports at 9600 baud. This value is most important
  // for the XBee. Make sure the baud rate matches the config
  // setting of your XBee.
  RedBotXBee.begin(9600);// Initialize SW for XBee for receiving serial
  Serial.begin(9600);// Initialize HW for Serial Monitor for DEBUGGING

  //Status LED to see if the RedBot is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  Serial.println("RedBot Initialized!");
}//end setup

void loop() {

  if (RedBotXBee.available() || Serial.available()) {
    if (RedBotXBee.available()) {
      c_data = RedBotXBee.read();//store received value from XBee into variable

    }

    else if (Serial.available()) {
      c_data = Serial.read();//store received value from Serial Monitor into variable

    }

    Serial.println("Character Received, ");
    Serial.write(c_data);//send it out to serial monitor
    Serial.println();
    digitalWrite(status_LED, HIGH); //turn ON Status LED
    delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

  }

  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

Code to Note

The code for the RedBot is similar to the SAMD21. However, since we are using the ATmega328, we will be setting up the software serial to receive characters from the XBee. The RedBot uses a custom software serial so we will need to include the <RedBotSoftwareSerial.h>. We will initialize the serial monitor for debugging using Serial and the software serial using using RedBotXBee to receive the characters from the XBee at 9600 baud. When using an XBee 3 with the RedBot mainboard, the XBee 3 did not have any issues during its initial power up so there was no need to toggle the XBee 3's reset pin. Once we are finished initializing, the LED will blink three times again. Then we will listen to the serial monitor or software serial for any characters received in the if() statement. If a character is received, we will display the character in the serial monitor for debugging.

What You Should See

We'll open a serial terminal for each board to see if a character was sent from the controller to the RedBot. For the controller, we'll open a serial terminal at 9600 that the controller enumerated on. For the RedBot, we'll use the Arduino serial monitor at 9600 since we just uploaded code to the board. Sending any character in the serial terminal will echo back and the have controller's XBee wirelessly transmit a character to the RedBot's XBee. Once received, the character will display in th Arduino serial monitor.

21_character

Congratulations, you have successfully sent a character wirelessly between two Arduinos!

Experiment 2: Wirelessly Driving Forward

Introduction

Now that we have successfully sent a character, the next step is to have the controller receive an input before sending a character. Once the receiving robot receives the character, we'll have the motors drive forward.

Parts Needed

You will need the following parts from the required materials:

  • 2x XBees (Configured to Series 1 Firmware)

  • 1x Cerberus Cable (or 1x micro-B USB and 1x mini-B USB Cable)

  • 1x Assembled Shadow Chassis w/ RedBot Mainboard

  • 4x AA Batteries1x Assembled Wireless Joystick

  • 1x LiPo Battery

2.1: Remote Control w/ the SAMD21

For this part of the experiment, we are going to send a character from the controller based on the input. For simplicity, we will send a character when a button is pressed (D2) and the left joystick is in the up position.

Note: If you soldered a joystick on the right side of the board as well, pressing down on the joystick will also be acceptable!

Hardware Hookup

If you have not already, connect the controller to your computer via USB cable.

22_USB-cable

Open the Sketch

Copy and paste the following code into the Arduino IDE. Remember to select the SAMD21 DEV Breakout for the controller, select the COM port that it enumerated on, flip the Wireless Joystick's switch to the ON position, and hit upload.

Copy Code
/* 2_1_Remote_Control_SAMD21.ino
   Remote Control SAMD21 Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   This is example code for the Wireless Joystick with SAMD21. Any character entered through the
   Serial Monitor or when a condition statement is satisfied will be sent to the hardware UART pins.
   Assuming that you have a pair of XBees Series 1 modules (or Series 3 modules configured with 802.15.4 protocol) on the
   same channel, a character will be transmitted wirelessly between the XBees. The receiving
   XBee will then pass the character to the an ATmega328P microcontroller to move the robot forward.

   Pressing down on D2 (if you soldered the joystick on the right or a button) will check
   the joystick on the left. A character will be transmitted when moving the joystick:

       up = forward

   The RedBot will need to be programmed to read those values.

   Note: You may need to connect A5 to the XBee Series 3's reset pin on the Wireless Joystick
   for certain XBee Series 3 modules. For more details, check out the xbee3_RESET() function.
*/

#define FORWARD_REVERSE_JOYSTICK A3   // Pin used for left joystick's y-component
#define TURN_JOYSTICK A2   // Pin used for left joystick x-component

int buttonACCELERATE_State; //value to store the state of the button press
#define ACCELERATE_BUTTON 2 // Pin used for right trigger

// We'll store the the analog joystick values here
int16_t forward_reverse_Stick_value;
int16_t turnStick_value;

char c_data;//send values through the serial monitor for debugging

//LED to check if the LED is initialized.
const int status_LED = 13;

//needed for certain XBee Series 3 modules
#define xbee_reset A5

void setup() {

  SerialUSB.begin(9600);// Initialize Serial Monitor for DEBUGGING

  //Uncomment this if you want to wait until the serial monitor is open.
  //while (!SerialUSB); //Wait for Serial Monitor to Open

  SerialUSB.println("Wireless Joystick Controller Initializing");
  Serial1.begin(9600); // Start serial communication with XBee at 9600 baud

  xbee3_RESET();//in case XBee3 has issues initializing, hardware reset

  pinMode(ACCELERATE_BUTTON, INPUT_PULLUP); // Enable pullup resistor for accelerate button D2

  //Status LED to see if the RedBot is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  SerialUSB.println("Wireless Joystick Controller's XBee Ready to Communicate");
  delay(10);
}//end setup

void loop() {

  //initialize variables to read buttons
  buttonACCELERATE_State = digitalRead(ACCELERATE_BUTTON);
  /***button1state
    - LOW or 0 means pressed
    - HIGH or 1 means not pressed
   ****/
  //Store values read joystick
  forward_reverse_Stick_value = analogRead(FORWARD_REVERSE_JOYSTICK);
  turnStick_value = analogRead(TURN_JOYSTICK);

  //send commands via serial monitor for testing here
  if (SerialUSB.available()) {
    c_data = SerialUSB.read();//take character from serial monitor and store in variable

    Serial1.print(c_data);//send to XBee

    //echo back what was sent to serial monitor
    SerialUSB.println("Sending Character Here, ");
    SerialUSB.println(c_data);
    digitalWrite(status_LED, HIGH); //turn ON Status LED
  }

  if (buttonACCELERATE_State == LOW) {
    SerialUSB.println("Accelerate Button has been pressed!");

    if (forward_reverse_Stick_value > 1000) {
      SerialUSB.println("Forward");
      Serial1.print('A');//transmit to RedBot via XBees on the same channel
      digitalWrite(status_LED, HIGH); //turn ON Status LED
    }

    //Debug left analog joystick here
    //Boundaries vary depending on the joystick's read value
    //You may need to adjust the values in the condition statements to calibrate
    //Additional condition statements will need to be written for pivoting
    //and turning in reverse
    SerialUSB.print("forward_reverse_Stick_value  = "); //~1023 up, ~7-9 down
    SerialUSB.println(forward_reverse_Stick_value);
    SerialUSB.println("turnStick_value = "); //~1023 left, ~5-6 right
    SerialUSB.println(turnStick_value);
  }

  delay(100); //add short delay for LED for feedback, this can be commented out if it is affecting performance
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

void xbee3_RESET() {

  //HARDWARE RESET
  /*
    - XBee Series 3 Hardware Reference Manual
    - Pg 31 Power Supply Design recommends decoupling capacitor between Vcc and GND.
      Tested with 10uF capacitor and without. This was not necessary.
    - Pg 60 Brown Out Detection. This is REQUIRED. Add a jumper between the XBee's Reset and A5
    https://www.digi.com/resources/documentation/digidocs/pdfs/90001543.pdf

    - Power cycle XBee Series 3 by grounding RESET Pin to avoid dicontinuities in ramp up and brown out detection
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2017/06/14/rmu_e203_avdd_ramp-j176

    - Minimum Time to Force Reset:
    - EFM32 devices = 50ns; EFM32PG/JG: Pearl and Jade Gecko =100ns
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2016/07/22/minimum_reset_holdt-PglD
  */
  pinMode(xbee_reset, OUTPUT);
  digitalWrite(xbee_reset, HIGH);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, LOW);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, HIGH);

  /*
    //SOFTWARE RESET
    //Software reset does not work with XBee Series 3... Needs a hardware reset
    delay(500);//wait until XBee Series 3 to start up after hardware reset
    Serial1.write("+++"); //Enter Command Mode
    delay(500);//short delay as the XBee gets into command mode
    Serial1.write("ATFR");//AT command for software reset
    Serial1.write("\r");//carriage return
    Serial1.write("\n");//new line
  */
}

Code to Note

Adding on to the code in 1.1, we'll set up the pins for the joystick. Since the joystick has two potentiometers to determine it's position, we'll set up the analog read pins and have a variable to store the readings. We'll also set up the pin for the button connected to D2 and create a variable to determine the button state.

After initializing the joystick, we'll read the button state and the analog pins before storing the values in their respective variables. We'll leave the section of code that takes in serial characters from the serial monitor for debugging. Finally, we'll check if the button D2 has been pressed and send a character when the joystick is in the up position. If we are connected to a computer, we'll echo the character back for debugging.

2.2 Robot Receive w/ the ATmega328P

For this part of the experiment, we are going to receive a character from the controller and have the RedBot drive forward.

Hardware Hookup

If you have not already, connect the Redbot to your computer via USB cable.

23_Robot-Receive

Open the Sketch

Copy and paste the following code into the Arduino IDE. Remember, we will need to select Arduino/Genuino Uno for the RedBot mainboard, select the corresponding COM port that it enumerated on, and flip the POWER switch to the ON position. Once these settings are adjusted, you can hit the upload button.

Copy Code
/* 2_2_Robot_Receive_ATmega328P.ino
   Robot Receive ATmega328P Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   The first step to controlling the RedBot remotely is to first drive it
   from the Serial Monitor in a tethered setup. This is example code
   for the RedBot Mainboard with ATmega328P. After uploading this sketch,
   keep the RedBot tethered to your computer with the USB cable. Flip the
   switches to the respective sides: MOTOR => RUN and POWER => ON. You
   will also need to have UART flipped to the XBee_SW_Serial side.

   Assuming that you have a pair of XBees 1s (or 3 configured with
   802.15.4 protocol) on the same channel, a character will be
   transmitted wirelessly between the XBees. Any charactered received
   from the XBee connected to the software serial defined pins will
   be passed to the Serial Monitor. For troubleshooting, any character
   sent through the Serial Monitor will be echoed back. Try testing the
   controller to see if the robot will move forward or sending the following
   character through the Serial Monitor.

       A = forward

  If your motors are not moving forward when you send the forward command,
  simply flip the wiring. You can adjust the code but that would require
  adjusting more than one line of code. This does not account for motor
  intensity like the example that is used with the Wireless Joystick Example
  and RedBot Experiment 9.

  WARNING: Make sure to flip the switch to the XBEE_SW_SERIAL when
  you are uploading to the RedBot Mainboard. You will have issues uploading
  code and possibly brick your XBee.
*/

#include <RedBot.h>  //include RedBot library
RedBotMotors motors; //make instance of RedBot

char c_data;  // variable for holding incoming data from XBee to Arduino

// We'll use RedBot SoftwareSerial to communicate with the XBee:
// For Atmega328P's
// XBee's DOUT (TX) is connected to pin 14 (Arduino's Software RX)
// XBee's DIN (RX) is connected to pin 15 (Arduino's Software TX)
#include <RedBotSoftwareSerial.h>
RedBotSoftwareSerial RedBotXBee; //make instance of Software Serial, pins     defined already in modified Software Serial Library

//LED to check if the LED is initialized.
const int status_LED = 13;

void setup() {
  // Set up both ports at 9600 baud. This value is most important
  // for the XBee. Make sure the baud rate matches the config
  // setting of your XBee.
  RedBotXBee.begin(9600);// Initialize SW for XBee for receiving serial
  Serial.begin(9600);// Initialize HW for Serial Monitor for DEBUGGING

  //Status LED to see if the RedBot is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  Serial.println("RedBot Initialized!");
}//end setup

void loop() {

  if (RedBotXBee.available() || Serial.available()) {
    if (RedBotXBee.available()) {
      c_data = RedBotXBee.read();//store received value from XBee into variable

    }

    else if (Serial.available()) {
      c_data = Serial.read();//store received value from Serial Monitor into variable

    }

    Serial.println("Character Received, ");
    Serial.write(c_data);//send it out to serial monitor
    Serial.println();
    digitalWrite(status_LED, HIGH); //turn ON Status LED
    //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

    if (c_data == 'A') {
      Serial.println("Drive Forward");
      RedBotXBee.write('A');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.drive(255); //forward
   }
    else {
      //nothing was received, do nothing
    }


  }

  delay(100); // short pause so we are not constantly receiving characters
  motors.stop();//turn off motors
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

Code to Note

Since we are using the RedBot's motors, we'll need to set up the motors right after including the library. Again, we'll leave the section of code that takes in serial characters from the serial monitor for debugging. Note that this section of code also takes in characters received from the XBee and saves it in a variable.

Shortly after, we'll check to see what if the character matches what we sent from the controller. If the character matches, we'll move the wheels forward at full power. A short delay was added to have the robot move forward before shutting off the motors. For debugging, we'll send a message to the serial monitor indicating that we received a character to drive forward and light the LED briefly.

What You Should See

Disconnect the controller and robot from your computer. Insert the batteries to the boards. Pressing on the button connected to D2 and moving the left joystick to the up position will send a character out from the controller. The receiving RedBot should drive forward remotely!

wireless rc redbot

Experiment 3: Wirelessly Controlling a Robot

Introduction

Now that we are able to wirelessly move our robot forward, we will want additional commands for turning and driving in reverse.

Parts Needed

You will need the following parts from the required materials:

  • 2x XBees (Configured to Series 1 Firmware)

  • 1x Cerberus Cable (or 1x micro-B USB and 1x mini-B USB Cable)

  • 1x Assembled Shadow Chassis w/ RedBot Mainboard

  • 4x AA Batteries

  • 1x Assembled Wireless Joystick

  • 1x LiPo Battery

3.1: Full Remote Control w/ the SAMD21

For this part of the experiment, we will repeat the steps in 2.1 to transmit commands for turning or driving in reverse.

Hardware Hookup

Reconnect the controller to your computer via USB cable.

25_reconnect

Open the Sketch

Copy and paste the following code into the Arduino IDE. Remember to select the SAMD21 DEV Breakout for the controller, select the COM port that it enumerated on, flip the Wireless Joystick's switch to the ON position, and hit upload.

Copy Code
/* 3_1_Full_Remote_Control_SAMD21.ino
   Full Remote Control SAMD21 Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   This is example code for the Wireless Joystick with SAMD21. Any character entered through the
   Serial Monitor or when a condition statement is satisfied will be sent to the hardware UART pins.
   Assuming that you have a pair of XBees Series 1 modules (or Series 3 modules configured with 802.15.4 protocol) on the
   same channel, a character will be transmitted wirelessly between the XBees. The receiving
   XBee will then pass the character to the an ATmega328P microcontroller to move the robot forward.

   Pressing down on D2 (if you soldered the joystick on the right or a button) will check
   the joystick on the left. A character will be transmitted when moving the joystick.

       up = forward
       right = forward turn right
       down = reverse
       left = forward turn left
       center = coast

   When D2 is not being pressed, a character will be sent to stop the motors.

   The RedBot will need to be programmed to read those values.

   Note: You may need to connect A5 to the XBee Series 3's reset pin on the Wireless Joystick
   for certain XBee Series 3 modules. For more details, check out the xbee3_RESET() function.
*/

#define FORWARD_REVERSE_JOYSTICK A3   // Pin used for left joystick's y-component
#define TURN_JOYSTICK A2   // Pin used for left joystick x-component

int prev_buttonACCELERATE_State;    //value to store the previous state of the button press
int current_buttonACCELERATE_State; //value to store the current state of the button press
#define ACCELERATE_BUTTON 2 // Pin used for right trigger

// We'll store the the analog joystick values here
int16_t forward_reverse_Stick_value;
int16_t turnStick_value;

char c_data;//send values through the serial monitor for debugging

//LED to check if the LED is initialized.
const int status_LED = 13;

//needed for certain XBee Series 3 modules
#define xbee_reset A5

void setup() {

  SerialUSB.begin(9600);// Initialize Serial Monitor for DEBUGGING

  //Uncomment this if you want to wait until the serial monitor is open.
  //while (!SerialUSB); //Wait for Serial Monitor to Open

  SerialUSB.println("Wireless Joystick Controller Initializing");
  Serial1.begin(9600); // Start serial communication with XBee at 9600 baud

  xbee3_RESET();//in case XBee3 has issues initializing, hardware reset

  pinMode(ACCELERATE_BUTTON, INPUT_PULLUP); // Enable pullup resistor for accelerate button D2

  //Status LED to see if the Controller is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }
  SerialUSB.println("Wireless Joystick Controller's XBee Ready to Communicate");
  delay(10);
}//end setup

void loop() {

  //initialize variables to read buttons
  current_buttonACCELERATE_State = digitalRead(ACCELERATE_BUTTON);
  /***button1state
    - LOW or 0 means pressed
    - HIGH or 1 means not pressed
   ****/
  //Store values read joystick
  forward_reverse_Stick_value = analogRead(FORWARD_REVERSE_JOYSTICK);
  turnStick_value = analogRead(TURN_JOYSTICK);

  //send commands via serial monitor for testing here
  if (SerialUSB.available()) {
    c_data = SerialUSB.read();//take character from serial monitor and store in variable

    Serial1.print(c_data);//send to XBee

    //echo back what was sent to serial monitor
    SerialUSB.println("Sending Character Here, ");
    SerialUSB.println(c_data);

  }

  if (current_buttonACCELERATE_State == LOW) {
    SerialUSB.println("Accelerate Button has been pressed!");

    if (forward_reverse_Stick_value > 1000) {
      SerialUSB.println("Forward");
      Serial1.print('A');//transmit to RedBot via XBees on the same channel
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if ( turnStick_value < 20) {
     SerialUSB.println("Turn Right");
      Serial1.print('B');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if (forward_reverse_Stick_value < 20) {

      SerialUSB.println("Reverse");
      Serial1.print('C');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if (turnStick_value > 1000) {
      SerialUSB.println("Turn Left");
      Serial1.print('D');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

    }
    else {
      SerialUSB.println("Coast");
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      Serial1.print('J');
    }

    //Debug left analog joystick here
    //Boundaries vary depending on the joystick's read value
    //You may need to adjust the values in the condition statements to calibrate
    //Additional condition statements will need to be written for pivoting
    //and turning in reverse
    SerialUSB.print("forward_reverse_Stick_value  = "); //~1023 up, ~7-9 down
    SerialUSB.println(forward_reverse_Stick_value);
    SerialUSB.println("turnStick_value = "); //~1023 left, ~5-6 right
    SerialUSB.println(turnStick_value);

  }
  else {//current_buttonACCELERATE_State == HIGH
    //if not sending a command to drive, automatically have the robot stop moving
      SerialUSB.println("Stop");
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      Serial1.print('K');

  }
  prev_buttonACCELERATE_State = current_buttonACCELERATE_State; //save current state

  delay(100); //add short delay for LED for feedback, this can be commented out if it is affecting performance
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

void xbee3_RESET() {

  //HARDWARE RESET
  /*
    - XBee Series 3 Hardware Reference Manual
    - Pg 31 Power Supply Design recommends decoupling capacitor between Vcc and GND.
      Tested with 10uF capacitor and without. This was not necessary.
    - Pg 60 Brown Out Detection. This is REQUIRED. Add a jumper between the XBee's Reset and A5
    https://www.digi.com/resources/documentation/digidocs/pdfs/90001543.pdf

    - Power cycle XBee Series 3 by grounding RESET Pin to avoid dicontinuities in ramp up and brown out detection
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2017/06/14/rmu_e203_avdd_ramp-j176

    - Minimum Time to Force Reset:
    - EFM32 devices = 50ns; EFM32PG/JG: Pearl and Jade Gecko =100ns
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2016/07/22/minimum_reset_holdt-PglD
  */
  pinMode(xbee_reset, OUTPUT);
  digitalWrite(xbee_reset, HIGH);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, LOW);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, HIGH);

  /*
    //SOFTWARE RESET
    //Software reset does not work with XBee Series 3... Needs a hardware reset
    delay(500);//wait until XBee Series 3 to start up after hardware reset
    Serial1.write("+++"); //Enter Command Mode
    delay(500);//short delay as the XBee gets into command mode
    Serial1.write("ATFR");//AT command for software reset
    Serial1.write("\r");//carriage return
    Serial1.write("\n");//new line
  */
}

Code to Note

To add more commands, we simply add more if() statements to check the position of the joystick on the right, down, and left positions. If the joystick is in any of those position, send a command to move the RedBot forward toward the right, reverse, and forward toward the left, respectively. If the joystick is in the center, we'll send a command to have the RedBot coast a bit. Otherwise, we'll continually send a command to have the RedBot stop when we are not pressing on D2.

3.2 Full Robot Control w/ the ATmega328P

For this part of the experiment, we will repeat the steps in 2.2 to receive the commands before moving the robot. Instead of just driving forward, the robot can now turn, and reverse.

Hardware Hookup

Reconnect the Redbot to your computer via USB cable.

26_Reconnect2

Open the Sketch

Copy and paste the following code into the Arduino IDE. Remember, we will need to select Arduino/Genuino Uno for the RedBot mainboard, select the corresponding COM port that it enumerated on, and flip the POWER switch to the ON position. Once these settings are adjusted, you can hit the upload button.

Copy Code
/* 3_2_Full_Robot_Control_ATmega328P.ino
   Full Robot Control ATmega328P Example
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   The first step to controlling the RedBot remotely is to first drive it
   from the Serial Monitor in a tethered setup. This is example code
   for the RedBot Mainboard with ATmega328P. After uploading this sketch,
   keep the RedBot tethered to your computer with the USB cable. Flip the
   switches to the respective sides: MOTOR => RUN and POWER => ON. You
   will also need to have UART flipped to the XBee_SW_Serial side.

   Assuming that you have a pair of XBees 1s (or 3 configured with
   802.15.4 protocol) on the same channel, a character will be
   transmitted wirelessly between the XBees. Any charactered received
   from the XBee connected to the software serial defined pins will
   be passed to the Serial Monitor. For troubleshooting, any character
   sent through the Serial Monitor will be echoed back. Try testing the
   controller to see if the robot will move forward or sending the following
   character through the Serial Monitor.

       A = forward
       B = forward turn right
       C = reverse
       D = forward turn left
       J = coast
       K = stop

  If your motors are not moving forward when you send the forward command,
  simply flip the wiring. You can adjust the code but that would require
  adjusting more than one line of code. This does not account for motor
  intensity like the example that is used with the Wireless Joystick Example
  and RedBot Experiment 9.

  WARNING: Make sure to flip the switch to the XBEE_SW_SERIAL when
  you are uploading to the RedBot Mainboard. You will have issues uploading
  code and possibly brick your XBee.
*/

#include <RedBot.h>  //include RedBot library
RedBotMotors motors; //make instance of RedBot

char c_data;  // variable for holding incoming data from XBee to Arduino

// We'll use RedBot SoftwareSerial to communicate with the XBee:
// For Atmega328P's
// XBee's DOUT (TX) is connected to pin 14 (Arduino's Software RX)
// XBee's DIN (RX) is connected to pin 15 (Arduino's Software TX)
#include <RedBotSoftwareSerial.h>
RedBotSoftwareSerial RedBotXBee; //make instance of Software Serial, pins     defined already in modified Software Serial Library

//LED to check if the LED is initialized.
const int status_LED = 13;

void setup() {
  // Set up both ports at 9600 baud. This value is most important
  // for the XBee. Make sure the baud rate matches the config
  // setting of your XBee.
  RedBotXBee.begin(9600);// Initialize SW for XBee for receiving serial
  Serial.begin(9600);// Initialize HW for Serial Monitor for DEBUGGING

  //Status LED to see if the RedBot is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  Serial.println("RedBot Initialized!");
}//end setup

void loop() {

  if (RedBotXBee.available() || Serial.available()) {
    if (RedBotXBee.available()) {
      c_data = RedBotXBee.read();//store received value from XBee into variable
    }

    else if (Serial.available()) {
      c_data = Serial.read();//store received value from Serial Monitor into variable
    }

    Serial.println("Character Received, ");
    Serial.write(c_data);//send it out to serial monitor
    Serial.println();
    digitalWrite(status_LED, HIGH); //turn ON Status LED
    //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

    if (c_data == 'A') {
      Serial.println("Drive Forward");
      RedBotXBee.write('A');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.drive(255); //forward
    }
    else if (c_data == 'B') {
      Serial.println("Turn Right");
      RedBotXBee.write('B');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.leftMotor(-200); // Turn on left motor power (motorPower = )
      motors.rightMotor(100); // Turn on right motor power (motorPower = )
    }
    else if (c_data == 'C') {
      Serial.println("Reverse");
      RedBotXBee.write('C');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.drive(-255); //reverse
    }
    else if (c_data == 'D') {
      Serial.println("Turn Left");
      RedBotXBee.write('D');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.leftMotor(-100); // Turn on left motor power (motorPower = )
      motors.rightMotor(200); // Turn on right motor power (motorPower = )
    }
    else if (c_data == 'J') {
      Serial.println("Coast");
      RedBotXBee.write('J');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      motors.coast();
    }
    else if (c_data == 'K') {
      Serial.println("Stop");
      RedBotXBee.write('K');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      motors.stop();
    }

  }

  //delay(100); // short pause so we are not constantly receiving characters
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

Code to Note

Similar to 3.1, we'll add additional if() statements to move the RedBot if the character matches what was sent. We'll adjust the motor power and direction for each condition when we receive the command to forward toward the right, reverse, forward toward the left, coast, or stop.

What You Should See

Disconnect the controller and robot from your computer. Press on D2 and move the joystick around. You should see the RedBot move toward the direction relative to the position of the joystick!

wireless rc redbot

Experiment 4: Wirelessly Triggering Audio

Introduction

Remember making sounds with the RedBot? In this section, we'll wirelessly control the buzzer to make a familiar sound.

Parts Needed

You will need the following parts from the required materials:

  • 2x XBees (Configured to Series 1 Firmware)

  • 1x Cerberus Cable (or 1x micro-B USB and 1x mini-B USB Cable)

  • 1x Assembled Shadow Chassis w/ RedBot Mainboard

  • 1x Piezo Buzzer

  • 4x AA Batteries

  • 1x Assembled Wireless Joystick

  • 1x LiPo Battery

4.1: Adding Audio Commands w/ the SAMD21

For this part of the experiment, we will add a few commands to trigger a familiar sound.

Hardware Hookup

If you have not already, insert the XBee and battery into the controller. Then connect the controller to your computer via USB cable.

28_Audio-Commands

Open the Sketch

Copy and paste the following code into the Arduino IDE. Remember to select the SAMD21 DEV Breakout for the controller, select the COM port that it enumerated on, flip the Wireless Joystick's switch to the ON position, and hit upload.

Copy Code
/* 4_1_Full_Remote_Control_SAMD_Audio.ino
   Full Remote Control SAMD21 Example with Buzzer
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   This is example code for the Wireless Joystick with SAMD21. Any character entered through the
   Serial Monitor or when a condition statement is satisfied will be sent to the hardware UART pins.
   Assuming that you have a pair of XBees Series 1 modules (or Series 3 modules configured with 802.15.4 protocol) on the
   same channel, a character will be transmitted wirelessly between the XBees. The receiving
   XBee will then pass the character to the an ATmega328P microcontroller to move the robot forward.

   Pressing down on D2 (if you soldered the joystick on the right or a button) will check
   the joystick on the left. A character will be transmitted when moving the joystick.

       up = forward
       right = forward turn right
       down = reverse
       left = forward turn left
       center = coast

   When D2 is not being pressed, a character will be sent to stop the motors.

   Pressing down on D6 (left trigger) or D3 (right trigger) will send another character

       left trigger = coin
       right trigger = fireball

   The RedBot will need to be programmed to read those values.

   Note: You may need to connect A5 to the XBee Series 3's reset pin on the Wireless Joystick
   for certain XBee Series 3 modules. For more details, check out the xbee3_RESET() function.
*/

#define L_TRIG 6        // Pin used for left trigger
#define R_TRIG 3        // Pin used for right trigger
boolean prev_buttonL_State = HIGH;    //value to store the previous state of the button press
boolean current_buttonL_State = HIGH; //value to store the current state of the button press

boolean prev_buttonR_State = HIGH;    //value to store the previous state of the button press
boolean current_buttonR_State = HIGH; //value to store the current state of the button press

#define FORWARD_REVERSE_JOYSTICK A3   // Pin used for left joystick's y-component
#define TURN_JOYSTICK A2   // Pin used for left joystick x-component

boolean current_buttonACCELERATE_State;
#define ACCELERATE_BUTTON 2 // Pin used for right trigger

// We'll store the the analog joystick values here
int16_t forward_reverse_Stick_value;
int16_t turnStick_value;

char c_data;//send values through the serial monitor for debugging

//LED to check if the LED is initialized.
const int status_LED = 13;

//needed for certain XBee Series 3 modules
#define xbee_reset A5

void setup() {

  pinMode(L_TRIG, INPUT_PULLUP); // Enable pullup resistor for left trigger
  pinMode(R_TRIG, INPUT_PULLUP); // Enable pullup resistor for right trigger

  SerialUSB.begin(9600);// Initialize Serial Monitor for DEBUGGING

  //Uncomment this if you want to wait until the serial monitor is open.
  //while (!SerialUSB); //Wait for Serial Monitor to Open

  SerialUSB.println("Wireless Joystick Controller Initializing");
  Serial1.begin(9600); // Start serial communication with XBee at 9600 baud

  xbee3_RESET();//in case XBee3 has issues initializing, hardware reset

  pinMode(ACCELERATE_BUTTON, INPUT_PULLUP); // Enable pullup resistor for accelerate button D2

  //Status LED to see if the Controller is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }
  SerialUSB.println("Wireless Joystick Controller's XBee Ready to Communicate");
  delay(10);
}//end setup

void loop() {

  current_buttonL_State = digitalRead(L_TRIG);
  current_buttonR_State = digitalRead(R_TRIG);

  //initialize variables to read buttons
  current_buttonACCELERATE_State = digitalRead(ACCELERATE_BUTTON);
  /***button1state
    - LOW or 0 means pressed
    - HIGH or 1 means not pressed
   ****/
  //Store values read joystick
  forward_reverse_Stick_value = analogRead(FORWARD_REVERSE_JOYSTICK);
  turnStick_value = analogRead(TURN_JOYSTICK);

  //send commands via serial monitor for testing here
  if (SerialUSB.available()) {
    c_data = SerialUSB.read();//take character from serial monitor and store in variable

    Serial1.print(c_data);//send to XBee

    //echo back what was sent to serial monitor
    SerialUSB.println("Sending Character Here, ");
    SerialUSB.println(c_data);

  }

  if (current_buttonACCELERATE_State == LOW) {
    SerialUSB.println("Accelerate Button has been pressed!");

    if (forward_reverse_Stick_value > 1000) {
      SerialUSB.println("Forward");
      Serial1.print('A');//transmit to RedBot via XBees on the same channel
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if ( turnStick_value < 20) {
      SerialUSB.println("Turn Right");
      Serial1.print('B');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if (forward_reverse_Stick_value < 20) {

      SerialUSB.println("Reverse");
      Serial1.print('C');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance
    }
    else if (turnStick_value > 1000) {
      SerialUSB.println("Turn Left");
      Serial1.print('D');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

    }
    else {
      SerialUSB.println("Coast");
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      Serial1.print('J');
    }

    //Debug left analog joystick here
    //Boundaries vary depending on the joystick's read value
    //You may need to adjust the values in the condition statements to calibrate
    //Additional condition statements will need to be written for pivoting
    //and turning in reverse
    SerialUSB.print("forward_reverse_Stick_value  = "); //~1023 up, ~7-9 down
    SerialUSB.println(forward_reverse_Stick_value);
    SerialUSB.println("turnStick_value = "); //~1023 left, ~5-6 right
    SerialUSB.println(turnStick_value);

  }
  else {//current_buttonACCELERATE_State == HIGH
    //if not sending a command to drive, automatically have the robot stop moving
    SerialUSB.println("Stop");
    digitalWrite(status_LED, HIGH); //turn ON Status LED
    Serial1.print('K');
  }


  if (current_buttonL_State == LOW) {
    if (prev_buttonL_State != current_buttonL_State) {
      SerialUSB.println("R Trigger Button has been pressed!");
      SerialUSB.println("Coin Sound");
      Serial1.print('X');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
    }
  }
  if (current_buttonR_State == LOW) {
    if (prev_buttonR_State != current_buttonR_State) {
      SerialUSB.println("R Trigger Button has been pressed!");
      SerialUSB.println("Fireball Sound");
      Serial1.print('Y');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
    }
  }

  prev_buttonL_State = current_buttonL_State; //save current state
  prev_buttonR_State = current_buttonR_State; //save current state
  delay(100); //add short delay for LED for feedback, this can be commented out if it is affecting performance
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

void xbee3_RESET() {

  //HARDWARE RESET
  /*
    - XBee Series 3 Hardware Reference Manual
    - Pg 31 Power Supply Design recommends decoupling capacitor between Vcc and GND.
      Tested with 10uF capacitor and without. This was not necessary.
    - Pg 60 Brown Out Detection. This is REQUIRED. Add a jumper between the XBee's Reset and A5
    https://www.digi.com/resources/documentation/digidocs/pdfs/90001543.pdf

    - Power cycle XBee Series 3 by grounding RESET Pin to avoid dicontinuities in ramp up and brown out detection
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2017/06/14/rmu_e203_avdd_ramp-j176

    - Minimum Time to Force Reset:
    - EFM32 devices = 50ns; EFM32PG/JG: Pearl and Jade Gecko =100ns
    https://www.silabs.com/community/mcu/32-bit/knowledge-base.entry.html/2016/07/22/minimum_reset_holdt-PglD
  */
  pinMode(xbee_reset, OUTPUT);
  digitalWrite(xbee_reset, HIGH);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, LOW);
  delayMicroseconds(1);
  digitalWrite(xbee_reset, HIGH);

  /*
    //SOFTWARE RESET
    //Software reset does not work with XBee Series 3... Needs a hardware reset
    delay(500);//wait until XBee Series 3 to start up after hardware reset
    Serial1.write("+++"); //Enter Command Mode
    delay(500);//short delay as the XBee gets into command mode
    Serial1.write("ATFR");//AT command for software reset
    Serial1.write("\r");//carriage return
    Serial1.write("\n");//new line
  */
}

Code to Note

Adding to the current list of defined commands, we'll define two more buttons at the top for the left and right triggers. You'll notice that there is additional code to keep track of the previous and current states of the two buttons.

Further down in the loop() after the commands, we create a nested if() statement for each button so that we only send the command to trigger the buzzer once when the button is pressed. We'll want to send these audio commands only after letting go of the button.

4.2 Adding Audio w/ the ATmega328P

For this part of the experiment, we will receive characters to control the piezo buzzer on the RedBot.

Hardware Hookup

We'll assume that the buzzer is attached to pin 9 like the assembly guide. If you have not already, insert the XBee into the RedBot. Then connect the Redbot to your computer via USB cable.

29_buzzer

Open the Sketch

Copy and paste the following code into the Arduino IDE.

Copy Code
/* 4_2_Full_Remote_Control_SAMD_Audio.ino
   Full Robot Control ATmega328P Example with Buzzer
   Written by: Ho Yun Bobby Chan
   Date: 2/15/19
   SparkFun Electronics

   license: Creative Commons Attribution-ShareAlike 4.0 (CC BY-SA 4.0)
   Do whatever you'd like with this code, use it for any purpose.
   Please attribute and keep this license.

   The first step to controlling the RedBot remotely is to first drive it
   from the Serial Monitor in a tethered setup. This is example code
   for the RedBot Mainboard with ATmega328P. After uploading this sketch,
   keep the RedBot tethered to your computer with the USB cable. Flip the
   switches to the respective sides: MOTOR => RUN and POWER => ON. You
   will also need to have UART flipped to the XBee_SW_Serial side.

   Assuming that you have a pair of XBees 1s (or 3 configured with
   802.15.4 protocol) on the same channel, a character will be
   transmitted wirelessly between the XBees. Any charactered received
   from the XBee connected to the software serial defined pins will
   be passed to the Serial Monitor. For troubleshooting, any character
   sent through the Serial Monitor will be echoed back. Try testing the
   controller to see if the robot will move forward or sending the following
   character through the Serial Monitor.

       A = forward
       B = forward turn right
       C = reverse
       D = forward turn left
       J = coast
       K = stop
       X = coin cointer sound effect
       Y = fireball sound effect

  If your motors are not moving forward when you send the forward command,
  simply flip the wiring. You can adjust the code but that would require
  adjusting more than one line of code. This does not account for motor
  intensity like the example that is used with the Wireless Joystick Example
  and RedBot Experiment 9.

  WARNING: Make sure to flip the switch to the XBEE_SW_SERIAL when
  you are uploading to the RedBot Mainboard. You will have issues uploading
  code and possibly brick your XBee.
*/

#include "pitches.h" //include pitches.h from tab

#include <RedBot.h>  //include RedBot library
RedBotMotors motors; //make instance of RedBot

char c_data;  // variable for holding incoming data from XBee to Arduino

// We'll use RedBot SoftwareSerial to communicate with the XBee:
// For Atmega328P's
// XBee's DOUT (TX) is connected to pin 14 (Arduino's Software RX)
// XBee's DIN (RX) is connected to pin 15 (Arduino's Software TX)
#include <RedBotSoftwareSerial.h>
RedBotSoftwareSerial RedBotXBee; //make instance of Software Serial, pins     defined already in modified Software Serial Library

//LED to check if the LED is initialized.
const int status_LED = 13;
int coin_counter = 0;//counter for coins and 1-up

void setup() {
  // Set up both ports at 9600 baud. This value is most important
  // for the XBee. Make sure the baud rate matches the config
  // setting of your XBee.
  RedBotXBee.begin(9600);// Initialize SW for XBee for receiving serial
  Serial.begin(9600);// Initialize HW for Serial Monitor for DEBUGGING

  //Status LED to see if the RedBot is initializing
  pinMode(status_LED, OUTPUT);
  for (int i = 0; i < 3; i++) {
    digitalWrite(status_LED, HIGH);//set Status LED on
    delay(50);
    digitalWrite(status_LED, LOW); //set Status LED off
    delay(50);
  }

  pinMode(9, OUTPUT); //buzzer

  tone(9, NOTE_E6, 125);
  delay(130);
  noTone(9);

  Serial.println("RedBot Initialized!");
}//end setup

void loop() {

  if (RedBotXBee.available() || Serial.available()) {
    if (RedBotXBee.available()) {
      c_data = RedBotXBee.read();//store received value from XBee into variable
    }

    else if (Serial.available()) {
      c_data = Serial.read();//store received value from Serial Monitor into variable
    }

    Serial.println("Character Received, ");
    Serial.write(c_data);//send it out to serial monitor
    Serial.println();
    digitalWrite(status_LED, HIGH); //turn ON Status LED
    //delayMicroseconds(500);//add short delay for LED for feedback, this can be commented out if it is affecting performance

    if (c_data == 'A') {
      Serial.println("Drive Forward");
      RedBotXBee.write('A');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.drive(255); //forward
    }
    else if (c_data == 'B') {
      Serial.println("Turn Right");
      RedBotXBee.write('B');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.leftMotor(-200); // Turn on left motor power (motorPower = )
      motors.rightMotor(100); // Turn on right motor power (motorPower = )
    }
    else if (c_data == 'C') {
      Serial.println("Reverse");
      RedBotXBee.write('C');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.drive(-255); //reverse
    }
    else if (c_data == 'D') {
      Serial.println("Turn Left");
      RedBotXBee.write('D');
      digitalWrite(status_LED, HIGH); //turn ON Status LED

      motors.leftMotor(-100); // Turn on left motor power (motorPower = )
      motors.rightMotor(200); // Turn on right motor power (motorPower = )
    }
    else if (c_data == 'J') {
      Serial.println("Coast");
      RedBotXBee.write('J');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      motors.coast();
    }
    else if (c_data == 'K') {
      Serial.println("Stop");
      RedBotXBee.write('K');
      digitalWrite(status_LED, HIGH); //turn ON Status LED
      motors.stop();
    }
    else if (c_data == 'X') {
      // Play coin sound
      Serial.println("Coin Sound");


      if (coin_counter < 100) {
        coin_counter = coin_counter + 1; //add 1 coin
        Serial.print("Coin Counter = ");
        Serial.println(coin_counter);
        RedBotXBee.write('X');

        digitalWrite(status_LED, HIGH);  // turn the LED on

        tone(9, NOTE_B5, 100);
        delay(50);
        tone(9, NOTE_E6, 850);
        delay(400);
        noTone(9);
      }
      else if (coin_counter <= 100) {
        coin_counter = 0;//set back coins to 0;

        Serial.print("100 Coins Received! 1-Up");
        Serial.print("Coin Counter reset to = ");
        Serial.println(coin_counter);
        RedBotXBee.write('X');
        digitalWrite(status_LED, HIGH); //turn ON Status LED


        tone(9, NOTE_E6, 125);
        delay(130);
        tone(9, NOTE_G6, 125);
        delay(130);
        tone(9, NOTE_E7, 125);
        delay(130);
        tone(9, NOTE_C7, 125);
        delay(130);
        tone(9, NOTE_D7, 125);
        delay(130);
        tone(9, NOTE_G7, 125);
        delay(125);
        noTone(9);
      }

    }
    else if (c_data == 'Y') {
      // Play coin sound
      Serial.println("Fireball Sound");
      RedBotXBee.write('Y');

      digitalWrite(status_LED, HIGH); //turn ON Status LED

      // Play Fireball sound
      tone(9, NOTE_G4, 35);
      delay(35);
      tone(9, NOTE_G5, 35);
      delay(35);
      tone(9, NOTE_G6, 35);
      delay(35);
      noTone(9);
    }
  }

  //delay(100); // short pause so we are not constantly receiving characters
  digitalWrite(status_LED, LOW); //turn OFF Status LED
}//end loop

Adding a Tabbed File

Along with the example, you will need to include the following pitches.h header file that was originally written by Brett Hagman. You may remember this file being named notes.h. To make the pitches.h file, either click on the arrow button just below the serial monitor icon and choose "New Tab", or use Ctrl+Shift+N shortcut. Name the file as pitches.h to help break up the example sketch.

30_Tabbed-File

Copy and paste the following code the Arduino IDE's new tab and save. As a result, a new file will be included in the same folder as the example code. Remember, we will need to select Arduino/Genuino Uno for the RedBot mainboard, select the corresponding COM port that it enumerated on, and flip the POWER switch to the ON position. Once these settings are adjusted, you can hit the upload button.

Copy Code
/*************************************************
 * Public Constants
 *************************************************/

#define NOTE_B0  31
#define NOTE_C1  33
#define NOTE_CS1 35
#define NOTE_D1  37
#define NOTE_DS1 39
#define NOTE_E1  41
#define NOTE_F1  44
#define NOTE_FS1 46
#define NOTE_G1  49
#define NOTE_GS1 52
#define NOTE_A1  55
#define NOTE_AS1 58
#define NOTE_B1  62
#define NOTE_C2  65
#define NOTE_CS2 69
#define NOTE_D2  73
#define NOTE_DS2 78
#define NOTE_E2  82
#define NOTE_F2  87
#define NOTE_FS2 93
#define NOTE_G2  98
#define NOTE_GS2 104
#define NOTE_A2  110
#define NOTE_AS2 117
#define NOTE_B2  123
#define NOTE_C3  131
#define NOTE_CS3 139
#define NOTE_D3  147
#define NOTE_DS3 156
#define NOTE_E3  165
#define NOTE_F3  175
#define NOTE_FS3 185
#define NOTE_G3  196
#define NOTE_GS3 208
#define NOTE_A3  220
#define NOTE_AS3 233
#define NOTE_B3  247
#define NOTE_C4  262
#define NOTE_CS4 277
#define NOTE_D4  294
#define NOTE_DS4 311
#define NOTE_E4  330
#define NOTE_F4  349
#define NOTE_FS4 370
#define NOTE_G4  392
#define NOTE_GS4 415
#define NOTE_A4  440
#define NOTE_AS4 466
#define NOTE_B4  494
#define NOTE_C5  523
#define NOTE_CS5 554
#define NOTE_D5  587
#define NOTE_DS5 622
#define NOTE_E5  659
#define NOTE_F5  698
#define NOTE_FS5 740
#define NOTE_G5  784
#define NOTE_GS5 831
#define NOTE_A5  880
#define NOTE_AS5 932
#define NOTE_B5  988
#define NOTE_C6  1047
#define NOTE_CS6 1109
#define NOTE_D6  1175
#define NOTE_DS6 1245
#define NOTE_E6  1319
#define NOTE_F6  1397
#define NOTE_FS6 1480
#define NOTE_G6  1568
#define NOTE_GS6 1661
#define NOTE_A6  1760
#define NOTE_AS6 1865
#define NOTE_B6  1976
#define NOTE_C7  2093
#define NOTE_CS7 2217
#define NOTE_D7  2349
#define NOTE_DS7 2489
#define NOTE_E7  2637
#define NOTE_F7  2794
#define NOTE_FS7 2960
#define NOTE_G7  3136
#define NOTE_GS7 3322
#define NOTE_A7  3520
#define NOTE_AS7 3729
#define NOTE_B7  3951
#define NOTE_C8  4186
#define NOTE_CS8 4435
#define NOTE_D8  4699
#define NOTE_DS8 4978

Code to Note

We'll include the pitches.h file at the beginning of the example to reference the notes. Then we'll setup the buzzer and play a sound to ensure that the buzzer is working as expected. Further in the loop() function after our condition statements, we'll add a few lines to make the buzzer play a sequence of notes. If one of the triggers is pressed 100 times, we'll play a special sequence of notes.

What You Should See (and Hear)

Press the triggers on the controller. You should hear a familiar 8-bit sound effect from a popular game coming from the piezo buzzer! Press one of the triggers 100 times to hear yet another familiar sound!

Coding Challenges

Broadcasting to an Army of Robots

Remember the GIF shown at the beginning of the tutorial? They were used to stress test the XBee 3's and examples used in this tutorial. Instead of controlling one robot, try broadcasting the commands from one controller to several robots! Just make sure to configure your XBees with unique addresses and adjust the controller's configuration for broadcasting.

wireless rc redbot

More with Buttons

The RedBot motor speed was set at one intensity. Instead of one set motor intensity for each character, try dividing the motor intensity for different characters by utilizing the other buttons. Or try adjusting the code to have the robot pivot left or right.

Methods of Transmitting Serial

Instead of sending one character to move, try adjusting the code to transmit different motor intensities and utilize the XBee's API packet structure. Or try sending serial through a mesh network configuration. You'll need to parse the data into an array and convert the string into numbers similar to the example code provided in the Remote Tank Steering Motor Controller. Instead of sending a character to a RedBot, the example had sent a string of characters to an Arduino with the Serial Controlled Motor Driver.

Controlling with Sensors

Instead of using buttons and a joystick, try using a motion sensor to control the RedBot based on movement like the RedBot''s accelerometer included in the kit. Or make a glove to control the RedBot based on gestures.

Hardware Upgrades

Remember, there are spots for additional Actobotics hardware cut into the Shadow Chassis!

31_Shadow-Chassis

Try adding a servo claw to pick up a small object like a pen.

  • Servo - Generic (Sub-Micro Size)

  • Pan/Tilt Bracket Kit (Multi Attachment)

  • Aluminum Channel - 4.50"

  • Micro Gripper Kit B - Hub Mount

LiPo Battery Monitoring

If you looked through the guide for the wireless controller, you'll notice that there are examples to monitor your LiPo battery! Try to combine code to control the RedBot with the LiPo Battery Monitor and micro OLED display.

32_LiPo-Battery-Monitoring

Sensing the Environment

Try sending data back from the line following sensors or encoders used in the RedBot kit back to the controller. Better yet, add the air quality sensor or humidity & temperature sensor to monitor the environment at a distance like a planetary rover. You'll need either a serial monitor or micro OLED connected to be able to view the data.

  • SparkFun Air Quality Breakout - CCS811

  • SparkFun Humidity and Temperature Sensor Breakout - Si7021

Efficiently Sending Commands

Try modifying the code to be efficient and save power instead of constantly sending commands. Currently, the controller repeatedly sends a command to notify the RedBot to stop, even when we are not pressing any buttons.

Troubleshooting

Not working as expected? Below are a few troubleshooting tips to get your micro:bits working as expected. For your convenience, relevant troubleshooting tips from the RedBot experiment guide were included below.

  • Having issues uploading?

    • Make sure your USB cable is plugged into both the robot and the computer you're using to write code.

    • Make sure the "POWER" switch is switched to "ON."

    • Double check that you have the right serial port selected under the "Tools" menu. The easiest way to check is to see which item disappears from the menu when you unplug the USB cable, and select that one when you plug the board back in.

    • If you have an Xbee module plugged in, make sure the Serial Select switch at the top edge of the board is switched to "XBEE SW SERIAL."

    • Check that you have the right board selected under the "Tools" menu. The Wireless Joystick uses the "SparkFun SAMD21 Dev Breakout" while the RedBot Mainboard uses "Arduino Uno". Also make sure that you have the correct COM port selected for each respective board.

  • My RedBot is not moving!

    • Make sure that the switches are set to the correct position for POWER, MOTORS, and XBEE SW Serial.

    • If you are using batteries, make sure that they have enough power.

    • Make sure that the XBees are configured correctly.

  • My RedBot is not driving straight! It is spinning or driving backward!

    • Make sure that the motor wires are wired correctly.

    • You can also adjust the code to tell what direction the motors to spin. Since the code is based on the setup used in the RedBot assembly guide, it would be easier to adjust the physical wire connection.

  • My RedBot is not driving straight! It drives in a curve!

    • This is a pretty common thing for the RedBot, and for all robots with independent drive wheels. There are lots of reasons for it, but it's something that simply must be dealt with. Here are a few possible reasons:

      • First -- check to make sure that there is nothing rubbing on either the wheels or on the magnetic motor encoder. Move the wheels out so that they are not rubbing, but still tightly seated into the motor. Any added friction on one side will cause one side to drive faster than the other (resulting in the RedBot pulling to one side.)

      • Second -- Driving straight requires equal power on both wheels. This requires equal amounts of traction on both wheels. Running the motors up at full power sometimes causes the wheels to "spin out" and lose traction. Try reducing the motorPower to something lower than 255.

      • Third -- use an encoder from the kit to ensure that both wheels turn the same distance each time.

Mfr Part # XB3-24Z8PT-J
RF TXRX MOD 802.15.4 TRC ANT TH
Digi
Mfr Part # 12649
INVENTOR'S KIT FOR REDBOT
SparkFun Electronics
$254.86
View More Details
Mfr Part # 14051
WIRELESS JOYSTICK KIT
SparkFun Electronics
Mfr Part # EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
Mfr Part # 11812
SPARKFUN XBEE EXPLORER USB
SparkFun Electronics
Mfr Part # 12016
CABLE USB2.0 A PLUG TO MCR B 6'
SparkFun Electronics
Mfr Part # 14456
SOLDERING IRON - 60W (ADJUSTABLE
SparkFun Electronics
Mfr Part # 08026
HOOK-UP SOLID 22AWG WHITE 25'
SparkFun Electronics
Mfr Part # JIC-2030
WIRE STRIPPER 20-30 AWG
Jonard Tools
Mfr Part # 14666
QWIIC FLEX GLOVE CONTROLLER
SparkFun Electronics
More Info
View More Details
Mfr Part # 09065
SERVOMOTOR RC 6V GENERIC SUB-MIC
SparkFun Electronics
Mfr Part # 13177
MICRO GRIPPER KIT B HUB MNT
SparkFun Electronics
Mfr Part # 14193
AIR QUALITY SENSOR BOARD
SparkFun Electronics
Mfr Part # 12589
SPARKFUN REDBOT SENSOR ACCEL
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.