Maker.io main logo

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously

749

2023-06-21 | By Don Wilcher

A task scheduler is a program that schedules, manages, and executes jobs or tasks in an ‎operating system or application, even those requiring specific operation times. A washing ‎machine or dishwasher would be one example of a task scheduler executing cycle times for ‎cleaning clothes and dishes based on specific time intervals. These intervals are programmed in ‎a microcontroller, which then executes various washing modes managed by the task scheduler. ‎This article will explain how you can code and use a task scheduler to blink 3 LEDs ‎simultaneously at various intervals.

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously

The Task Scheduler Demo Concept

The task scheduler concept demonstrates how to automate and execute tasks at predetermined ‎times under specific conditions. Sensors and digital switches can both set off conditions in a ‎manufacturing setting. If the condition is true or false, the task will then run for a specific ‎amount of time or duration. Once complete, the scheduler initiates the new task according to ‎its conditional requirements. This demo concept illustrates blinking three LEDs at discrete or ‎unique timing intervals and is constructed using three basic elements: a scheduler, the task, and ‎the time interval.

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously The Multi-Blink LED tasks scheduler.

Based on a conditional statement, the scheduler will initiate the Blink 1 task. The system’s ‎current time will then be utilized to check the LED 3’s last toggle state. If the difference ‎between the current time and the last toggle state time is greater than or equal to the defined ‎blink interval time, then LED3 will blink. LED2 and LED1’s blink tasks will execute this same ‎checking process used by LED3. The blink intervals used in the task scheduler demo are listed ‎below.

  • const long BLINK_TIME_1 = 1000; // 1 second
  • const long BLINK_TIME_2 = 500; // 0.5 seconds
  • const long BLINK_TIME_3 = 250; // 0.25 seconds

This scheduling time interval process will continue until the task scheduler has been instructed ‎to stop. There are a few unique aspects on display here — for one, a reset button can ‎temporarily stop the task scheduler from completing the multi-blink tasks. Additionally, no ‎delay() instructions are used in the code. Although the delay () instruction method provides a ‎specific pause function of an executable instruction, the timing operation is inaccurate. For ‎real-time systems, it’s imperative for the timing to be as accurate as possible. Therefore, a ‎real-time operating system (RTOS) will use the system’s internal clock or timing feature to ‎provide accurate time for activating events. The Arduino instruction millis() will provide ‎accurate timing for the Multi-Blink Tasks Scheduler. You may find additional information on ‎RTOS here.

Building an Arduino Task Scheduler

Building an Arduino Task Scheduler is quite easy to achieve. You may use a library such as the Scheduler library to explore the concept of task schedulers. The Scheduler library can be easily ‎installed, and once active, the example code will provide information for wiring three LEDs to ‎the specific digital pins of an Arduino SAMD-based microcontroller board, such as the Due, Zero, ‎or many of the MKR boards among others.

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously The Scheduler Library installed.

Running the Scheduler code on an Arduino Uno will cause a compilation error due to the ‎ATMEGA328 microcontroller being incompatible with the Scheduler Library’s header file. An ‎alternative solution is to use a faux Arduino Task Scheduler code:

Copy Code
‎// Define LED pins‎
const int LED_PIN_1 = 11;‎
const int LED_PIN_2 = 12;‎
const int LED_PIN_3 = 13;‎
‎// Define delay times‎
const long BLINK_TIME_1 = 1000; // 1 second
const long BLINK_TIME_2 = 500;  // 0.5 seconds
const long BLINK_TIME_3 = 250;  // 0.25 seconds
‎// Define task times‎
unsigned long task1Time = 0;‎
unsigned long task2Time = 0;‎
unsigned long task3Time = 0;‎
‎// Define task intervals
const long TASK_INTERVAL_1 = 2000; // 2 seconds
const long TASK_INTERVAL_2 = 1000; // 1 second
const long TASK_INTERVAL_3 = 500;  // 0.5 seconds
void setup() {‎
‎  // Set LED pins as output‎
‎  pinMode(LED_PIN_1, OUTPUT);‎
‎  pinMode(LED_PIN_2, OUTPUT);‎
‎  pinMode(LED_PIN_3, OUTPUT);‎
‎}‎
void loop() {‎
‎  // Check if it's time to run task 1‎
‎  if (millis() - task1Time >= TASK_INTERVAL_1) {‎
‎    task1Time = millis();‎
‎    digitalWrite(LED_PIN_1, !digitalRead(LED_PIN_1)); // Toggle LED 1‎
‎  }‎
‎    // Check if it's time to run task 2‎
‎  if (millis() - task2Time >= TASK_INTERVAL_2) {‎
‎    task2Time = millis();‎
‎    digitalWrite(LED_PIN_2, !digitalRead(LED_PIN_2)); // Toggle LED 2‎
‎  }‎
‎    // Check if it's time to run task 3‎
‎  if (millis() - task3Time >= TASK_INTERVAL_3) {‎
‎    task3Time = millis();‎
‎    digitalWrite(LED_PIN_3, !digitalRead(LED_PIN_3)); // Toggle LED 3‎
‎  }‎
‎    // Add a delay to prevent the loop from running too fast‎
‎  delay(10);‎
‎}‎
 

Open the Arduino IDE and copy and paste this code into the editor. The hardware components, ‎Bill of Materials (BOM), and the electronic circuit schematic diagram required to build the ‎Multi-Blink LED Task Scheduler are located here. You can use the hardware demonstrator ‎electrical wiring diagram as an additional source of construction information for the task ‎scheduler.

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously The Multi-Blink LED Task Scheduler solderless breadboard electrical wiring diagram.

The Multi Blink LED Tasks scheduler final assembly serves as another build reference for device ‎construction.

How to Use an Arduino Task Scheduler to Run Multiple Functions Simultaneously The Multi-Blink LED Task Scheduler.

The Arduino IDE’s pasted code can be compiled and uploaded to the Arduino Uno. LED 1 will ‎blink at 0.5 seconds, with LED2 operating at 1 second and LED3 running at 2 seconds. The ‎onboard LED will blink at 0.5 seconds due to being hardwired to the Arduino board’s digital pin ‎‎13. Explore the tasks scheduler further by changing the blink interval times and observing the ‎LED’s responses. Aside from using discrete LEDs, you can modify the task scheduler device’s ‎code to switch devices like servo motors ON/OFF at specific intervals. Click here to see the task ‎scheduler in operation.

Mfr Part # A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
Mfr Part # CF14JT220R
RES 220 OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
Mfr Part # SSL-LX5093HD-TR
LED RED DIFFUSED T-1 3/4 T/H
Lumex Opto/Components Inc.
More Info
View More Details
Mfr Part # HLMP-1401-D0002
LED YELLOW DIFFUSED T-1 T/H
Broadcom Limited
Mfr Part # LTL-4233
LED GREEN DIFFUSED T-1 3/4 T/H
Lite-On Inc.
Mfr Part # DKS-BBOARD3.3
DIGI-KEY BREADBOARD 3.3
DigiKey Standard
Mfr Part # A000062
ARDUINO DUE ATSAM3X8E EVAL BRD
Arduino
Mfr Part # ABX00027
ARDUINO NANO 33 IOT
Arduino
Mfr Part # ABX00012
ARDUINO MKR ZERO W/ HDR ATSAMD21
Arduino
Mfr Part # ABX00023
ARDUINO MKR WIFI 1010
Arduino
Mfr Part # ABX00029
MKR WAN 1310 W/O ANTENNA
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.