Maker.io main logo

Laser Cut Santa Stop Here Edge Lit Sign

48

2025-12-11 | By Kitronik Maker

License: See Original Project Laser Cutters LEDs / Discrete / Modules

Courtesy of Kitronik Maker

Guide by Kitronik Maker

Christmas is now just around the corner but there's still plenty of time for making. Emma's been back on the laser cutter to produce something for you to have a go at. All you'll need is some acrylic and a Kitronik USB RGB LED strip and you're good to go.

In this project we’re making a very simple edge lit sign that would look at home among your existing Christmas decorations. Grab the DXFs and let’s get started!

We Used:

The Base:

base_1

Step 1:

Download our DXF, which contains the design and the Base which fits the new RGB USB LED Strip.

Step 2:

Cut out the Base from your choice of Acrylic. We have used Orange Fizz Sweet Pastels Perspex® but you can use any colour you want. Use the screws and encase the RGB LED Strip in the base.

The Laser Cut Edge-Lit Sign:

sign_2

Step 1:

Grab the DXF and either load it straight into your laser cutter software or if you want to personalise it, you can load the design into your CAD program of choice and tweak it to taste (pictured above is LibreCAD).

Step 2:

stop_3

Following the guide above, pop some 5mm clear acrylic (we used our Value cheap acrylic sheets) on your laser cutter and cut as shown. There are three different types of cut in the design; cut all of the way through, engraving and kiss cut.

Step 3:

sign_4

Introduce the base to the edge-lit sign, plug the strip into a suitable power source and you're done. You should now have something that resembles the sign above, mince pies not included.

If you have a go at making one of these signs, or one that is inspired by it, we would love to see it. Please share them via social media and tag us so we can share it with everyone.

Make sure you don't miss out on other news or free resources by signing up for our newsletter here.

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.

Mfr Part # 3561
LED MOD RGB LNR LGT STRIP
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.