Maker.io main logo

Send Temperature & Humidity SMS Every Minute to Your Phone - SIM900GSM &

2026-04-07 | By Ron Cutts

License: GNU Lesser General Public License Humidity Temperature Wifi Arduino ESP32

In this tutorial, you will learn how to send sms with Temperature and Humidity data using the SIM900 GSM Shield, DHT11 sensor and Visuino.

You can set your own timing. In this tutorial, we will use approx. 1 minute, but you can easily adjust the timing according to your needs,

Watch the Video!

Also check out these tutorials: 

Make a Phone Call Using the SIM900 GSM Shield & Arduino - Visuino Tutorial

Send SMS Using SIM900 GSM Shield & Arduino - Visuino Tutorial

Learn more about Visuino: What is Visuino

What You Will Need

  • SIM900 GSM Shield

  • Arduino UNO

  • SIM card (You should disable the PIN request on the SIM card before using it with the GSM shield)

  • DHT11 Temperature & Humidity sensor

  • Jumper wires

  • 5V power supply with enough amps for the shield

  • Visuino program: Download Visuino

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

The Circuit

  • Connect the SIM900 GSM Shield to the Arduino

  • Connect DHT11 pin [VCC] to Arduino pin [5V]

  • Connect DHT11 pin [GND] to Arduino pin [GND]

  • Connect DHT11 signal pin [S] to Arduino (shield) Digital pin [2]

  • Connect with the Jumpers on the shield pins D8(RX) & D7(TX) as you see it in the picture

  • Make sure that the antenna is connected to the shield

  • Connect the 5V Power Supply to the shield, and set the switch on the shield to the External Power (See the picture)

  • Once the Power is connected, hold the Power button for 2 seconds

  • Once the connection with the Network is established, the LED will blink every 3 seconds

The Circuit

The Circuit photo 2

The Circuit photo 3

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Software Serial Port" component

  • Add "Text Value" component

  • Add "Sequence" component

  • Add "DHT11" component

  • Add "Char Value" component

  • Add "Text Multi-Source Merger" component

  • Add "Formatted Text" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Add Components photo 5

In Visuino Add Components photo 6

In Visuino Add Components photo 7

In Visuino Add Components photo 8

In Visuino Set Components

  • Double-click on the "TextValue1" and in the Elements window

  • Command to set GSM shield to text mode: drag "Set Value" to the left side and in the properties window set "Value" to AT+CMGF=1

  • Command to set Phone number (International Format): drag another "Set Value" to the left side and in the properties window set "Value" to AT+CMGS="+495XXXXXX" 

  • Command to set Text Message: In the Elements window, drag another "Set Value" to the left side and in the properties window select "Value" and click on the pin Icon and select "String SinkPin"

  • Close the Elements window

  • Double click on the "FormattedText1" and in the "Elements" window drag 2X "Analog Element" to the left side, and for both set in the properties window "Precision" to 1

  • Close the Elements window

  • Select "FormattedText1" and in the properties window set "Text" to: TEMP: %0 HUM: %1

  • Select "CharValue1" and in the properties window set "Value" to #26

  • Select "Sequence1" and in the properties window set "Repeat" to: true

  • Double click on the "Sequence1" and in the "Elements" window, drag 4X "Period" to the left side

  • For the "Period1" in the properties window, set "Delay" to 5000

  • For the "Period1" in the properties window, set "Delay" to 15000

  • For the "Period1" in the properties window, set "Delay" to 20000

  • For the "Period1" in the properties window, set "Delay" to 25000

  • Close the Elements window

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Set Components photo 5

In Visuino Set Components photo 6

In Visuino Set Components photo 7

In Visuino Set Components photo 8

In Visuino Set Components photo 9

In Visuino Set Components photo 10

In Visuino Set Components photo 11

In Visuino Connect Components

  • Connect "Start1" pin [Out] to "Sequence1" pin [Start]

  • Connect "HumidityThermometer1" pin [Sensor] to Arduino Digital pin [2]

  • Connect "HumidityThermometer1" pin [Temperature] to to "FormattedText1" > "AnalogElement1" pin [In]

  • Connect "HumidityThermometer1" pin [Humidity] to to "FormattedText1" > "AnalogElement2" pin [In]

  • Connect "FormattedText1" pin [Out] to "TextValue1" > "Set Value3" pin [Value]

  • Connect "Sequence1" > "Period1" pin [Out] to "TextValue1" > "Set Value1" pin [Clock]

  • Connect "Sequence1" > "Period2" pin [Out] to "TextValue1" > "Set Value2" pin [Clock]

  • Connect "Sequence1" > "Period3" pin [Out] to "TextValue1" > "Set Value3" pin [Clock]

  • Connect "Sequence1" > "Period4" pin [Out] to "TCharValue1" pin [Clock]

  • Connect "TextValue1" pin [Out] to "TextMultiMerger1" pin [0]

  • Connect "CharValue1" pin [Out] to "TextMultiMerger1" pin [1]

  • Connect "TextMultiMerger1" pin [Out] to "SoftwareSerial1" pin [In]

  • Connect "SoftwareSerial1" pin [RX] to Arduino Digital pin [7]

  • Connect "SoftwareSerial1" pin [TX] to Arduino Digital pin [8]

Optional if you want to monitor response from the GSM shield: Connect "SoftwareSerial1" pin [Out] to Arduino Serial pin [In]

In Visuino Connect Components

In Visuino Connect Components photo 2

In Visuino Connect Components photo 3

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

When you power the Shield, wait a bit for the connection with the network to be established. Once the connection is established, the LED on the shield will blink every 3s.

The "Start" component will automatically start the "Sequence" component, and the "Sequence" component will first set the GSM shield into Text mode, set the phone number, set the sms based on values from the DHT11 sensor, and send sms.

Congratulations! You have completed your GSM project with Visuino. Also attached is the Visuino project that I created for this Tutorial. You can download and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.