Maker.io main logo

Artemis Development with Arduino

31

2019-08-28 | By SparkFun Electronics

License: See Original Project Programmers Wireless

Courtesy of SparkFun

The SparkFun Artemis is an amazing module. So much functionality packed into a tiny 10x15mm footprint! But what really makes it powerful is the ability to quickly write sketches and build projects using only Arduino code. Whether you are using one of our boards that has the Artemis module pre-integrated or have your own, this tutorial will show you how to install SparkFun's Apollo3 Arduino core and get you up and blinking in less than 5 minutes!

 

 

Required Materials

To follow along with this tutorial, you'll need one of the following Artemis carrier boards such as the BlackBoard, BlackBoard Nano, or BlackBoard ATP and a USB C cable.

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

  • Installing an Arduino Library: How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

  • Designing with the SparkFun Artemis: Let's chat about layout and design considerations when using the Artemis module.

Arduino Installation

With the Arduino Board Manager, installing new board support within your Arduino IDE is a breeze!

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Installing the Arduino Core for Apollo3

We've built the Arduino core for Apollo3 from scratch, making it as lightweight and easy to use as possible.

To install the SparkFun Apollo3 Arduino Core:

  • Open the Arduino IDE (must be v1.6.12 or later)

  • Navigate to Preferences

Navigate to Preferences

  • In the "Additional Board Manager URL" box, add 

Copy Code
https://raw.githubusercontent.com/sparkfun/Arduino_Boards/master/IDE_Board_Manager/
package_sparkfun_index.json

 

Preferences

  • Go to Tools > Board and select the Boards Manager

Arduino-BoardsManager

  • Search for "Apollo", and you should find the SparkFun Apollo3 board package.

  • Make sure the latest version is selected and click Install.

SparkFun-Arduino-Apollo3-Boards-Install

Installation may take a few minutes -- included in the install are all necessary source files for the Arduino core and Apollo3 libraries, plus all of the compiler and software-upload tools you'll need to use the Artemis with Arduino.

Once the board definitions have been installed, you should see a new set of Artemis boards under your Tools > Board menu.

SparkFun-Arduino-Apollo3-Boards-List

Example: Blink It Up!

The Blink example is about as basic as it gets. But it is also a good benchmark to make sure you've got your core installed correctly and you can upload code to your module. To run this example, select your board from the Board Managers pulldown and choose the correct USB port. You can load the blink example by clicking on File->Examples->01.Basics->Blink.

ArtemisBlinkItUp

Hit the upload button and enjoy the blinky goodness!

BlackBoard-Artemis

Look at all the blinky!

Example: All the Features

We've built the Arduino core for Artemis from the ground up. Be sure to checkout the large number of built-in examples. You'll find them under File->Examples->'Examples for Artemis'.

Artemis-I2C-Examples-SmallMenu

We've got examples for setting up multiple I2C ports (it's amazingly easy), writing to EEPROM, using SoftwareSerial (all 48 pins can be serial!), using the the onboard microphone, and using servos (up to 32!). We're adding more all the time so be sure to keep your core up to date.

Bootloader Options

Each Artemis comes preloaded with two bootloaders. The SparkFun Variable Bootloader (SVL) will allow you reliably and conveniently load new code at data rates up to 921600bps. In addition to the SVL, we also enable the Ambiq factory bootloader for secure boot applications. Almost all users should use the SparkFun Variable Bootloader and forget about the Ambiq factory bootloader. For more information checkout the programming section of the Designing with the Artemis Module tutorial. Don't worry - you cannot damage or brick your Artemis using the incorrect bootloader.

SparkFun_Artemis_Core-Bootloading_Type

Don't select Ambiq Secure Bootloader unless you know what you're doing

Beyond Arduino

The SparkFun Apollo3 core supports all the standard Arduino functions. This means you can program digitalWrite I/O, analogRead ADC pins, Serial print to the Serial monitor, interact with hardware serial using Serial1, and even perform more complex I2C or SPI writes with the Wire and SPI libraries. The basics are there, so let's dive in to some more advanced capabilities of the Artemis!

Ambiq has created a software development kit to fully flex the Apollo3. The Ambiq SDK contains a large number of examples and demonstrates all sorts of incredible aspects of the Apollo3. Each example uses various functions that look like this:

Ambiq-SDK-HAL

These long-named-functions are part of what's called a HAL or hardware abstraction layer. We aren't going to go into the specifics of setting up or using the SDK right now, but just know that the the SparkFun Arduino Apollo3 core is built upon this HAL which means you can call HAL functions directly inside the Arduino environment.

Copy Code
// Clear the RTC alarm interrupt.
am_hal_rtc_int_clear(AM_HAL_RTC_INT_ALM);

Ambiq_HAL_inside_Arduino_IDE

This is a powerful tool for advanced users; you can use the built in Arduino functions such as Serial.begin(9600) and delay(100) while integrating more advanced HAL functions for controlling things like interrupts.

If you do decide to dig into the SDK, head on over to our Using SparkFun Edge Board with Ambiq Apollo3 SDK tutorial for more information!

Board

Using SparkFun Edge Board with Ambiq Apollo3 SDK

MARCH 28, 2019

We will demonstrate how to get started with your SparkFun Edge Board bysetting up the toolchain on your computer, examining an example program, andusing the serial uploader tool to flash the chip.

Troubleshooting

Need help?

If your product is not working as you expected or you need technical assistance or information, head on over to the SparkFun Technical Assistance page for some initial troubleshooting.

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for help. If this is your first visit, you'll need to create a Forum Account to search product forums and post questions.

SparkFun Artemis Forums

Resources and Going Further

And lastly, Artemis has been designed and proven to work with our entire range of 50 Qwiic boards. Be sure to checkout and get inspired by what's possible by just plugging in the sensors and outputs you need to build something amazing!

Mfr Part # 15444
REDBOARD ARTEMIS
SparkFun Electronics
Mfr Part # 15442
REDBOARD ARTEMIS ATP
SparkFun Electronics
Mfr Part # 15425
CBL USB2.0 A PLUG TO C PLG 2.62'
SparkFun Electronics
Mfr Part # 15484
RF TXRX MOD BT TH SMD
SparkFun Electronics
Mfr Part # 15443
REDBOARD ARTEMIS NANO
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.