Maker.io main logo

How to Create a Reaction Game for HaloHD for micro:bit with EduBlocks

41

2024-05-09 | By Kitronik Maker

License: See Original Project micro:bit

Courtesy of Kitronik

Guide by Kitronik Maker

Introduction

Hello, I am Luke from Aquinas College. I have always enjoyed the challenge of ‎writing software and learning about how technology can solve a variety of real-‎world problems. Kitronik allowed me to experience this by allowing me to create an ‎extension for their HaloHD product for the micro:bit. This developed my ‎understanding of different programming languages whilst learning what a job in the ‎industry truly is like. My week at Kitronik bettered my skills in programming in ‎multiple languages.‎

How I Coded an Extension for the HaloHD

I programmed an extension that allowed users to code onto the HaloHD, using a ‎micro:bit, with the EduBlocks platform. This code contained three core files: ‎definitions, generators, and toolbox. The definitions contain the name of the block ‎and what information will be displayed and passed. The generators generate code ‎into Python code which is used by EduBlocks. The toolbox links the definitions and ‎the generators. When put together, these files made the extension for EduBlocks ‎which I used to code my game. I coded five blocks which did the following: ‎imported the 'neopixel' feature, initialise 'neopixel', set individual led colour, set all ‎LEDs to a certain colour, and show LEDs.‎

Concept of the Game

I then coded a game on the platform in which a user battled an enemy led. The ‎user and enemy would randomly generate at different LEDs and would be ‎represented by a green and a red colour. They would move towards each other, ‎and the user would have to press the A button so that it destroyed the enemy when ‎they were in the pixels next to each other. If the user failed too, they would lose. If ‎the user was successful then the next round would start, at a faster pace. To win, ‎the user must complete the game at the fastest pace.‎

Main Techniques

The main stages to creating the game are:‎

  • Importing libraries, we will need
  • Setting up our variables
  • The main game loop
  • Validation of pixel numbers
  • Generating random numbers
  • Array bounds
  • Setting and showing pixels
  • Checking if the game is won/lost
  • Validating variables

Creating an EduBlocks Project

To code the game, we need to create a new project in EduBlocks. For the project ‎we need to select BBC micro:bit mode and click the Start Coding button at the ‎bottom right corner of the screen to being.‎

Once in the project editor, we want to add the Kitronik HaloHD extension. We can ‎do this by clicking the plus (+) button in the bottom left corner of the screen and ‎select ZIP Halo HD from the approved extension list.‎

Coding the Game

For the first stage, we need to import the libraries that the program will need to use. ‎Firstly, the micro:bit import allows us to use features on the micro:bit. Secondly, ‎the random import, which will allow us to generate a random integer. Lastly, the ‎import KitronikHaloHD library which is a block from the HaloHD extension which ‎will allow us to use the pixels on the HaloHD. We do this by dragging the following ‎blocks onto the startcode.‎

blocks_1

Here, we create the variables we need for the program. Firstly, the halo variable ‎which is a HaloHD object (collection of variables and methods), in this instance for ‎our LEDs. Secondly, we create the delay variable which determines how long the ‎game sleeps for each round. Next the value for the enemy and player pixels. Lastly ‎two boolean values, one which loops the main game, and the other which is used to ‎validate values.‎

blocks_2

Here we use a loop to keep the game in play whilst the player is winning. We use ‎the winning variable here, which changes when the player loses. All the code for ‎the game is in this loop.‎

loop_3

Next, above the while winning loop use a function checkValid to use a series of ‎conditions to validate the enemy and player variables. We use this to validate the ‎player and enemy pixels. The if statement which will be called from inside the while ‎not valid loop, determines when the variables are not valid and so return False. ‎Here add if statements to return that the positions are not valid when they are next ‎to each other.‎

Next, they are not valid unless they are both on either even or odd pixels. This ‎ensures the pixels meet each other at some point around the HaloHD circle. If they ‎are then none of the conditions are true and the loop reaches to bottom to exited ‎exit, returning True.‎

loop_4

Now inside the while winning loop create a while statement so that the program will ‎continue to generate a random combination of numbers until they are valid by using ‎the checkValid function. We use the 'import random' feature. To generate the ‎random number, we use the random.randint function. This isn't built into EduBlocks, ‎so you will need to use 'your own code' blocks. This will be used to pick a random ‎spawning location for the enemy and player. We do this twice to get a more ‎effective result.‎

random_5

Next, outside of the while not valid loop, the pixels both rotate one value along the ‎circle.‎

circle_6

Next, we will use IF statements, which works by determining if the condition is true, ‎and if it is it will perform some code. We use if statements for many things like to ‎check; the spawning point of the pixels is fair, and that they don't spawn next to ‎each other. Here use if statements to guarantee that the pixels keep moving even ‎when they meet the end of the LEDs on the HaloHD.‎

statements_7

Next the value for the colour of the enemy pixel is set to red and the player pixel is ‎set to green and then shown on the HaloHD. Before doing this clear the previously ‎shown LEDs on the HaloHD so the enemy and player pixels last position are ‎removed.‎

color_8

This condition checks whether the player lost against the enemy pixel. It ‎determines whether the game loop is exited or not, and therefore if the game is ‎continued.‎

condition_9

This statement decides whether the game has been won, and the challenge has ‎been completed at the fastest speed. The next bit of code sleeps the loop for the ‎amount of time that’s set related to the round.‎

statement_10

Full Game Code

Copy Code
# Start Code Here
from microbit import *
import random
from KitronikHaloHD import *
halo = HaloHD()
delay = 1000
enemy = 0
player = 0
winning = True
valid = False
def checkValid(enemy, player):
if enemy == player:
return False
elif enemy + 1 == player:
return False
elif enemy == player + 1:
return False
elif enemy % 2 != player % 2:
return False
return True
while winning:
while not valid:
enemy = random.randint(0, 59) # your own code
player = random.randint(0, 59) # your own code
valid = checkValid(enemy, player) # your own code
enemy += 1
player -= 1
if enemy > 59:
enemy = 0
if player < 0:
player = 59
halo.clearLEDs()
halo.setLED(enemy, (64, 0, 0))
halo.setLED(player, (0, 64, 0))
halo.showLEDs()
if enemy == player:
if button_a.was_pressed():
delay -= 50
valid = False
else:
display.scroll("Game LOST!")
winning = False
if delay == 100:
display.scroll("Game WON!")
winning = False
sleep(delay)

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik’s prior written consent.

Mfr Part # 5672
KITRONIK ZIP HALO HD FOR MICRO:B
Kitronik Ltd.
Mfr Part # EDUBIT
EDU:BIT WITH MICRO:BIT V2
Cytron Technologies Sdn Bhd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.