Maker.io main logo

Tips and Tricks: Maximizing Bed Adhesion with Cura LE

168

2024-03-14 | By Lulzbot

License: See Original Project 3D Printing

Courtesy of LulzBot

Guide by LulzBot

lulzbot_1

‎3D printer bed adhesion is the foundation of a successful print, but there are ‎circumstances that make adhesion a challenge, even if your PEI surface has ‎been properly maintained.‎

  • 3D models don't always load in Cura LulzBot Edition with the optimal orientation ‎for printing

  • Some 3D models lack a flat surface or obvious base

  • Some models have minimal surface area for bed contact in any orientation

  • Certain filament materials are more prone to warping or curling

printer_2

The following LulzBot 3D printer tips and tricks will help you improve those challenging ‎‎3D prints by maximizing print bed adhesion during the printing process.‎‎ ‎

Optimally Orienting Your Model

Models do not always load in Cura LE with the optimal orientation. Before you begin ‎printing, it's always a good idea to consider how rotating your model could potentially ‎improve bed adhesion and overall print quality. Your goal is to maximize print bed ‎contact and layer bonding while minimizing the number of overhangs and bridges.‎

Note: The maximum overhang angle your LulzBot printer can successfully produce is a ‎factor of the material being used, the layer thickness, the cooling fan speed, and the ‎tolerance for surface imperfections for a given use case. If you're not sure how shallow ‎of an angle the filament can handle, try printing an overhang angle test object.‎ ‎

  1. In Cura, select your model, then select the Rotate icon on the left-hand side of ‎your screen.‎‎

  2. The Rotate tool gives you the ability to orient your model along three axes. The ‎red circle will allow you to rotate around the X-axis. The blue circle will rotate ‎around the Z-axis. The green circle will rotate around the Y-axis.‎‎

  3. When you’ve found the optimal side to print as the base, use the Lay Flat icon to ‎ensure that the flat portion of your print is securely attached to the print surface. ‎It is highly recommended to use this option after rotating your model on the Z-‎axis as it will help prevent adhesion issues during the print.

icon_3

Note: Adding brim to your print can help improve adhesion as well. Brim adds concentric ‎perimeters around the base of the print, better adhering the print to the heated plate. ‎This is only one layer thick, and easily removed post-print. To add Brim to your print, ‎select Custom Print Setup, and then select Brim under Build Plate Adhesion Type.‎‎ ‎‎

‎Tricks for Improving Adhesion

By altering the model, itself, you can be much more selective in how the model is printed. ‎Here are four methods to get you started manually altering your models.‎

‎1. Drop the Base‎

Depending on how you intend to use your printed object, you can lower the model’s Z-‎axis in order to create a greater surface area in contact with the bed. The model will lose ‎some of its height but will widen the base in the process, stabilizing the print with ‎improved bed adhesion.‎

This technique works well for organic shapes likes models of bones, artifacts, and ‎sculptures. Spheres are a good example because Cura shows the section of the model ‎that is too steep to print in red. Simply select the blue Z-axis arrow and move your model ‎downwards slowly until the red area is underneath the print surface, creating a 30-‎degree print angle or less.‎

base_4

‎‎2. Divide and Conquer‎

You can use a similar technique to effectively cut your model in half, and then bond the ‎halves together with glue. Using this technique, your model won't have an artificial flat ‎surface, but will have a glue seam.‎

Take note of the total height of the Z-axis by selecting the model and then Scale. Divide ‎the number in half and write it down. Then select Move and enter the number into Z as ‎a negative value. You should now see half of the model pushed down below the print ‎surface.‎

If your model is symmetrical all around, like a sphere, simply right click the model and ‎make a duplicate, and repeat dividing it in half.‎

If your model is asymmetrical, right click the model and make a duplicate, then rotate the ‎duplicate 180 degrees along the Y-axis, until it’s completely upside down. Type in a ‎negative Z value for half the Z-axis of your object and hit enter.‎

divide_5

‎3. Mouse Ears‎ ‎

*Requires modeling software

Mouse ears are an excellent method for increasing adhesion of warp-prone materials like ‎ABS or Nylon, particularly if your model has limited print surface contact. Note that the ‎mouse ears will need to be manually cut off of your model after printing.‎

Download a mouse ears stl file, then in your modeling software, place the single-layered ‎discs (mouse ears) through areas with poor print adhesion. Make sure the mouse ears are ‎a single-layer tall, and then center the mouse ears around any section of your model that ‎might warp during printing. This added layer will create a greater bond to keep the print ‎steady and help prevent warping.

mouse_6

Example Scenario: How to Print an L-Shaped Pipe

Using this L-shaped pipe model as an example, take a moment to imagine how the tool ‎head would move during printing. From the bottom up, layer by layer, you can tell the ‎print would have difficulty adhering to the bed because there isn't a flat base to build on. ‎What a perfect opportunity to use one of the techniques discussed earlier!‎

Drop The Base wouldn't be appropriate here because the model is mechanical, and ‎altering the shape would affect the functionality. Instead, try the Divide and Conquer ‎technique - sinking half the model through the surface, duplicating, rotating 180 degrees ‎if needed, moving the halves apart, printing, and the adhering the halves together. Once ‎this has been set up in Cura, adding Brim to the Build Plate Adhesion settings will help ‎ensure that each half maintains a strong bond during printing.‎

example_7‎ ‎

Step 1: Rotate model to find optimal side.

step_1

Step 2: Calculate half the Z-axis height 37.7734/2 = 18.8867.

step_2

‎Step 3: Select Move, and in the Z field, enter half the Z-axis height as a negative value.

‎‎step_3

Step 4: Right click the model, Select Multiple Selected Model, and select 1 for Number ‎of Copies.‎

‎‎step_4‎ ‎‎

Step 5: Enter in negative value for half the Z-axis height.‎ ‎

step_5‎ ‎

Step 6: Select Brim for Build Plate Adhesion ‎ ‎‎

step_6 ‎‎

‎Step 7: Remove print, trim brim off the prints, and adhere sides together.‎ ‎ ‎

step_7 ‎‎

‎Related Products

LulzBot TAZ Dual Extruder v3.1 Tool Head | 0.5 mm

PolyDissolve S1 Polymaker

Mfr Part # KT-CP0162
LULZBOT TAZ DUAL EXTRUDER V3.1 T
LulzBot
$882.34
View More Details
Mfr Part # RM-PE0032
POLYMAKER POLYLITE PETG FILAMENT
LulzBot
More Info
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.