Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Current-Sense-Slide8

Another type of current sensor is essentially a high voltage difference amplifier. This type of part features a precision input resistor bridge, which is used to attenuate the input voltage to a range that is tolerable by the input amplifier. High common mode rejection is achieved by laser trimming the input resistor network to within 0.01% matching.

PTM Published on: 2009-04-23