Some additional terms include: USB 3.0 (SuperSpeed USB) is the latest version of the USB specification. It operates at 5 Gbps, 10 times faster than USB 2.0 and provides up to 4.5 W of power which is 1.8 times more than what USB 2.0 provides. USB 3.0 is backward compatible with USB 2.0 such that a brand new PC or tablet equipped with USB 3.0 ports can still work seamlessly with older USB 2.0 devices. The USB 3.0 Host is a controller on the bus that directs traffic flow and distributes power over the bus. USB 3.0 Device is a peripheral on the bus such as a video camera or a portable hard disk drive. The USB 3.0 peripheral controller is a microcontroller in the USB 3.0 device that handles the USB 3.0 protocol and communicates with the USB 3.0 host. For example, CX3 is a USB 3.0 peripheral controller. The USB video class (UVC) is a specification that defines the standard behavior of a USB video camera, known as UVC camera. UVC cameras are widely adopted and are supported by major PC operating systems. All built-in webcams in Notebook computers are UVC cameras. The USB 3 vision is a specification that defines the standard behavior of a USB 3.0 video camera using machine vision, known as a USB 3 Vision camera. USB 3 vision specification was ratified in 2013 and has been widely adopted by machine vision and industrial cameras.
 
                 
                 
                 
 
 
 
 Settings
        Settings
     Fast Delivery
                                    Fast Delivery
                                 Free Shipping
                                    Free Shipping
                                 Incoterms
                                    Incoterms
                                 Payment Types
                                    Payment Types
                                





 Marketplace Product
                                    Marketplace Product
                                 
             
                     
                                 
                                 
                                 
                         
                                 
                                 
                                 
                                 
                                 
                                 
                                 New Zealand
New Zealand