Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Tiva C Series TM4C123x Low Power Slide 3

This slide shows the details of the run mode. This mode provides normal operation of the processor and enabled peripherals, i.e., the ones that are enabled in the RCGC registers. The microcontroller actively executes code with maximum performance in this mode, and the system clock can be any of the available clock sources such as the main oscillator, precision internal oscillator, low-frequency internal oscillator, or PLL.

PTM Published on: 2013-09-09