Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
RF-Synthesizers-Slide1

Welcome to the STMicroelectronics RF Synthesizers Up to 16 Gigahertz product training module. This presentation will introduce the STuW81300 and STW81200 RF synthesizers, and include a brief review of ST’s RF synthesizer offerings. The tutorial will focus on ST’s standard product RF synthesizers, covering frequencies from 47 MHz up to 16 GHz. It will highlight the STuW81300 mWave synthesizer and the STW81200 wide band RF synthesizer. The presentation will also discuss the potential markets for these devices.  

PTM Published on: 2016-03-01